Struct containing the parameters required for encrypting/decrypting a message in a segmented operation. Must be updated between each add data step of a segmented operation.
More...
#include <AESCCM.h>
Struct containing the parameters required for encrypting/decrypting a message in a segmented operation. Must be updated between each add data step of a segmented operation.
§ input
| uint8_t* AESCCM_SegmentedDataOperation::input |
- Encryption: The plaintext buffer to be encrypted and authenticated in the CCM operation.
- Decryption: The ciphertext to be decrypted and verified.
§ output
| uint8_t* AESCCM_SegmentedDataOperation::output |
- Encryption: The output ciphertext buffer that the encrypted plaintext is copied to.
- Decryption: The plaintext derived from the decrypted and verified ciphertext is copied here.
§ inputLength
| size_t AESCCM_SegmentedDataOperation::inputLength |
Length of the input/output data in bytes. Must be non-zero, multiple of the AES block size (16 bytes) unless the last chunk of data is being passed in. In that case, this value doesn't need to a block size multiple. Max length supported may be limited depending on the return behavior.
The documentation for this struct was generated from the following file: