![]() |
![]() |
AESCBCLPF3 Object. More...
#include <AESCBCLPF3.h>

Data Fields | |
| AESCommonLPF3_Object | common |
| volatile uint32_t | iv [AES_IV_LENGTH_BYTES/4] |
| AESCBC_CallbackFxn | callbackFxn |
| AESCBC_OperationUnion * | operation |
| AESCBC_OperationType | operationType |
| bool | threadSafe |
AESCBCLPF3 Object.
The application must not access any member variables of this structure!
| AESCommonLPF3_Object AESCBCLPF3_Object::common |
| volatile uint32_t AESCBCLPF3_Object::iv[AES_IV_LENGTH_BYTES/4] |
| AESCBC_CallbackFxn AESCBCLPF3_Object::callbackFxn |
| AESCBC_OperationUnion* AESCBCLPF3_Object::operation |
| AESCBC_OperationType AESCBCLPF3_Object::operationType |
| bool AESCBCLPF3_Object::threadSafe |