File List
Here is a list of all files with brief descriptions:
 ADC.hAnalog to Digital Conversion (ADC) Input Driver
 ADCLPF3.hADC driver implementation for the ADC peripheral on Low Power F3 devices
 AESCBC.hAESCBC driver header
 AESCBCLPF3.hAESCBC driver implementation for the Low Power F3 devices
 AESCCM.hAESCCM driver header
 AESCCMLPF3.hAESCCM driver implementation for the Low Power F3 family
 AESCMAC.hAESCMAC (CMAC and CBC-MAC) driver header
 AESCMACLPF3.hAESCMAC (CMAC & CBC-MAC) driver implementation for the Low Power F3 family
 AESCommon.hAES common module header for all devices
 AESCommonLPF3.hAESCommon driver implementation for the Low Power F3 family
 AESCTR.hAESCTR driver header
 AESCTRDRBG.hAESCTRDRBG driver header
 AESCTRDRBGXX.hGeneric AESCTRDRBG implementation based on the AESCTR driver
 AESCTRLPF3.hAESCTR driver implementation for the Low Power F3 family
 AESECB.hAESECB driver header
 AESECBLPF3.hAESECB driver implementation for the Low Power F3 family
 AESGCM.hAESGCM driver header
 AESGCMLPF3.hAESGCM driver implementation for the Low Power F3 family
 AnsiColor.h
 ANSIX936KDF.hANSIX936KDF driver header
 ANSIX936KDFXX.hANSI-X9.63 Key Derivation Function driver implementation for the CC13X1/CC26X1, CC13X2/CC26X2, CC13X4/CC26X4, and CC23X0 families
 BatMonSupportLPF3.hBatMon Support layer
 BatteryMonitor.hBattery Monitor driver
 BatteryMonitorLPF3.hBattery Monitor driver implementation for the LPF3 family
 BigNum.hBigNum module provides APIs for performing big number operations
 Board.hPortable board-specific symbols
 Button.hButton driver
 CAN.hController Area Network (CAN) Driver Interface
 CANMCAN.hCommon CAN functions for MCAN configuration
 ClockP.hClock interface for the RTOS Porting Interface
 ClockPLPF3.h
 Comparator.hComparator Driver
 ComparatorLPF3LP.h
 CryptoKey.hThe CryptoKey type is an opaque representation of a cryptographic key
 CryptoKeyKeyStore_PSA.hCryptoKeyKeyStore_PSA driver header
 CryptoKeyKeyStore_PSA_helpers.hCryptoKeyKeyStore driver header
 CryptoKeyKeyStore_PSA_init.h
 CryptoKeyKeyStore_PSA_s.hSecure Crypto Service
 CryptoKeyPlaintext.h
 CryptoResourceLPF3.hShared resources to arbitrate access to the AES engine
 CryptoUtils.hA collection of utility functions for cryptographic purposes
 DebugP.hDebug support
 Display.hGeneric interface for text output
 DisplayExt.hExtention of Display to access GrLib functionality in capable displays
 DisplayHost.hDisplay driver for printf-like output
 DisplaySharp.h
 DisplayUart2.hDisplay.h implementation for UART output
 Driver_Init.h
 ECCInitLPF3SW.h
 ECCParams.h
 ECDH.hTI Driver for Elliptic Curve Diffie-Hellman key agreement scheme
 ECDHLPF3SW.hECDH software driver implementation for the Low Power F3 family
 ECDSA.hTI Driver for Elliptic Curve Digital Signature Algorithm
 ECDSALPF3SW.hECDSA software driver implementation for the Low Power F3 family
 ECIES.hECIES driver header
 ECIESXX.hElliptic Curve Integrated Encryption Scheme (ECIES) driver implementation
 EventP.hEvent Group support
 GPIO.hGeneral Purpose I/O driver interface
 GPIOLPF3.hGPIO driver implementation for Low Power F3 devices
 HwiP.hHardware Interrupt module for the RTOS Porting Interface
 I2C.hInter-Integrated Circuit (I2C) Driver
 I2CLPF3.hI2C driver implementation for a Low Power F3 device I2C controller
 I2CSupport.hHolder of common helper functions for the I2C driver
 ITM.hITM driver header
 LED.hLED driver
 LGPTimerLPF3.hLGPTimer driver implementation for Low Power F3 devices
 List.hLinked List interface for use in drivers
 LogSinkBuf.h
 LogSinkITM.hPRELIMINARY LogSinkITM interface
 Math.hMath utility functions
 MCAN.hHardware abstraction layer for M_CAN Controller v3.2.1
 MCAN_reg.hM_CAN controller v3.2.1 register definitions
 MutexP.hMutex module for the RTOS Porting Interface
 NoRTOS.hNoRTOS framework module
 NVS.hNon-Volatile Storage driver interface
 NVSLPF3.hNon-Volatile Storage driver for Low Power F3 devices
 NVSRAM.hRAM implementation of the NVS driver
 NVSSPI25X.hNon-Volatile Storage driver implementation for SPI flash peripherals
 Power.hPower Manager
 PowerCC23X0.hPower manager interface for CC23X0 devices
 PowerCC27XX.hPower manager interface for CC27XX
 PWM.hPulse Width Modulation (PWM) driver
 PWMTimerLPF3.hPWM driver implementation for Low Power F3 devices
 QueueP.h
 Random.hInterface to generate pseudo-random numbers
 RingBuf.h
 RNG.hRNG driver header
 RNGLPF3RF.hRNG driver implementation for the CC23X0 family
 SD.hSecure Digital (SD) Driver
 SDFatFS.hFile Allocation Table File System (FATFS) Driver
 SDSPI.hSD driver implementation built on the TI SPI driver
 SemaphoreP.hSemaphore module for the RTOS Porting Interface
 SHA2.hSHA2 driver header
 SHA2LPF3SW.hSHA2 software driver implementation for the Low Power F3 family
 SharpGrLib.h
 SPI.hSerial Peripheral Interface (SPI) Driver Interface
 spiffs.h
 SPIFFSNVS.hModule to enable the SPI Flash File System (SPIFFS) on the TI NVS driver
 SPILPF3DMA.hSPI driver implementation for a Low Power F3 device SPI controller using the UDMA controller
 StructRingBuf.h
 SwiP.hSoftware Interrupt module for the RTOS Porting Interface
 SystemP.hSystem module for the RTOS Porting Interface
 TaskP.hTask module for the RTOS Porting Interface
 TCAN455X.hTCAN455X Driver Interface
 TCAN455X_reg.hTCAN455X device-specific register definitions
 Temperature.hTemperature driver
 TemperatureLPF3.hTemperature driver implementation for the Low Power F3 family
 TimestampP.hTimestamp module for the RTOS Porting Interface
 types.h
 UART2.hPRELIMINARY UART driver interface
 UART2LPF3.hUART driver implementation for a Low Power F3 device UART controller
 UART2Support.hHolder of common helper functions for the UART driver
 UDMALPF3.hUDMALPF3 driver implementation
 unistd.h
 Watchdog.hWatchdog driver interface
 WatchdogLPF3.hWatchdog driver implementation for Low Power F3 devices
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale