#include <hw_fcfg.h>
§ trim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::trim |
§ zero [1/2]
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::zero |
§ pa0
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::pa0 |
§ zero0
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::zero0 |
§ irefTrim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::irefTrim |
§ zero1
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::zero1 |
§ atstRefH
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::atstRefH |
§ lna
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::lna |
§ ifampRfLdo
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifampRfLdo |
§ voutTrim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::voutTrim |
§ divLdo
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::divLdo |
§ tdcLdo
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::tdcLdo |
§ firstTrim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::firstTrim |
§ secondTrim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::secondTrim |
§ dcoLdo0
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::dcoLdo0 |
§ trimout
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::trimout |
§ ifadcAldo
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadcAldo |
§ ifadcDldo
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadcDldo |
§ tailresTrim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::tailresTrim |
§ dco
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::dco |
§ quantThr
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::quantThr |
§ ifadcQuant
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadcQuant |
§ aafcap [1/2]
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::aafcap |
§ int2Adj
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::int2Adj |
§ ditheren
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::ditheren |
§ dithertrim
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::dithertrim |
§ zero2
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::zero2 |
§ ifadc0
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadc0 |
§ ifadc1
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadc1 |
§ int3
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::int3 |
§ ff1
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::ff1 |
§ ff2
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::ff2 |
§ ff3
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::ff3 |
§ ifadclf
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadclf |
§ ifadcQuantWbw
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadcQuantWbw |
§ ifadc0Wbw
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadc0Wbw |
§ ifadc1Wbw
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadc1Wbw |
§ ifadclfWbw
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifadclfWbw |
§ rtrimMinOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::rtrimMinOffset |
§ rtrimMaxOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::rtrimMaxOffset |
§ divLdoMinOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::divLdoMinOffset |
§ divLdoMaxOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::divLdoMaxOffset |
§ tdcLdoMinOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::tdcLdoMinOffset |
§ tdcLdoMaxOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::tdcLdoMaxOffset |
§ tThrl
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::tThrl |
§ tThrh
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::tThrh |
§ hfxtPdError
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::hfxtPdError |
§ res
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::res |
§ lrfdrfeExtTrim1
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::lrfdrfeExtTrim1 |
§ rssiTcomp
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::rssiTcomp |
§ magnTcomp
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::magnTcomp |
§ magnOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::magnOffset |
§ rfu
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::rfu |
§ agcThrTcomp
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::agcThrTcomp |
§ agcThrOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::agcThrOffset |
§ lowGainOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::lowGainOffset |
§ highGainOffset
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::highGainOffset |
§ lrfdrfeExtTrim0
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::lrfdrfeExtTrim0 |
§ offset
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::offset |
§ trimCompleteN
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::trimCompleteN |
§ fend0Rssi
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::fend0Rssi |
§ iqmc
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::iqmc |
§ syntDiv0
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::syntDiv0 |
§ res1
| uint8_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::res1[2] |
§ zero [2/2]
| uint8_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::zero |
§ aafcap [2/2]
| uint8_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::aafcap |
§ ifamprfldo
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifamprfldo |
§ ifamprfldoWbw
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::ifamprfldoWbw |
§ auxDiodeGnd
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::auxDiodeGnd |
§ auxDiodeVoltage
| uint16_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::auxDiodeVoltage |
§ auxDiodeCal30C
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::auxDiodeCal30C |
§ auxDiodeCal125C
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::auxDiodeCal125C |
§ res2
| uint8_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::res2[20] |
§ adcOffsetVdds
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcOffsetVdds |
§ adcOffsetExtref
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcOffsetExtref |
§ adcOffsetIntref2P5V
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcOffsetIntref2P5V |
§ adcOffsetIntref1P4V
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcOffsetIntref1P4V |
§ adcOffset
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcOffset |
§ adcGainVdds
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcGainVdds |
§ adcGainExtref
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcGainExtref |
§ adcGainWord0
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcGainWord0 |
§ adcGainIntref2P5V
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcGainIntref2P5V |
§ adcGainIntref1P4V
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcGainIntref1P4V |
§ adcGainWord1
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::adcGainWord1 |
§ res3
| uint8_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::res3[28] |
§ i2v20k
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::i2v20k |
§ i2v50k
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::i2v50k |
§ i2v100k
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::i2v100k |
§ i2v1m
| uint32_t fcfg_t::appTrims_struct::appTrimsCc23x0_s::i2v1m |
§ i2vCompact
| struct { ... } fcfg_t::appTrims_struct::appTrimsCc23x0_s::i2vCompact |
The documentation for this struct was generated from the following file: