CC23x0R5DriverLibrary
fcfg_t::appTrims_struct Struct Reference

#include <hw_fcfg.h>

Collaboration diagram for fcfg_t::appTrims_struct:

Data Structures

struct  appTrimsCc23x0_s
 

Data Fields

uint8_t revision
 
uint8_t nToolsClientOffset
 
uint8_t res [2]
 
struct fcfg_t::appTrims_struct::appTrimsCc23x0_s cc23x0r5
 

Field Documentation

§ revision

uint8_t fcfg_t::appTrims_struct::revision

§ nToolsClientOffset

uint8_t fcfg_t::appTrims_struct::nToolsClientOffset

§ res

uint8_t fcfg_t::appTrims_struct::res[2]

§ cc23x0r5

struct fcfg_t::appTrims_struct::appTrimsCc23x0_s fcfg_t::appTrims_struct::cc23x0r5

The documentation for this struct was generated from the following file: