59 #include "../inc/hw_lrfddbell.h" 62 #define LRFD_NUM_CLK_DEP 2 63 #define LRFD_CLK_DEP_POWER 0 65 #define LRFD_CLK_DEP_RCL 1 void LRFDApplyClockDependencies(void)
Apply the currently set clock dependencies.
Definition: lrfd.c:82
void LRFDReleaseClockDependency(uint16_t mask, uint8_t dependencySetId)
Release clock dependency on a set of modules in LRFD.
Definition: lrfd.c:68
void LRFDSetClockDependency(uint16_t mask, uint8_t dependencySetId)
Set clock dependency on a set of modules in LRFD.
Definition: lrfd.c:54