CC23x0R5DriverLibrary
lrfd.c File Reference
#include "lrfd.h"
#include <stdbool.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_clkctl.h"
#include "../inc/hw_lrfddbell.h"
#include "../driverlib/interrupt.h"
Include dependency graph for lrfd.c:

Functions

void LRFDSetClockDependency (uint16_t mask, uint8_t dependencySetId)
 Set clock dependency on a set of modules in LRFD. More...
 
void LRFDReleaseClockDependency (uint16_t mask, uint8_t dependencySetId)
 Release clock dependency on a set of modules in LRFD. More...
 
void LRFDApplyClockDependencies (void)
 Apply the currently set clock dependencies. More...
 

Variables

static uint16_t lrfdClockDependencySets [LRFD_NUM_CLK_DEP]
 
static bool lrfdClocked = false
 

Variable Documentation

§ lrfdClockDependencySets

uint16_t lrfdClockDependencySets[LRFD_NUM_CLK_DEP]
static

§ lrfdClocked

bool lrfdClocked = false
static