CC23x0R5DriverLibrary
hw_uart.h
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: hw_uart_h
3 ******************************************************************************
4 * Copyright (c) 2021 Texas Instruments Incorporated. All rights reserved.
5 *
6 * Redistribution and use in source and binary forms, with or without
7 * modification, are permitted provided that the following conditions are met:
8 *
9 * 1) Redistributions of source code must retain the above copyright notice,
10 * this list of conditions and the following disclaimer.
11 *
12 * 2) Redistributions in binary form must reproduce the above copyright notice,
13 * this list of conditions and the following disclaimer in the documentation
14 * and/or other materials provided with the distribution.
15 *
16 * 3) Neither the name of the copyright holder nor the names of its contributors
17 * may be used to endorse or promote products derived from this software
18 * without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
22 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
23 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
24 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
25 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
26 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
27 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
28 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
29 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
30 * POSSIBILITY OF SUCH DAMAGE.
31 ******************************************************************************/
32 
33 #ifndef __HW_UART_H__
34 #define __HW_UART_H__
35 
36 //*****************************************************************************
37 //
38 // This section defines the register offsets of
39 // UART component
40 //
41 //*****************************************************************************
42 // Data
43 #define UART_O_DR 0x00000000U
44 
45 // Status
46 #define UART_O_RSR_ECR 0x00000004U
47 
48 // Flag
49 #define UART_O_FR 0x00000018U
50 
51 // IrDA Low-Power Counter Register
52 #define UART_O_UARTILPR 0x00000020U
53 
54 // Integer Baud-Rate Divisor
55 #define UART_O_IBRD 0x00000024U
56 
57 // Fractional Baud-Rate Divisor
58 #define UART_O_FBRD 0x00000028U
59 
60 // Line Control
61 #define UART_O_LCRH 0x0000002CU
62 
63 // Control
64 #define UART_O_CTL 0x00000030U
65 
66 // Interrupt FIFO Level Select
67 #define UART_O_IFLS 0x00000034U
68 
69 // Interrupt Mask Set/Clear
70 #define UART_O_IMSC 0x00000038U
71 
72 // Raw Interrupt Status
73 #define UART_O_RIS 0x0000003CU
74 
75 // Masked Interrupt Status
76 #define UART_O_MIS 0x00000040U
77 
78 // Interrupt Clear
79 #define UART_O_ICR 0x00000044U
80 
81 // DMA Control
82 #define UART_O_DMACTL 0x00000048U
83 
84 //*****************************************************************************
85 //
86 // Register: UART_O_DR
87 //
88 //*****************************************************************************
89 // Field: [11] OE
90 //
91 // UART Overrun Error:
92 // This bit is set to 1 if data is received and the receive FIFO is already
93 // full. The FIFO contents remain valid because no more data is written when
94 // the FIFO is full, only the contents of the shift register are overwritten.
95 // This is cleared to 0 once there is an empty space in the FIFO and a new
96 // character can be written to it.
97 #define UART_DR_OE 0x00000800U
98 #define UART_DR_OE_M 0x00000800U
99 #define UART_DR_OE_S 11U
100 
101 // Field: [10] BE
102 //
103 // UART Break Error:
104 // This bit is set to 1 if a break condition was detected, indicating that the
105 // received data input (UARTRXD input pin) was held LOW for longer than a
106 // full-word transmission time (defined as start, data, parity and stop bits).
107 // In FIFO mode, this error is associated with the character at the top of the
108 // FIFO (i.e., the oldest received data character since last read). When a
109 // break occurs, a 0 character is loaded into the FIFO. The next character is
110 // enabled after the receive data input (UARTRXD input pin) goes to a 1
111 // (marking state), and the next valid start bit is received.
112 #define UART_DR_BE 0x00000400U
113 #define UART_DR_BE_M 0x00000400U
114 #define UART_DR_BE_S 10U
115 
116 // Field: [9] PE
117 //
118 // UART Parity Error:
119 // When set to 1, it indicates that the parity of the received data character
120 // does not match the parity that the LCRH.EPS and LCRH.SPS select.
121 // In FIFO mode, this error is associated with the character at the top of the
122 // FIFO (i.e., the oldest received data character since last read).
123 #define UART_DR_PE 0x00000200U
124 #define UART_DR_PE_M 0x00000200U
125 #define UART_DR_PE_S 9U
126 
127 // Field: [8] FE
128 //
129 // UART Framing Error:
130 // When set to 1, it indicates that the received character did not have a valid
131 // stop bit (a valid stop bit is 1).
132 // In FIFO mode, this error is associated with the character at the top of the
133 // FIFO (i.e., the oldest received data character since last read).
134 #define UART_DR_FE 0x00000100U
135 #define UART_DR_FE_M 0x00000100U
136 #define UART_DR_FE_S 8U
137 
138 // Field: [7:0] DATA
139 //
140 // Data transmitted or received:
141 // On writes, the transmit data character is pushed into the FIFO.
142 // On reads, the oldest received data character since the last read is
143 // returned.
144 #define UART_DR_DATA_W 8U
145 #define UART_DR_DATA_M 0x000000FFU
146 #define UART_DR_DATA_S 0U
147 
148 //*****************************************************************************
149 //
150 // Register: UART_O_RSR_ECR
151 //
152 //*****************************************************************************
153 // Field: [3] OE
154 //
155 // UART Overrun Error:
156 // This bit is set to 1 if data is received and the receive FIFO is already
157 // full. The FIFO contents remain valid because no more data is written when
158 // the FIFO is full, only the contents of the shift register are overwritten.
159 // This is cleared to 0 once there is an empty space in the FIFO and a new
160 // character can be written to it.
161 // ENUMs:
162 // CLEAR_ERROR_1 Clears error flag if error is set. Write value is
163 // not important.
164 // ERROR_NOTSET Error flag is not set
165 #define UART_RSR_ECR_OE 0x00000008U
166 #define UART_RSR_ECR_OE_M 0x00000008U
167 #define UART_RSR_ECR_OE_S 3U
168 #define UART_RSR_ECR_OE_CLEAR_ERROR_1 0x00000008U
169 #define UART_RSR_ECR_OE_ERROR_NOTSET 0x00000000U
170 
171 // Field: [2] BE
172 //
173 // UART Break Error:
174 // This bit is set to 1 if a break condition was detected, indicating that the
175 // received data input (UARTRXD input pin) was held LOW for longer than a
176 // full-word transmission time (defined as start, data, parity and stop bits).
177 // When a break occurs, a 0 character is loaded into the FIFO. The next
178 // character is enabled after the receive data input (UARTRXD input pin) goes
179 // to a 1 (marking state), and the next valid start bit is received.
180 // ENUMs:
181 // CLEAR_ERROR_1 Clears error flag if error is set. Write value is
182 // not important.
183 // ERROR_NOTSET Error flag is not set
184 #define UART_RSR_ECR_BE 0x00000004U
185 #define UART_RSR_ECR_BE_M 0x00000004U
186 #define UART_RSR_ECR_BE_S 2U
187 #define UART_RSR_ECR_BE_CLEAR_ERROR_1 0x00000004U
188 #define UART_RSR_ECR_BE_ERROR_NOTSET 0x00000000U
189 
190 // Field: [1] PE
191 //
192 // UART Parity Error:
193 // When set to 1, it indicates that the parity of the received data character
194 // does not match the parity that the LCRH.EPS and LCRH.SPS select.
195 // ENUMs:
196 // CLEAR_ERROR_1 Clears error flag if error is set. Write value is
197 // not important.
198 // ERROR_NOTSET Error flag is not set
199 #define UART_RSR_ECR_PE 0x00000002U
200 #define UART_RSR_ECR_PE_M 0x00000002U
201 #define UART_RSR_ECR_PE_S 1U
202 #define UART_RSR_ECR_PE_CLEAR_ERROR_1 0x00000002U
203 #define UART_RSR_ECR_PE_ERROR_NOTSET 0x00000000U
204 
205 // Field: [0] FE
206 //
207 // UART Framing Error:
208 // When set to 1, it indicates that the received character did not have a valid
209 // stop bit (a valid stop bit is 1).
210 // ENUMs:
211 // CLEAR_ERROR_1 Clears error flag if error is set. Write value is
212 // not important.
213 // ERROR_NOTSET Error flag is not set
214 #define UART_RSR_ECR_FE 0x00000001U
215 #define UART_RSR_ECR_FE_M 0x00000001U
216 #define UART_RSR_ECR_FE_S 0U
217 #define UART_RSR_ECR_FE_CLEAR_ERROR_1 0x00000001U
218 #define UART_RSR_ECR_FE_ERROR_NOTSET 0x00000000U
219 
220 //*****************************************************************************
221 //
222 // Register: UART_O_FR
223 //
224 //*****************************************************************************
225 // Field: [7] TXFE
226 //
227 // UART Transmit FIFO Empty:
228 // The meaning of this bit depends on the state of LCRH.FEN .
229 // - If the FIFO is disabled, this bit is set when the transmit holding
230 // register is empty.
231 // - If the FIFO is enabled, this bit is set when the transmit FIFO is empty.
232 // This bit does not indicate if there is data in the transmit shift register.
233 #define UART_FR_TXFE 0x00000080U
234 #define UART_FR_TXFE_M 0x00000080U
235 #define UART_FR_TXFE_S 7U
236 
237 // Field: [6] RXFF
238 //
239 // UART Receive FIFO Full:
240 // The meaning of this bit depends on the state of LCRH.FEN.
241 // - If the FIFO is disabled, this bit is set when the receive holding
242 // register is full.
243 // - If the FIFO is enabled, this bit is set when the receive FIFO is full.
244 #define UART_FR_RXFF 0x00000040U
245 #define UART_FR_RXFF_M 0x00000040U
246 #define UART_FR_RXFF_S 6U
247 
248 // Field: [5] TXFF
249 //
250 // UART Transmit FIFO Full:
251 // Transmit FIFO full. The meaning of this bit depends on the state of
252 // LCRH.FEN.
253 // - If the FIFO is disabled, this bit is set when the transmit holding
254 // register is full.
255 // - If the FIFO is enabled, this bit is set when the transmit FIFO is full.
256 #define UART_FR_TXFF 0x00000020U
257 #define UART_FR_TXFF_M 0x00000020U
258 #define UART_FR_TXFF_S 5U
259 
260 // Field: [4] RXFE
261 //
262 // UART Receive FIFO Empty:
263 // Receive FIFO empty. The meaning of this bit depends on the state of
264 // LCRH.FEN.
265 // - If the FIFO is disabled, this bit is set when the receive holding
266 // register is empty.
267 // - If the FIFO is enabled, this bit is set when the receive FIFO is empty.
268 #define UART_FR_RXFE 0x00000010U
269 #define UART_FR_RXFE_M 0x00000010U
270 #define UART_FR_RXFE_S 4U
271 
272 // Field: [3] BUSY
273 //
274 // UART Busy:
275 // If this bit is set to 1, the UART is busy transmitting data. This bit
276 // remains set until the complete byte, including all the stop bits, has been
277 // sent from the shift register.
278 // This bit is set as soon as the transmit FIFO becomes non-empty, regardless
279 // of whether the UART is enabled or not.
280 #define UART_FR_BUSY 0x00000008U
281 #define UART_FR_BUSY_M 0x00000008U
282 #define UART_FR_BUSY_S 3U
283 
284 // Field: [0] CTS
285 //
286 // Clear To Send:
287 // This bit is the complement of the active-low UART CTS input pin.
288 // That is, the bit is 1 when CTS input pin is LOW.
289 #define UART_FR_CTS 0x00000001U
290 #define UART_FR_CTS_M 0x00000001U
291 #define UART_FR_CTS_S 0U
292 
293 //*****************************************************************************
294 //
295 // Register: UART_O_UARTILPR
296 //
297 //*****************************************************************************
298 // Field: [7:0] ILPDVSR
299 //
300 // 8 bit low-power divisor value. In low-power IrDA mode the UART rejects
301 // random noise on the received serial data
302 // input by ignoring SIRIN pulses that are less than 3 periods of IrLPBaud16.
303 #define UART_UARTILPR_ILPDVSR_W 8U
304 #define UART_UARTILPR_ILPDVSR_M 0x000000FFU
305 #define UART_UARTILPR_ILPDVSR_S 0U
306 
307 //*****************************************************************************
308 //
309 // Register: UART_O_IBRD
310 //
311 //*****************************************************************************
312 // Field: [15:0] DIVINT
313 //
314 // The integer baud rate divisor:
315 // The baud rate divisor is calculated using the formula below:
316 // Baud rate divisor = (UART reference clock frequency) / (16 * Baud rate)
317 // Baud rate divisor must be minimum 1 and maximum 65535.
318 // That is, DIVINT=0 does not give a valid baud rate.
319 // Similarly, if DIVINT=0xFFFF, any non-zero values in FBRD.DIVFRAC will be
320 // illegal.
321 // Refer to Section 19.1.5 for an example calculation.
322 // A valid value must be written to this field before the UART can be used for
323 // RX or TX operations.
324 #define UART_IBRD_DIVINT_W 16U
325 #define UART_IBRD_DIVINT_M 0x0000FFFFU
326 #define UART_IBRD_DIVINT_S 0U
327 
328 //*****************************************************************************
329 //
330 // Register: UART_O_FBRD
331 //
332 //*****************************************************************************
333 // Field: [5:0] DIVFRAC
334 //
335 // Fractional Baud-Rate Divisor:
336 // The baud rate divisor is calculated using the formula below:
337 // Baud rate divisor = (UART reference clock frequency) / (16 * Baud rate)
338 // Baud rate divisor must be minimum 1 and maximum 65535.
339 // That is, IBRD.DIVINT=0 does not give a valid baud rate.
340 // Similarly, if IBRD.DIVINT=0xFFFF, any non-zero values in DIVFRAC will be
341 // illegal.
342 // Refer to Section 19.1.5 for an example calculation.
343 // A valid value must be written to this field before the UART can be used for
344 // RX or TX operations.
345 #define UART_FBRD_DIVFRAC_W 6U
346 #define UART_FBRD_DIVFRAC_M 0x0000003FU
347 #define UART_FBRD_DIVFRAC_S 0U
348 
349 //*****************************************************************************
350 //
351 // Register: UART_O_LCRH
352 //
353 //*****************************************************************************
354 // Field: [7] SPS
355 //
356 // UART Stick Parity Select:
357 //
358 // 0: Stick parity is disabled
359 // 1: The parity bit is transmitted and checked as invert of EPS field (i.e.
360 // the parity bit is transmitted and checked as 1 when EPS = 0).
361 //
362 // This bit has no effect when PEN disables parity checking and generation.
363 #define UART_LCRH_SPS 0x00000080U
364 #define UART_LCRH_SPS_M 0x00000080U
365 #define UART_LCRH_SPS_S 7U
366 
367 // Field: [6:5] WLEN
368 //
369 // UART Word Length:
370 // These bits indicate the number of data bits transmitted or received in a
371 // frame.
372 // ENUMs:
373 // BITL8 Word Length 8 bits
374 // BITL7 Word Length 7 bits
375 // BITL6 Word Length 6 bits
376 // BITL5 Word Length 5 bits
377 #define UART_LCRH_WLEN_W 2U
378 #define UART_LCRH_WLEN_M 0x00000060U
379 #define UART_LCRH_WLEN_S 5U
380 #define UART_LCRH_WLEN_BITL8 0x00000060U
381 #define UART_LCRH_WLEN_BITL7 0x00000040U
382 #define UART_LCRH_WLEN_BITL6 0x00000020U
383 #define UART_LCRH_WLEN_BITL5 0x00000000U
384 
385 // Field: [4] FEN
386 //
387 // UART Enable FIFOs
388 // ENUMs:
389 // EN Transmit and receive FIFO buffers are enabled
390 // (FIFO mode)
391 // DIS FIFOs are disabled (character mode) that is, the
392 // FIFOs become 1-byte-deep holding registers.
393 #define UART_LCRH_FEN 0x00000010U
394 #define UART_LCRH_FEN_M 0x00000010U
395 #define UART_LCRH_FEN_S 4U
396 #define UART_LCRH_FEN_EN 0x00000010U
397 #define UART_LCRH_FEN_DIS 0x00000000U
398 
399 // Field: [3] STP2
400 //
401 // UART Two Stop Bits Select:
402 // If this bit is set to 1, two stop bits are transmitted at the end of the
403 // frame. The receive logic does not check for two stop bits being received.
404 #define UART_LCRH_STP2 0x00000008U
405 #define UART_LCRH_STP2_M 0x00000008U
406 #define UART_LCRH_STP2_S 3U
407 
408 // Field: [2] EPS
409 //
410 // UART Even Parity Select
411 // ENUMs:
412 // EVEN Even parity: The UART generates or checks for an
413 // even number of 1s in the data and parity bits.
414 // ODD Odd parity: The UART generates or checks for an
415 // odd number of 1s in the data and parity bits.
416 #define UART_LCRH_EPS 0x00000004U
417 #define UART_LCRH_EPS_M 0x00000004U
418 #define UART_LCRH_EPS_S 2U
419 #define UART_LCRH_EPS_EVEN 0x00000004U
420 #define UART_LCRH_EPS_ODD 0x00000000U
421 
422 // Field: [1] PEN
423 //
424 // UART Parity Enable
425 // This bit controls generation and checking of parity bit.
426 // ENUMs:
427 // EN Parity checking and generation is enabled.
428 // DIS Parity is disabled and no parity bit is added to
429 // the data frame
430 #define UART_LCRH_PEN 0x00000002U
431 #define UART_LCRH_PEN_M 0x00000002U
432 #define UART_LCRH_PEN_S 1U
433 #define UART_LCRH_PEN_EN 0x00000002U
434 #define UART_LCRH_PEN_DIS 0x00000000U
435 
436 // Field: [0] BRK
437 //
438 // UART Send Break
439 // If this bit is set to 1, a low-level is continually output on the UARTTXD
440 // output pin, after completing transmission of the current character. For the
441 // proper execution of the break command, the
442 // software must set this bit for at least two complete frames. For normal use,
443 // this bit must be cleared to 0.
444 #define UART_LCRH_BRK 0x00000001U
445 #define UART_LCRH_BRK_M 0x00000001U
446 #define UART_LCRH_BRK_S 0U
447 
448 //*****************************************************************************
449 //
450 // Register: UART_O_CTL
451 //
452 //*****************************************************************************
453 // Field: [15] CTSEN
454 //
455 // CTS hardware flow control enable
456 // ENUMs:
457 // EN CTS hardware flow control enabled
458 // DIS CTS hardware flow control disabled
459 #define UART_CTL_CTSEN 0x00008000U
460 #define UART_CTL_CTSEN_M 0x00008000U
461 #define UART_CTL_CTSEN_S 15U
462 #define UART_CTL_CTSEN_EN 0x00008000U
463 #define UART_CTL_CTSEN_DIS 0x00000000U
464 
465 // Field: [14] RTSEN
466 //
467 // RTS hardware flow control enable
468 // ENUMs:
469 // EN RTS hardware flow control enabled
470 // DIS RTS hardware flow control disabled
471 #define UART_CTL_RTSEN 0x00004000U
472 #define UART_CTL_RTSEN_M 0x00004000U
473 #define UART_CTL_RTSEN_S 14U
474 #define UART_CTL_RTSEN_EN 0x00004000U
475 #define UART_CTL_RTSEN_DIS 0x00000000U
476 
477 // Field: [11] RTS
478 //
479 // Request to Send
480 // This bit is the complement of the active-low UART RTS output. That is, when
481 // the bit is programmed to a 1 then RTS output on the pins is LOW.
482 #define UART_CTL_RTS 0x00000800U
483 #define UART_CTL_RTS_M 0x00000800U
484 #define UART_CTL_RTS_S 11U
485 
486 // Field: [9] RXE
487 //
488 // UART Receive Enable
489 // If the UART is disabled in the middle of reception, it completes the current
490 // character before stopping.
491 // ENUMs:
492 // EN UART Receive enabled
493 // DIS UART Receive disabled
494 #define UART_CTL_RXE 0x00000200U
495 #define UART_CTL_RXE_M 0x00000200U
496 #define UART_CTL_RXE_S 9U
497 #define UART_CTL_RXE_EN 0x00000200U
498 #define UART_CTL_RXE_DIS 0x00000000U
499 
500 // Field: [8] TXE
501 //
502 // UART Transmit Enable
503 // If the UART is disabled in the middle of transmission, it completes the
504 // current character before stopping.
505 // ENUMs:
506 // EN UART Transmit enabled
507 // DIS UART Transmit disabled
508 #define UART_CTL_TXE 0x00000100U
509 #define UART_CTL_TXE_M 0x00000100U
510 #define UART_CTL_TXE_S 8U
511 #define UART_CTL_TXE_EN 0x00000100U
512 #define UART_CTL_TXE_DIS 0x00000000U
513 
514 // Field: [7] LBE
515 //
516 // UART Loop Back Enable
517 // Enabling the loop-back mode connects the UARTTXD output from the UART to
518 // UARTRXD input of the UART.
519 // ENUMs:
520 // EN Loop Back enabled
521 // DIS Loop Back disabled
522 #define UART_CTL_LBE 0x00000080U
523 #define UART_CTL_LBE_M 0x00000080U
524 #define UART_CTL_LBE_S 7U
525 #define UART_CTL_LBE_EN 0x00000080U
526 #define UART_CTL_LBE_DIS 0x00000000U
527 
528 // Field: [6] FCEN
529 //
530 // UART FIFO Concatenation Enable
531 // Enabling the FIFO concatenation in TX mode resulting in 16 TX buffers.
532 // ENUMs:
533 // EN UART FIFO Concatenation enabled
534 // DIS UART FIFO Concatenation disabled
535 #define UART_CTL_FCEN 0x00000040U
536 #define UART_CTL_FCEN_M 0x00000040U
537 #define UART_CTL_FCEN_S 6U
538 #define UART_CTL_FCEN_EN 0x00000040U
539 #define UART_CTL_FCEN_DIS 0x00000000U
540 
541 // Field: [2] SIRLP
542 //
543 // SIR low power IrDA mode
544 // This bit selects the IrDA encoding mode
545 // ENUMs:
546 // EN Low-level bits are transmitted with a pulse width
547 // of 3 times the period of IrLPBaud16(which has a
548 // frequency of (UARTCLK
549 // frequency)/UARTILP.ILPDVSR), regardless of the
550 // selected bit rate.
551 // In low-power IrDA mode
552 // the UART rejects random noise on the received
553 // serial data
554 // input by ignoring SIRIN
555 // pulses that are less than 3 periods of
556 // IrLPBaud16.
557 // DIS Low-level bits are transmitted as active high with
558 // a 3/16th period width,
559 #define UART_CTL_SIRLP 0x00000004U
560 #define UART_CTL_SIRLP_M 0x00000004U
561 #define UART_CTL_SIRLP_S 2U
562 #define UART_CTL_SIRLP_EN 0x00000004U
563 #define UART_CTL_SIRLP_DIS 0x00000000U
564 
565 // Field: [1] SIREN
566 //
567 // SIR Enable
568 // This bit has no effect if UARTEN bit disables the UART.
569 // ENUMs:
570 // EN IrDA SIR ENDEC is enabled. Data is transmitted and
571 // received via nSIROUT and SIRIN.
572 // DIS IrDA SIR ENDEC is disabled
573 #define UART_CTL_SIREN 0x00000002U
574 #define UART_CTL_SIREN_M 0x00000002U
575 #define UART_CTL_SIREN_S 1U
576 #define UART_CTL_SIREN_EN 0x00000002U
577 #define UART_CTL_SIREN_DIS 0x00000000U
578 
579 // Field: [0] UARTEN
580 //
581 // UART Enable
582 // ENUMs:
583 // EN UART enabled
584 // DIS UART disabled
585 #define UART_CTL_UARTEN 0x00000001U
586 #define UART_CTL_UARTEN_M 0x00000001U
587 #define UART_CTL_UARTEN_S 0U
588 #define UART_CTL_UARTEN_EN 0x00000001U
589 #define UART_CTL_UARTEN_DIS 0x00000000U
590 
591 //*****************************************************************************
592 //
593 // Register: UART_O_IFLS
594 //
595 //*****************************************************************************
596 // Field: [5:3] RXSEL
597 //
598 // Receive interrupt FIFO level select:
599 // This field sets the trigger points for the receive interrupt. Values
600 // 0b101-0b111 are reserved.
601 // ENUMs:
602 // THREEQU Receive FIFO becomes >= 3/4 full
603 // HALF Receive FIFO becomes >= 1/2 full
604 // QUARTER Receive FIFO becomes >= 1/4 full
605 #define UART_IFLS_RXSEL_W 3U
606 #define UART_IFLS_RXSEL_M 0x00000038U
607 #define UART_IFLS_RXSEL_S 3U
608 #define UART_IFLS_RXSEL_THREEQU 0x00000018U
609 #define UART_IFLS_RXSEL_HALF 0x00000010U
610 #define UART_IFLS_RXSEL_QUARTER 0x00000008U
611 
612 // Field: [2:0] TXSEL
613 //
614 // Transmit interrupt FIFO level select:
615 // This field sets the trigger points for the transmit interrupt. Values
616 // 0b101-0b111 are reserved.
617 // ENUMs:
618 // THREEQU Transmit FIFO becomes <= 3/4 full
619 // HALF Transmit FIFO becomes <= 1/2 full
620 // QUARTER Transmit FIFO becomes <= 1/4 full
621 #define UART_IFLS_TXSEL_W 3U
622 #define UART_IFLS_TXSEL_M 0x00000007U
623 #define UART_IFLS_TXSEL_S 0U
624 #define UART_IFLS_TXSEL_THREEQU 0x00000003U
625 #define UART_IFLS_TXSEL_HALF 0x00000002U
626 #define UART_IFLS_TXSEL_QUARTER 0x00000001U
627 
628 //*****************************************************************************
629 //
630 // Register: UART_O_IMSC
631 //
632 //*****************************************************************************
633 // Field: [13] RXDMADONE
634 //
635 // RX DMA done interrupt mask. A read returns the current mask for UART's
636 // RXDMADONE interrupt. On a write of 1, the mask of the RXDMADONE interrupt is
637 // set which means the interrupt state will be reflected in MIS.RXDMADONE. A
638 // write of 0 clears the mask which means MIS.RXDMADONE will not reflect the
639 // interrupt.
640 #define UART_IMSC_RXDMADONE 0x00002000U
641 #define UART_IMSC_RXDMADONE_M 0x00002000U
642 #define UART_IMSC_RXDMADONE_S 13U
643 
644 // Field: [12] TXDMADONE
645 //
646 // TX DMA done interrupt mask. A read returns the current mask for UART's
647 // TXDMADONE interrupt. On a write of 1, the mask of the TXDMADONE interrupt is
648 // set which means the interrupt state will be reflected in MIS.TXDMADONE. A
649 // write of 0 clears the mask which means MIS.TXDMADONE will not reflect the
650 // interrupt.
651 #define UART_IMSC_TXDMADONE 0x00001000U
652 #define UART_IMSC_TXDMADONE_M 0x00001000U
653 #define UART_IMSC_TXDMADONE_S 12U
654 
655 // Field: [11] EOT
656 //
657 // End of Transmission interrupt mask. A read returns the current mask for
658 // UART's EoT interrupt. On a write of 1, the mask of the EoT interrupt is set
659 // which means the interrupt state will be reflected in MIS.EOT. A write of 0
660 // clears the mask which means MIS.EOT will not reflect the interrupt.
661 #define UART_IMSC_EOT 0x00000800U
662 #define UART_IMSC_EOT_M 0x00000800U
663 #define UART_IMSC_EOT_S 11U
664 
665 // Field: [10] OE
666 //
667 // Overrun error interrupt mask. A read returns the current mask for UART's
668 // overrun error interrupt. On a write of 1, the mask of the overrun error
669 // interrupt is set which means the interrupt state will be reflected in
670 // MIS.OE. A write of 0 clears the mask which means MIS.OE will not reflect the
671 // interrupt.
672 #define UART_IMSC_OE 0x00000400U
673 #define UART_IMSC_OE_M 0x00000400U
674 #define UART_IMSC_OE_S 10U
675 
676 // Field: [9] BE
677 //
678 // Break error interrupt mask. A read returns the current mask for UART's break
679 // error interrupt. On a write of 1, the mask of the overrun error interrupt is
680 // set which means the interrupt state will be reflected in MIS.BE. A write of
681 // 0 clears the mask which means MIS.BE will not reflect the interrupt.
682 #define UART_IMSC_BE 0x00000200U
683 #define UART_IMSC_BE_M 0x00000200U
684 #define UART_IMSC_BE_S 9U
685 
686 // Field: [8] PE
687 //
688 // Parity error interrupt mask. A read returns the current mask for UART's
689 // parity error interrupt. On a write of 1, the mask of the overrun error
690 // interrupt is set which means the interrupt state will be reflected in
691 // MIS.PE. A write of 0 clears the mask which means MIS.PE will not reflect the
692 // interrupt.
693 #define UART_IMSC_PE 0x00000100U
694 #define UART_IMSC_PE_M 0x00000100U
695 #define UART_IMSC_PE_S 8U
696 
697 // Field: [7] FE
698 //
699 // Framing error interrupt mask. A read returns the current mask for UART's
700 // framing error interrupt. On a write of 1, the mask of the overrun error
701 // interrupt is set which means the interrupt state will be reflected in
702 // MIS.FE. A write of 0 clears the mask which means MIS.FE will not reflect the
703 // interrupt.
704 #define UART_IMSC_FE 0x00000080U
705 #define UART_IMSC_FE_M 0x00000080U
706 #define UART_IMSC_FE_S 7U
707 
708 // Field: [6] RT
709 //
710 // Receive timeout interrupt mask. A read returns the current mask for UART's
711 // receive timeout interrupt. On a write of 1, the mask of the overrun error
712 // interrupt is set which means the interrupt state will be reflected in
713 // MIS.RT. A write of 0 clears the mask which means this bitfield will not
714 // reflect the interrupt.
715 // The raw interrupt for receive timeout RIS.RT cannot be set unless the mask
716 // is set (RT = 1). This is because the mask acts as an enable for power
717 // saving. That is, the same status can be read from MIS.RT and RIS.RT.
718 #define UART_IMSC_RT 0x00000040U
719 #define UART_IMSC_RT_M 0x00000040U
720 #define UART_IMSC_RT_S 6U
721 
722 // Field: [5] TX
723 //
724 // Transmit interrupt mask. A read returns the current mask for UART's transmit
725 // interrupt. On a write of 1, the mask of the overrun error interrupt is set
726 // which means the interrupt state will be reflected in MIS.TX. A write of 0
727 // clears the mask which means MIS.TX will not reflect the interrupt.
728 #define UART_IMSC_TX 0x00000020U
729 #define UART_IMSC_TX_M 0x00000020U
730 #define UART_IMSC_TX_S 5U
731 
732 // Field: [4] RX
733 //
734 // Receive interrupt mask. A read returns the current mask for UART's receive
735 // interrupt. On a write of 1, the mask of the overrun error interrupt is set
736 // which means the interrupt state will be reflected in MIS.RX. A write of 0
737 // clears the mask which means MIS.RX will not reflect the interrupt.
738 #define UART_IMSC_RX 0x00000010U
739 #define UART_IMSC_RX_M 0x00000010U
740 #define UART_IMSC_RX_S 4U
741 
742 // Field: [1] CTSM
743 //
744 // Clear to Send (CTS) modem interrupt mask. A read returns the current mask
745 // for UART's clear to send interrupt. On a write of 1, the mask of the overrun
746 // error interrupt is set which means the interrupt state will be reflected in
747 // MIS.CTSM. A write of 0 clears the mask which means MIS.CTSM will not reflect
748 // the interrupt.
749 #define UART_IMSC_CTSM 0x00000002U
750 #define UART_IMSC_CTSM_M 0x00000002U
751 #define UART_IMSC_CTSM_S 1U
752 
753 //*****************************************************************************
754 //
755 // Register: UART_O_RIS
756 //
757 //*****************************************************************************
758 // Field: [13] RXDMADONE
759 //
760 // RX DMA done interrupt status:
761 // This field returns the raw interrupt state of UART's RX DMA done interrupt.
762 // RX DMA done flag is set when you recieve RX DMA done status from dma module.
763 #define UART_RIS_RXDMADONE 0x00002000U
764 #define UART_RIS_RXDMADONE_M 0x00002000U
765 #define UART_RIS_RXDMADONE_S 13U
766 
767 // Field: [12] TXDMADONE
768 //
769 // TX DMA done interrupt status:
770 // This field returns the raw interrupt state of UART's TX DMA done interrupt.
771 // TX DMA done flag is set when you recieve TX DMA done status from dma module.
772 #define UART_RIS_TXDMADONE 0x00001000U
773 #define UART_RIS_TXDMADONE_M 0x00001000U
774 #define UART_RIS_TXDMADONE_S 12U
775 
776 // Field: [11] EOT
777 //
778 // End of Transmission interrupt status:
779 // This field returns the raw interrupt state of UART's end of transmission
780 // interrupt. End of transmission flag is set when all the Transmit data in the
781 // FIFO and on the TX Line is tranmitted.
782 #define UART_RIS_EOT 0x00000800U
783 #define UART_RIS_EOT_M 0x00000800U
784 #define UART_RIS_EOT_S 11U
785 
786 // Field: [10] OE
787 //
788 // Overrun error interrupt status:
789 // This field returns the raw interrupt state of UART's overrun error
790 // interrupt. Overrun error occurs if data is received and the receive FIFO is
791 // full.
792 #define UART_RIS_OE 0x00000400U
793 #define UART_RIS_OE_M 0x00000400U
794 #define UART_RIS_OE_S 10U
795 
796 // Field: [9] BE
797 //
798 // Break error interrupt status:
799 // This field returns the raw interrupt state of UART's break error interrupt.
800 // Break error is set when a break condition is detected, indicating that the
801 // received data input (UARTRXD input pin) was held LOW for longer than a
802 // full-word transmission time (defined as start, data, parity and stop bits).
803 #define UART_RIS_BE 0x00000200U
804 #define UART_RIS_BE_M 0x00000200U
805 #define UART_RIS_BE_S 9U
806 
807 // Field: [8] PE
808 //
809 // Parity error interrupt status:
810 // This field returns the raw interrupt state of UART's parity error interrupt.
811 // Parity error is set if the parity of the received data character does not
812 // match the parity that the LCRH.EPS and LCRH.SPS select.
813 #define UART_RIS_PE 0x00000100U
814 #define UART_RIS_PE_M 0x00000100U
815 #define UART_RIS_PE_S 8U
816 
817 // Field: [7] FE
818 //
819 // Framing error interrupt status:
820 // This field returns the raw interrupt state of UART's framing error
821 // interrupt. Framing error is set if the received character does not have a
822 // valid stop bit (a valid stop bit is 1).
823 #define UART_RIS_FE 0x00000080U
824 #define UART_RIS_FE_M 0x00000080U
825 #define UART_RIS_FE_S 7U
826 
827 // Field: [6] RT
828 //
829 // Receive timeout interrupt status:
830 // This field returns the raw interrupt state of UART's receive timeout
831 // interrupt. The receive timeout interrupt is asserted when the receive FIFO
832 // is not empty, and no more data is received during a 32-bit period. The
833 // receive timeout interrupt is cleared either when the FIFO becomes empty
834 // through reading all the data, or when a 1 is written to ICR.RT.
835 // The raw interrupt for receive timeout cannot be set unless the mask is set
836 // (IMSC.RT = 1). This is because the mask acts as an enable for power saving.
837 // That is, the same status can be read from MIS.RT and RT.
838 #define UART_RIS_RT 0x00000040U
839 #define UART_RIS_RT_M 0x00000040U
840 #define UART_RIS_RT_S 6U
841 
842 // Field: [5] TX
843 //
844 // Transmit interrupt status:
845 // This field returns the raw interrupt state of UART's transmit interrupt.
846 // When FIFOs are enabled (LCRH.FEN = 1), the transmit interrupt is asserted if
847 // the number of bytes in transmit FIFO is equal to or lower than the
848 // programmed trigger level (IFLS.TXSEL). The transmit interrupt is cleared by
849 // writing data to the transmit FIFO until it becomes greater than the trigger
850 // level, or by clearing the interrupt through ICR.TX.
851 // When FIFOs are disabled (LCRH.FEN = 0), that is they have a depth of one
852 // location, the transmit interrupt is asserted if there is no data present in
853 // the transmitters single location. It is cleared by performing a single write
854 // to the transmit FIFO, or by clearing the interrupt through ICR.TX.
855 #define UART_RIS_TX 0x00000020U
856 #define UART_RIS_TX_M 0x00000020U
857 #define UART_RIS_TX_S 5U
858 
859 // Field: [4] RX
860 //
861 // Receive interrupt status:
862 // This field returns the raw interrupt state of UART's receive interrupt.
863 // When FIFOs are enabled (LCRH.FEN = 1), the receive interrupt is asserted if
864 // the receive FIFO reaches the programmed trigger
865 // level (IFLS.RXSEL). The receive interrupt is cleared by reading data from
866 // the receive FIFO until it becomes less than the trigger level, or by
867 // clearing the interrupt through ICR.RX.
868 // When FIFOs are disabled (LCRH.FEN = 0), that is they have a depth of one
869 // location, the receive interrupt is asserted if data is received
870 // thereby filling the location. The receive interrupt is cleared by performing
871 // a single read of the receive FIFO, or by clearing the interrupt through
872 // ICR.RX.
873 #define UART_RIS_RX 0x00000010U
874 #define UART_RIS_RX_M 0x00000010U
875 #define UART_RIS_RX_S 4U
876 
877 // Field: [1] CTSM
878 //
879 // Clear to Send (CTS) modem interrupt status:
880 // This field returns the raw interrupt state of UART's clear to send
881 // interrupt.
882 #define UART_RIS_CTSM 0x00000002U
883 #define UART_RIS_CTSM_M 0x00000002U
884 #define UART_RIS_CTSM_S 1U
885 
886 //*****************************************************************************
887 //
888 // Register: UART_O_MIS
889 //
890 //*****************************************************************************
891 // Field: [13] RXDMADONE
892 //
893 // RX DMA done interrupt status:
894 // This field returns the masked interrupt state of the RX DMA done interrupt
895 // which is the bitiwse AND product of raw interrupt state RIS.RXDMADONE and
896 // the mask setting IMSC.RXDMADONE.
897 #define UART_MIS_RXDMADONE 0x00002000U
898 #define UART_MIS_RXDMADONE_M 0x00002000U
899 #define UART_MIS_RXDMADONE_S 13U
900 
901 // Field: [12] TXDMADONE
902 //
903 // TX DMA done interrupt status:
904 // This field returns the masked interrupt state of the TX DMA done interrupt
905 // which is the bitwise AND product of raw interrupt state RIS.TXDMADONE and
906 // the mask setting IMSC.TXDMADONE.
907 #define UART_MIS_TXDMADONE 0x00001000U
908 #define UART_MIS_TXDMADONE_M 0x00001000U
909 #define UART_MIS_TXDMADONE_S 12U
910 
911 // Field: [11] EOT
912 //
913 // End of Transmission interrupt status:
914 // This field returns the masked interrupt state of the End of transmission
915 // interrupt which is the bitwise AND product of raw interrupt state RIS.EOT
916 // and the mask setting IMSC.EOT.
917 #define UART_MIS_EOT 0x00000800U
918 #define UART_MIS_EOT_M 0x00000800U
919 #define UART_MIS_EOT_S 11U
920 
921 // Field: [10] OE
922 //
923 // Overrun error masked interrupt status:
924 // This field returns the masked interrupt state of the overrun interrupt which
925 // is the bitwise AND product of raw interrupt state RIS.OE and the mask
926 // setting IMSC.OE.
927 #define UART_MIS_OE 0x00000400U
928 #define UART_MIS_OE_M 0x00000400U
929 #define UART_MIS_OE_S 10U
930 
931 // Field: [9] BE
932 //
933 // Break error masked interrupt status:
934 // This field returns the masked interrupt state of the break error interrupt
935 // which is the bitiwse AND product of raw interrupt state RIS.BE and the mask
936 // setting IMSC.BE.
937 #define UART_MIS_BE 0x00000200U
938 #define UART_MIS_BE_M 0x00000200U
939 #define UART_MIS_BE_S 9U
940 
941 // Field: [8] PE
942 //
943 // Parity error masked interrupt status:
944 // This field returns the masked interrupt state of the parity error interrupt
945 // which is the bitiwise AND product of raw interrupt state RIS.PE and the mask
946 // setting IMSC.PE.
947 #define UART_MIS_PE 0x00000100U
948 #define UART_MIS_PE_M 0x00000100U
949 #define UART_MIS_PE_S 8U
950 
951 // Field: [7] FE
952 //
953 // Framing error masked interrupt status: Returns the masked interrupt state of
954 // the framing error interrupt which is the bitiwse AND product of raw
955 // interrupt state RIS.FE and the mask setting IMSC.FE.
956 #define UART_MIS_FE 0x00000080U
957 #define UART_MIS_FE_M 0x00000080U
958 #define UART_MIS_FE_S 7U
959 
960 // Field: [6] RT
961 //
962 // Receive timeout masked interrupt status:
963 // Returns the masked interrupt state of the receive timeout interrupt.
964 // The raw interrupt for receive timeout cannot be set unless the mask is set
965 // (IMSC.RT = 1). This is because the mask acts as an enable for power saving.
966 // That is, the same status can be read from MIS.RT and RIS.RT.
967 #define UART_MIS_RT 0x00000040U
968 #define UART_MIS_RT_M 0x00000040U
969 #define UART_MIS_RT_S 6U
970 
971 // Field: [5] TX
972 //
973 // Transmit masked interrupt status:
974 // This field returns the masked interrupt state of the transmit interrupt
975 // which is the bitiwse AND product of raw interrupt state RIS.TX and the mask
976 // setting IMSC.TX.
977 #define UART_MIS_TX 0x00000020U
978 #define UART_MIS_TX_M 0x00000020U
979 #define UART_MIS_TX_S 5U
980 
981 // Field: [4] RX
982 //
983 // Receive masked interrupt status:
984 // This field returns the masked interrupt state of the receive interrupt
985 // which is the bitwise AND product of raw interrupt state RIS.RX and the mask
986 // setting IMSC.RX.
987 #define UART_MIS_RX 0x00000010U
988 #define UART_MIS_RX_M 0x00000010U
989 #define UART_MIS_RX_S 4U
990 
991 // Field: [1] CTSM
992 //
993 // Clear to Send (CTS) modem masked interrupt status:
994 // This field returns the masked interrupt state of the clear to send interrupt
995 // which is the bitwise AND product of raw interrupt state RIS.CTS and the mask
996 // setting IMSC.CTS.
997 #define UART_MIS_CTSM 0x00000002U
998 #define UART_MIS_CTSM_M 0x00000002U
999 #define UART_MIS_CTSM_S 1U
1000 
1001 //*****************************************************************************
1002 //
1003 // Register: UART_O_ICR
1004 //
1005 //*****************************************************************************
1006 // Field: [13] RXDMADONE
1007 //
1008 // RX DMA Done interrupt clear:
1009 // Writing 1 to this field clears the RX DMA done interrupt (RIS.RXDMADONE).
1010 // Writing 0 has no effect.
1011 #define UART_ICR_RXDMADONE 0x00002000U
1012 #define UART_ICR_RXDMADONE_M 0x00002000U
1013 #define UART_ICR_RXDMADONE_S 13U
1014 
1015 // Field: [12] TXDMADONE
1016 //
1017 // TX DMA Done interrupt clear:
1018 // Writing 1 to this field clears the TX DMA done interrupt (RIS.TXDMADONE).
1019 // Writing 0 has no effect.
1020 #define UART_ICR_TXDMADONE 0x00001000U
1021 #define UART_ICR_TXDMADONE_M 0x00001000U
1022 #define UART_ICR_TXDMADONE_S 12U
1023 
1024 // Field: [11] EOT
1025 //
1026 // End of Transmission interrupt clear:
1027 // Writing 1 to this field clears the End of Transmission interrupt (RIS.EOT).
1028 // Writing 0 has no effect.
1029 #define UART_ICR_EOT 0x00000800U
1030 #define UART_ICR_EOT_M 0x00000800U
1031 #define UART_ICR_EOT_S 11U
1032 
1033 // Field: [10] OE
1034 //
1035 // Overrun error interrupt clear:
1036 // Writing 1 to this field clears the overrun error interrupt (RIS.OE). Writing
1037 // 0 has no effect.
1038 #define UART_ICR_OE 0x00000400U
1039 #define UART_ICR_OE_M 0x00000400U
1040 #define UART_ICR_OE_S 10U
1041 
1042 // Field: [9] BE
1043 //
1044 // Break error interrupt clear:
1045 // Writing 1 to this field clears the break error interrupt (RIS.BE). Writing 0
1046 // has no effect.
1047 #define UART_ICR_BE 0x00000200U
1048 #define UART_ICR_BE_M 0x00000200U
1049 #define UART_ICR_BE_S 9U
1050 
1051 // Field: [8] PE
1052 //
1053 // Parity error interrupt clear:
1054 // Writing 1 to this field clears the parity error interrupt (RIS.PE). Writing
1055 // 0 has no effect.
1056 #define UART_ICR_PE 0x00000100U
1057 #define UART_ICR_PE_M 0x00000100U
1058 #define UART_ICR_PE_S 8U
1059 
1060 // Field: [7] FE
1061 //
1062 // Framing error interrupt clear:
1063 // Writing 1 to this field clears the framing error interrupt (RIS.FE). Writing
1064 // 0 has no effect.
1065 #define UART_ICR_FE 0x00000080U
1066 #define UART_ICR_FE_M 0x00000080U
1067 #define UART_ICR_FE_S 7U
1068 
1069 // Field: [6] RT
1070 //
1071 // Receive timeout interrupt clear:
1072 // Writing 1 to this field clears the receive timeout interrupt (RIS.RT).
1073 // Writing 0 has no effect.
1074 #define UART_ICR_RT 0x00000040U
1075 #define UART_ICR_RT_M 0x00000040U
1076 #define UART_ICR_RT_S 6U
1077 
1078 // Field: [5] TX
1079 //
1080 // Transmit interrupt clear:
1081 // Writing 1 to this field clears the transmit interrupt (RIS.TX). Writing 0
1082 // has no effect.
1083 #define UART_ICR_TX 0x00000020U
1084 #define UART_ICR_TX_M 0x00000020U
1085 #define UART_ICR_TX_S 5U
1086 
1087 // Field: [4] RX
1088 //
1089 // Receive interrupt clear:
1090 // Writing 1 to this field clears the receive interrupt (RIS.RX). Writing 0 has
1091 // no effect.
1092 #define UART_ICR_RX 0x00000010U
1093 #define UART_ICR_RX_M 0x00000010U
1094 #define UART_ICR_RX_S 4U
1095 
1096 // Field: [1] CTSM
1097 //
1098 // Clear to Send (CTS) modem interrupt clear:
1099 // Writing 1 to this field clears the clear to send interrupt (RIS.CTS).
1100 // Writing 0 has no effect.
1101 #define UART_ICR_CTSM 0x00000002U
1102 #define UART_ICR_CTSM_M 0x00000002U
1103 #define UART_ICR_CTSM_S 1U
1104 
1105 //*****************************************************************************
1106 //
1107 // Register: UART_O_DMACTL
1108 //
1109 //*****************************************************************************
1110 // Field: [2] DMAONERR
1111 //
1112 // DMA on error. If this bit is set to 1, the DMA receive request outputs (for
1113 // single and burst requests) are disabled when the UART error interrupt is
1114 // asserted (more specifically if any of the error interrupts RIS.PERIS,
1115 // RIS.BERIS, RIS.FERIS or RIS.OERIS are asserted).
1116 #define UART_DMACTL_DMAONERR 0x00000004U
1117 #define UART_DMACTL_DMAONERR_M 0x00000004U
1118 #define UART_DMACTL_DMAONERR_S 2U
1119 
1120 // Field: [1] TXDMAE
1121 //
1122 // Transmit DMA enable. If this bit is set to 1, DMA for the transmit FIFO is
1123 // enabled.
1124 #define UART_DMACTL_TXDMAE 0x00000002U
1125 #define UART_DMACTL_TXDMAE_M 0x00000002U
1126 #define UART_DMACTL_TXDMAE_S 1U
1127 
1128 // Field: [0] RXDMAE
1129 //
1130 // Receive DMA enable. If this bit is set to 1, DMA for the receive FIFO is
1131 // enabled.
1132 #define UART_DMACTL_RXDMAE 0x00000001U
1133 #define UART_DMACTL_RXDMAE_M 0x00000001U
1134 #define UART_DMACTL_RXDMAE_S 0U
1135 
1136 
1137 #endif // __UART__