CC23x0R5DriverLibrary
[setup.h] Setup
Collaboration diagram for [setup.h] Setup:

Functions

void SetupTrimDevice (void)
 Performs the necessary trim of the device which is not done in ROM boot code. More...
 

Detailed Description

This module contains functions for device setup which is not done in boot code.

Function Documentation

§ SetupTrimDevice()

void SetupTrimDevice ( void  )

Performs the necessary trim of the device which is not done in ROM boot code.

This function should only execute coming from ROM boot.

The following is handled by this function:

  • Checks if the driverlib variant used by the application is supported by the device. Execution is halted in case of unsupported driverlib variant.
  • Configures VIMS cache mode based on setting in CCFG.
  • Configures functionalities like DCDC and XOSC dependent on startup modes like cold reset, wakeup from shutdown and wakeup from from powerdown.
  • Configures VIMS power domain control.
  • Configures optimal wait time for flash FSM in cases where flash pump wakes up from sleep.
Note
The current implementation does not take soft reset into account. However, it does no damage to execute it again. It only consumes time.
This function is called by the compiler specific device startup codes that are integrated in the SimpleLink SDKs for CC13xx/CC26XX devices.
Returns
None

References CKMD_BASE, CKMD_HFXTINIT_AMPTHR_S, CKMD_HFXTINIT_IDAC_S, CKMD_HFXTINIT_IREF_S, CKMD_HFXTINIT_Q1CAP_S, CKMD_HFXTINIT_Q2CAP_S, CKMD_HFXTTARG_AMPHYST_S, CKMD_HFXTTARG_AMPTHR_S, CKMD_HFXTTARG_IDAC_S, CKMD_HFXTTARG_IREF_S, CKMD_HFXTTARG_Q1CAP_S, CKMD_HFXTTARG_Q2CAP_S, CKMD_O_HFXTINIT, CKMD_O_HFXTTARG, fcfg, HWREG, and HWREGB.