61 #include "../inc/hw_types.h" 62 #include "../inc/hw_memmap.h" 63 #include "../inc/hw_ckmd.h" __STATIC_INLINE void CKMDSetTargetQ1CapTrim(uint32_t q1Cap)
Sets target HFXT Q1 capacitor ramp trim.
Definition: ckmd.h:353
#define CKMD_HFXTTARG_Q1CAP_M
Definition: hw_ckmd.h:2824
#define CKMD_HFXTTARG_Q2CAP_M
Definition: hw_ckmd.h:2817
#define CKMD_HFXTINIT_AMPTHR_S
Definition: hw_ckmd.h:2746
#define CKMD_HFXTTARG_Q1CAP_S
Definition: hw_ckmd.h:2825
#define CKMD_HFXTTARG_AMPTHR_M
Definition: hw_ckmd.h:2796
__STATIC_INLINE void CKMDSetTargetIrefTrim(uint32_t iref)
Sets target HFXT IREF ramp trim.
Definition: ckmd.h:401
#define HWREG(x)
Definition: hw_types.h:79
#define __STATIC_INLINE
Definition: hw_types.h:58
__STATIC_INLINE uint32_t CKMDGetTargetAmplitudeThresholdTrim(void)
Gets target HFXT amplitude threshold ramp trim.
Definition: ckmd.h:531
#define CKMD_HFXTTARG_Q2CAP_S
Definition: hw_ckmd.h:2818
__STATIC_INLINE void CKMDSetTargetIdacTrim(uint32_t idac)
Sets target HFXT IDAC ramp trim.
Definition: ckmd.h:425
__STATIC_INLINE uint32_t CKMDGetTargetIdacTrim(void)
Gets target HFXT IDAC ramp trim.
Definition: ckmd.h:515
__STATIC_INLINE void CKMDSetInitialCapTrim(uint32_t q1CapTrim, uint32_t q2CapTrim)
Sets initial HFXT capacitor ramp trims.
Definition: ckmd.h:91
#define CKMD_O_HFXTINIT
Definition: hw_ckmd.h:142
#define CKMD_HFXTINIT_Q1CAP_M
Definition: hw_ckmd.h:2773
__STATIC_INLINE void CKMDSetInitialQ1CapTrim(uint32_t q1Cap)
Sets initial HFXT Q1 capacitor ramp trim.
Definition: ckmd.h:118
__STATIC_INLINE void CKMDSetInitialAmplitudeThresholdTrim(uint32_t amplitudeThreshold)
Sets initial HFXT amplitude threshold ramp trim.
Definition: ckmd.h:222
#define CKMD_HFXTINIT_IDAC_M
Definition: hw_ckmd.h:2752
#define CKMD_BASE
Definition: hw_memmap.h:49
#define CKMD_HFXTINIT_IREF_M
Definition: hw_ckmd.h:2759
#define CKMD_O_HFXTTARG
Definition: hw_ckmd.h:145
__STATIC_INLINE void CKMDSetInitialQ2CapTrim(uint32_t q2Cap)
Sets initial HFXT Q2 capacitor ramp trim.
Definition: ckmd.h:144
__STATIC_INLINE uint32_t CKMDGetTargetQ2CapTrim(void)
Gets target HFXT Q2 capacitor ramp trim.
Definition: ckmd.h:483
__STATIC_INLINE uint32_t CKMDGetInitialQ1CapTrim(void)
Gets initial HFXT Q1 capacitor ramp trim.
Definition: ckmd.h:240
__STATIC_INLINE uint32_t CKMDGetInitialIdacTrim(void)
Gets initial HFXT IDAC ramp trim.
Definition: ckmd.h:288
#define CKMD_HFXTTARG_IREF_S
Definition: hw_ckmd.h:2811
#define CKMD_HFXTTARG_AMPTHR_S
Definition: hw_ckmd.h:2797
__STATIC_INLINE void CKMDSetTargetAmplitudeThresholdTrim(uint32_t amplitudeThreshold)
Sets target HFXT amplitude threshold ramp trim.
Definition: ckmd.h:449
__STATIC_INLINE uint32_t CKMDGetTargetQ1CapTrim(void)
Gets target HFXT Q1 capacitor ramp trim.
Definition: ckmd.h:467
#define CKMD_HFXTTARG_IDAC_M
Definition: hw_ckmd.h:2803
#define CKMD_HFXTINIT_IDAC_S
Definition: hw_ckmd.h:2753
__STATIC_INLINE void CKMDSetTargetCapTrim(uint32_t q1CapTrim, uint32_t q2CapTrim)
Sets target HFXT capacitor ramp trims.
Definition: ckmd.h:329
__STATIC_INLINE uint32_t CKMDGetInitialIrefTrim(void)
Gets initial HFXT IREF ramp trim.
Definition: ckmd.h:272
__STATIC_INLINE void CKMDSetInitialIrefTrim(uint32_t iref)
Sets initial HFXT IREF ramp trim.
Definition: ckmd.h:170
__STATIC_INLINE uint32_t CKMDGetInitialAmplitudeThresholdTrim(void)
Gets initial HFXT amplitude threshold ramp trim.
Definition: ckmd.h:304
#define CKMD_HFXTTARG_IDAC_S
Definition: hw_ckmd.h:2804
__STATIC_INLINE void CKMDSetTargetQ2CapTrim(uint32_t q2Cap)
Sets target HFXT Q2 capacitor ramp trim.
Definition: ckmd.h:377
#define CKMD_HFXTINIT_Q1CAP_S
Definition: hw_ckmd.h:2774
__STATIC_INLINE void CKMDSetInitialIdacTrim(uint32_t idac)
Sets initial HFXT IDAC ramp trim.
Definition: ckmd.h:196
#define CKMD_HFXTINIT_Q2CAP_M
Definition: hw_ckmd.h:2766
#define CKMD_HFXTINIT_IREF_S
Definition: hw_ckmd.h:2760
#define CKMD_HFXTTARG_IREF_M
Definition: hw_ckmd.h:2810
#define CKMD_HFXTINIT_AMPTHR_M
Definition: hw_ckmd.h:2745
#define CKMD_HFXTINIT_Q2CAP_S
Definition: hw_ckmd.h:2767
__STATIC_INLINE uint32_t CKMDGetTargetIrefTrim(void)
Gets target HFXT IREF ramp trim.
Definition: ckmd.h:499
__STATIC_INLINE uint32_t CKMDGetInitialQ2CapTrim(void)
Gets initial HFXT Q2 capacitor ramp trim.
Definition: ckmd.h:256