CC23x0R5DriverLibrary
ckmd.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_ckmd.h"
Include dependency graph for ckmd.h:

Go to the source code of this file.

Functions

__STATIC_INLINE void CKMDSetInitialCapTrim (uint32_t q1CapTrim, uint32_t q2CapTrim)
 Sets initial HFXT capacitor ramp trims. More...
 
__STATIC_INLINE void CKMDSetInitialQ1CapTrim (uint32_t q1Cap)
 Sets initial HFXT Q1 capacitor ramp trim. More...
 
__STATIC_INLINE void CKMDSetInitialQ2CapTrim (uint32_t q2Cap)
 Sets initial HFXT Q2 capacitor ramp trim. More...
 
__STATIC_INLINE void CKMDSetInitialIrefTrim (uint32_t iref)
 Sets initial HFXT IREF ramp trim. More...
 
__STATIC_INLINE void CKMDSetInitialIdacTrim (uint32_t idac)
 Sets initial HFXT IDAC ramp trim. More...
 
__STATIC_INLINE void CKMDSetInitialAmplitudeThresholdTrim (uint32_t amplitudeThreshold)
 Sets initial HFXT amplitude threshold ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetInitialQ1CapTrim (void)
 Gets initial HFXT Q1 capacitor ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetInitialQ2CapTrim (void)
 Gets initial HFXT Q2 capacitor ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetInitialIrefTrim (void)
 Gets initial HFXT IREF ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetInitialIdacTrim (void)
 Gets initial HFXT IDAC ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetInitialAmplitudeThresholdTrim (void)
 Gets initial HFXT amplitude threshold ramp trim. More...
 
__STATIC_INLINE void CKMDSetTargetCapTrim (uint32_t q1CapTrim, uint32_t q2CapTrim)
 Sets target HFXT capacitor ramp trims. More...
 
__STATIC_INLINE void CKMDSetTargetQ1CapTrim (uint32_t q1Cap)
 Sets target HFXT Q1 capacitor ramp trim. More...
 
__STATIC_INLINE void CKMDSetTargetQ2CapTrim (uint32_t q2Cap)
 Sets target HFXT Q2 capacitor ramp trim. More...
 
__STATIC_INLINE void CKMDSetTargetIrefTrim (uint32_t iref)
 Sets target HFXT IREF ramp trim. More...
 
__STATIC_INLINE void CKMDSetTargetIdacTrim (uint32_t idac)
 Sets target HFXT IDAC ramp trim. More...
 
__STATIC_INLINE void CKMDSetTargetAmplitudeThresholdTrim (uint32_t amplitudeThreshold)
 Sets target HFXT amplitude threshold ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetTargetQ1CapTrim (void)
 Gets target HFXT Q1 capacitor ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetTargetQ2CapTrim (void)
 Gets target HFXT Q2 capacitor ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetTargetIrefTrim (void)
 Gets target HFXT IREF ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetTargetIdacTrim (void)
 Gets target HFXT IDAC ramp trim. More...
 
__STATIC_INLINE uint32_t CKMDGetTargetAmplitudeThresholdTrim (void)
 Gets target HFXT amplitude threshold ramp trim. More...