CC23x0R5DriverLibrary
chipinfo.h File Reference
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_fcfg.h"
#include "../inc/hw_sys0.h"
Include dependency graph for chipinfo.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Enumerations

enum  ChipType { CHIP_TYPE_CC2340R = 0x2DDAU }
 Chip type enumeration. More...
 
enum  ChipPartId { CC2340R52E0RGER = 0x012DDAU, CC2340R52E0RKPR = 0x3B2DDAU }
 Chip part ID enumeration. More...
 

Functions

__STATIC_INLINE uint32_t ChipInfoGetVersion (void)
 Returns hardware version number. More...
 
__STATIC_INLINE ChipType ChipInfoGetChipType (void)
 Returns chip type. More...
 
__STATIC_INLINE ChipPartId ChipInfoGetPartId (void)
 Returns part ID. More...