HCI_EXT_SetRxGainDone
---------------------
:Opcode: 0x0400
:Event Description: This event is sent to indicate the RF receiver gain has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetTxPowerDone
----------------------
:Opcode: 0x0401
:Event Description: This event is sent to indicate the RF transmitter power has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_OnePacketPerEventDone
-----------------------------
:Opcode: 0x0402
:Event Description: This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_DecryptCommandDone
--------------------------
:Opcode: 0x0405
:Event Description: This event is sent to indicate Decryption has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:Decrypted Data: 128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.

 :Size: 16 byte(s)
 :Range: Any 16 byte value


HCI_EXT_WriteLocalFeatureSupportDone
------------------------------------
:Opcode: 0x0406
:Event Description: This event is sent to indicate the Set Local Supported Features command has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetFastTxResponseTimeDone
---------------------------------
:Opcode: 0x0407
:Event Description: This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_ModemTestTxDone
-----------------------
:Opcode: 0x0408
:Event Description: This event is sent to indicate the Modem Test Transmit test has started, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_ModemHopTestTxDone
--------------------------
:Opcode: 0x0409
:Event Description: This event is sent to indicate the Modem Hop Test Transmit test has started, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_ModemTestRxDone
-----------------------
:Opcode: 0x040A
:Event Description: This event is sent to indicate the Modem Test Receive test has started, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_EnhancedModemTestTxDone
-------------------------------
:Opcode: 0x0427
:Event Description: This event is sent to indicate the enhanced Modem Test Transmit test has started, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_EnhancedModemHopTestTxDone
----------------------------------
:Opcode: 0x0428
:Event Description: This event is sent to indicate the enhanced Modem Hop Test Transmit test has started, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_EnhancedModemTestRxDone
-------------------------------
:Opcode: 0x0429
:Event Description: This event is sent to indicate the enhanced Modem Test Receive test has started, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_EndModemTestDone
------------------------
:Opcode: 0x040B
:Event Description: This event is sent to indicate the modem test has been shutdown, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetBDADDRDone
---------------------
:Opcode: 0x040C
:Event Description: This event is sent to indicate the devices BLE address has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetVirtualAdvAddrDone
-----------------------------
:Opcode: 0x042D
:Event Description: This event is sent to indicate the advertise's virtual address has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetSCADone
------------------
:Opcode: 0x040D
:Event Description: This event is sent to indicate the devices SCA has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_EnablePTMDone
---------------------
:Opcode: 0x040E
:Event Description: There is not a corresponding event opcode (0x040E) and parameters for this command as it is only allowed as a direct function call by the application software.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetMaxDtmTxPowerDone
----------------------------
:Opcode: 0x0411
:Event Description: This event is sent to indicate the maximum Direct Test Mode (DTM) RF transmitter power has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_DisconnectImmedDone
---------------------------
:Opcode: 0x0413
:Event Description: This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_PER
-----------
:Opcode: 0x0414
:Event Description: This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:PER Command Type: Read or Reset

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Reset PER Counters
         1                     Read PER Counters
         ===================== ========================================================

:RX Pkts: Number of received packets.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:RX CRC Fails: Number of received packets with CRC error.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:Events: Number of connection events.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:Missed Events: Number of missed connection events.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value


HCI_EXT_OverrideSLDone
----------------------
:Opcode: 0x041A
:Event Description: This event is sent to indicate the Set Slave Latency Override feature has been enabled or disabled, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_BuildRevisionDone
-------------------------
:Opcode: 0x041B
:Event Description: This event is sent to indicate the user revision number and the build revision of the stack, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:User Revision Number: The user revision number set by the application software. If no value was ever set, than 0x0000.

 :Condition: ( cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:Build Revision Number: The build revision number of the BLE stack.

 :Condition: ( cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value


HCI_EXT_ResetSystemDone
-----------------------
:Opcode: 0x041D
:Event Description: This event is sent to indicate the Reset System command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_NumComplPktsLimitDone
-----------------------------
:Opcode: 0x041F
:Event Description: This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_GetConnInfoDone
-----------------------
:Opcode: 0x0420
:Event Description: This event is sent to indicate the Get Connection Information command has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:Alloc Conns: Total number of allocated connections

 :Size: 1 byte(s)
 :Range: 

:Active Conns: Number of currently active connections

 :Size: 1 byte(s)
 :Range: 


An array of size "numConn" will be returned containing the parameters starting here:

:Conn Handle: Connection Handle

 :Size: 1 byte(s)
 :Range: 

:Conn Role: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x22                  LMP/LL Response Timeout
         0x23                  LMP Error Transaction Collision
         0x24                  LMP PDU Not Allowed
         0x25                  Encryption Mode Not Acceptable
         0x26                  Link Key Can Not be Changed
         0x27                  Requested QoS Not Supported
         0x28                  Instant Passed
         0x29                  Pairing With Unit Key Not Supported
         0x2A                  Different Transaction Collision
         0x2B                  Reserved
         0x2C                  QoS Unacceptable Parameter
         0x2D                  QoS Rejected
         0x2E                  Channel Assessment Not Supported
         0x2F                  Insufficient Security
         0x30                  Parameter Out Of Mandatory Range
         0x31                  Reserved
         0x32                  Role Switch Pending
         0x33                  Reserved
         0x34                  Reserved Slot Violation
         0x35                  Role Switch Failed
         0x36                  Extended Inquiry Response Too Large
         0x37                  Simple Pairing Not Supported By Host
         0x38                  Host Busy - Pairing
         0x39                  Connection Rejected Due To No Suitable Channel Found
         0x3A                  Controller Busy
         0x3B                  Unacceptable Connection Interval
         0x3C                  Directed Advertising Timeout
         0x3D                  Connection Terminated Due To MIC Failure
         0x3E                  Connection Failed To Be Established
         0x3F                  MAC Connection Failed
         0x40                  Coarse Clock Adjust Rejected
         0x41                  Type0 Submap Not Defined
         0x42                  Unknown Advertising Identifier
         0x43                  Limit Reached
         0x44                  Operation Cancelled by Host
         0x45                  Packet Too Long
         ===================== ========================================================

:Peer Addr: 

 :Size: 6 byte(s)
 :Range: 

:Peer Addr Type: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  Public
         0x01                  Random
         0x02                  Public Identity
         0x03                  Random Identity
         ===================== ========================================================


The array of parameters ends here.

HCI_EXT_SetMaxDataLengthDone
----------------------------
:Opcode: 0x0421
:Event Description: This event is sent to indicate the Set Max Data Length command has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetDtmTxPktCntDone
--------------------------
:Opcode: 0x0424
:Event Description: This event is sent to indicate the DTM TX Packet Count has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_LE_ADV_EVENT
--------------------
:Opcode: 0x0425
:Event Description: Extended advertisement event.

**Event Parameters**

:eventID: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  Adv Start After Enable
         0x01                  Adv End After Disable
         0x02                  Adv Start
         0x03                  Adv End
         0x04                  Adv Report
         0x05                  Adv Set Terminated
         0x06                  Scan req received
         0x07                  Scan Timeout
         0x08                  Scan Start
         0x09                  Scan End
         0x0A                  Scan Window End
         0x0B                  Scan Interval End
         0x0C                  Scan Duration End
         0x0D                  Scan Period End
         0x0E                  LL Out of memory
         0x0F                  Adv Data Truncated
         ===================== ========================================================

:handle: 

 :Size: 1 byte(s)
 :Range: 

:Adv Data Len: 

 :Condition: ( eventID==0x0f)
 :Size: 2 byte(s)
 :Range: 

:Available Adv Data Len: 

 :Condition: ( eventID==0x0f)
 :Size: 1 byte(s)
 :Range: 


HCI_EXT_LE_SCAN_EVENT
---------------------
:Opcode: 0x0426
:Event Description: Extended Scanner event.

**Event Parameters**

:eventID: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  Adv Start After Enable
         0x01                  Adv End After Disable
         0x02                  Adv Start
         0x03                  Adv End
         0x04                  Adv Report
         0x05                  Adv Set Terminated
         0x06                  Scan req received
         0x07                  Scan Timeout
         0x08                  Scan Start
         0x09                  Scan End
         0x0A                  Scan Window End
         0x0B                  Scan Interval End
         0x0C                  Scan Duration End
         0x0D                  Scan Period End
         0x0E                  LL Out of memory
         0x0F                  Adv Data Truncated
         ===================== ========================================================


HCI_EXT_SetPinOutputDone
------------------------
:Opcode: 0x042A
:Event Description: This event is sent to indicate the Enable Pin Output has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetLocationingAccuracyDone
----------------------------------
:Opcode: 0x042B
:Event Description: This event is sent to indicate the locationing accuracy has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_GetActiveConnInfoDone
-----------------------------
:Opcode: 0x042C
:Event Description: This event is sent to provide active connection information as requested.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


An array of size "cmConnInfo" will be returned containing the parameters starting here:

:Access Addr: 

 :Size: 4 byte(s)
 :Range: 

:Conn Interval (in 0.625ms units): 

 :Size: 2 byte(s)
 :Range: 

:Hop Value: 

 :Size: 1 byte(s)
 :Range: 

:mSCA: 

 :Size: 2 byte(s)
 :Range: 

:next chan: 

 :Size: 1 byte(s)
 :Range: 

:Chann Map: 

 :Size: 5 byte(s)
 :Range: 

:CrcInit: 

 :Size: 3 byte(s)
 :Range: 


The array of parameters ends here.

HCI_EXT_CoexEnableDone
----------------------
:Opcode: 0x042E
:Event Description: This event is sent to indicate the Enable Coex feature, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetDefaultChannelMapDone
--------------------------------
:Opcode: 0x042F
:Event Description: This event is sent to indicate the Set Default Channel Map feature, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetConnectionChannelMapDone
-----------------------------------
:Opcode: 0x0430
:Event Description: This event is sent to indicate the Set Connection Channel Map feature, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_LLTestModeDone
----------------------
:Opcode: 0x0470
:Event Description: LL Test Mode event.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


CommandStatus
-------------
:Opcode: 0x067F
:Event Description: The Command Status event is used to indicate that the command given by opCode parameter has been received and is being processed. If successful, an HCI vendor specific event that corresponds to the command will follow if applicable. Otherwise, no event will follow since the command was not started.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  SUCCESS
         0x12                  bleIncorrectMode
         0x02                  INVALIDPARAMETER
         ===================== ========================================================

:opCode: opCode from the corresponding command

 :Size: 2 byte(s)
 :Range: See Command Table

:length: Payload length

 :Condition: (StatOpCode!=0x010C && StatOpCode!=0xFCF3 && StatOpCode!=0xFCF4 && StatOpCode!=0xFCF5 && StatOpCode!=0xFE84 && StatOpCode!=0xFE87 && StatOpCode!=0xFE3E && StatOpCode!=0xFE54 && StatOpCode!=0xFE56 && StatOpCode!=0xFE58 && StatOpCode!=0xFE61 && StatOpCode!=0x0682 && StatOpCode!=0xFE43 && StatOpCode!=0xFE37 && StatOpCode!=0xFE49)
 :Size: 1 byte(s)

:payload: See the corresponding command for payload parsing information if it exists.

 :Condition: (StatOpCode!=0x010C && StatOpCode!=0xFCF3 && StatOpCode!=0xFCF4 && StatOpCode!=0xFCF5 && StatOpCode!=0xFE84 && StatOpCode!=0xFE87 && StatOpCode!=0xFE3E && StatOpCode!=0xFE54 && StatOpCode!=0xFE56 && StatOpCode!=0xFE58 && StatOpCode!=0xFE61 && StatOpCode!=0x0682 && StatOpCode!=0xFE43 && StatOpCode!=0xFE37 && StatOpCode!=0xFE49)
 :Size: length byte(s)