HCI_EXT_SetRxGainDone

Opcode:

0x0400

Event Description:

This event is sent to indicate the RF receiver gain has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetTxPowerDone

Opcode:

0x0401

Event Description:

This event is sent to indicate the RF transmitter power has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_OnePacketPerEventDone

Opcode:

0x0402

Event Description:

This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_DecryptCommandDone

Opcode:

0x0405

Event Description:

This event is sent to indicate Decryption has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

Decrypted Data:

128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.

Size:

16 byte(s)

Range:

Any 16 byte value

HCI_EXT_WriteLocalFeatureSupportDone

Opcode:

0x0406

Event Description:

This event is sent to indicate the Set Local Supported Features command has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetFastTxResponseTimeDone

Opcode:

0x0407

Event Description:

This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_ModemTestTxDone

Opcode:

0x0408

Event Description:

This event is sent to indicate the Modem Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_ModemHopTestTxDone

Opcode:

0x0409

Event Description:

This event is sent to indicate the Modem Hop Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_ModemTestRxDone

Opcode:

0x040A

Event Description:

This event is sent to indicate the Modem Test Receive test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnhancedModemTestTxDone

Opcode:

0x0427

Event Description:

This event is sent to indicate the enhanced Modem Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnhancedModemHopTestTxDone

Opcode:

0x0428

Event Description:

This event is sent to indicate the enhanced Modem Hop Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnhancedModemTestRxDone

Opcode:

0x0429

Event Description:

This event is sent to indicate the enhanced Modem Test Receive test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EndModemTestDone

Opcode:

0x040B

Event Description:

This event is sent to indicate the modem test has been shutdown, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetBDADDRDone

Opcode:

0x040C

Event Description:

This event is sent to indicate the devices BLE address has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetVirtualAdvAddrDone

Opcode:

0x042D

Event Description:

This event is sent to indicate the advertise’s virtual address has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetSCADone

Opcode:

0x040D

Event Description:

This event is sent to indicate the devices SCA has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnablePTMDone

Opcode:

0x040E

Event Description:

There is not a corresponding event opcode (0x040E) and parameters for this command as it is only allowed as a direct function call by the application software.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetMaxDtmTxPowerDone

Opcode:

0x0411

Event Description:

This event is sent to indicate the maximum Direct Test Mode (DTM) RF transmitter power has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_DisconnectImmedDone

Opcode:

0x0413

Event Description:

This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_PER

Opcode:

0x0414

Event Description:

This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

PER Command Type:

Read or Reset

Size:

1 byte(s)

Range:

Value

Description

0

Reset PER Counters

1

Read PER Counters

RX Pkts:

Number of received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX CRC Fails:

Number of received packets with CRC error.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Events:

Number of connection events.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Missed Events:

Number of missed connection events.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_OverrideSLDone

Opcode:

0x041A

Event Description:

This event is sent to indicate the Set Slave Latency Override feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_BuildRevisionDone

Opcode:

0x041B

Event Description:

This event is sent to indicate the user revision number and the build revision of the stack, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

User Revision Number:

The user revision number set by the application software. If no value was ever set, than 0x0000.

Condition:

( cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Build Revision Number:

The build revision number of the BLE stack.

Condition:

( cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_ResetSystemDone

Opcode:

0x041D

Event Description:

This event is sent to indicate the Reset System command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_NumComplPktsLimitDone

Opcode:

0x041F

Event Description:

This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_GetConnInfoDone

Opcode:

0x0420

Event Description:

This event is sent to indicate the Get Connection Information command has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

Alloc Conns:

Total number of allocated connections

Size:

1 byte(s)

Range:

Active Conns:

Number of currently active connections

Size:

1 byte(s)

Range:

An array of size “numConn” will be returned containing the parameters starting here:

Conn Handle:

Connection Handle

Size:

1 byte(s)

Range:

Conn Role:
Size:

1 byte(s)

Range:

Value

Description

0x22

LMP/LL Response Timeout

0x23

LMP Error Transaction Collision

0x24

LMP PDU Not Allowed

0x25

Encryption Mode Not Acceptable

0x26

Link Key Can Not be Changed

0x27

Requested QoS Not Supported

0x28

Instant Passed

0x29

Pairing With Unit Key Not Supported

0x2A

Different Transaction Collision

0x2B

Reserved

0x2C

QoS Unacceptable Parameter

0x2D

QoS Rejected

0x2E

Channel Assessment Not Supported

0x2F

Insufficient Security

0x30

Parameter Out Of Mandatory Range

0x31

Reserved

0x32

Role Switch Pending

0x33

Reserved

0x34

Reserved Slot Violation

0x35

Role Switch Failed

0x36

Extended Inquiry Response Too Large

0x37

Simple Pairing Not Supported By Host

0x38

Host Busy - Pairing

0x39

Connection Rejected Due To No Suitable Channel Found

0x3A

Controller Busy

0x3B

Unacceptable Connection Interval

0x3C

Directed Advertising Timeout

0x3D

Connection Terminated Due To MIC Failure

0x3E

Connection Failed To Be Established

0x3F

MAC Connection Failed

0x40

Coarse Clock Adjust Rejected

0x41

Type0 Submap Not Defined

0x42

Unknown Advertising Identifier

0x43

Limit Reached

0x44

Operation Cancelled by Host

0x45

Packet Too Long

Peer Addr:
Size:

6 byte(s)

Range:

Peer Addr Type:
Size:

1 byte(s)

Range:

Value

Description

0x00

Public

0x01

Random

0x02

Public Identity

0x03

Random Identity

The array of parameters ends here.

HCI_EXT_SetMaxDataLengthDone

Opcode:

0x0421

Event Description:

This event is sent to indicate the Set Max Data Length command has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetDtmTxPktCntDone

Opcode:

0x0424

Event Description:

This event is sent to indicate the DTM TX Packet Count has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_LE_ADV_EVENT

Opcode:

0x0425

Event Description:

Extended advertisement event.

Event Parameters

eventID:
Size:

1 byte(s)

Range:

Value

Description

0x00

Adv Start After Enable

0x01

Adv End After Disable

0x02

Adv Start

0x03

Adv End

0x04

Adv Report

0x05

Adv Set Terminated

0x06

Scan req received

0x07

Scan Timeout

0x08

Scan Start

0x09

Scan End

0x0A

Scan Window End

0x0B

Scan Interval End

0x0C

Scan Duration End

0x0D

Scan Period End

0x0E

LL Out of memory

0x0F

Adv Data Truncated

handle:
Size:

1 byte(s)

Range:

Adv Data Len:
Condition:

( eventID==0x0f)

Size:

2 byte(s)

Range:

Available Adv Data Len:
Condition:

( eventID==0x0f)

Size:

1 byte(s)

Range:

HCI_EXT_LE_SCAN_EVENT

Opcode:

0x0426

Event Description:

Extended Scanner event.

Event Parameters

eventID:
Size:

1 byte(s)

Range:

Value

Description

0x00

Adv Start After Enable

0x01

Adv End After Disable

0x02

Adv Start

0x03

Adv End

0x04

Adv Report

0x05

Adv Set Terminated

0x06

Scan req received

0x07

Scan Timeout

0x08

Scan Start

0x09

Scan End

0x0A

Scan Window End

0x0B

Scan Interval End

0x0C

Scan Duration End

0x0D

Scan Period End

0x0E

LL Out of memory

0x0F

Adv Data Truncated

HCI_EXT_SetPinOutputDone

Opcode:

0x042A

Event Description:

This event is sent to indicate the Enable Pin Output has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetLocationingAccuracyDone

Opcode:

0x042B

Event Description:

This event is sent to indicate the locationing accuracy has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_GetActiveConnInfoDone

Opcode:

0x042C

Event Description:

This event is sent to provide active connection information as requested.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

An array of size “cmConnInfo” will be returned containing the parameters starting here:

Access Addr:
Size:

4 byte(s)

Range:

Conn Interval (in 0.625ms units):
Size:

2 byte(s)

Range:

Hop Value:
Size:

1 byte(s)

Range:

mSCA:
Size:

2 byte(s)

Range:

next chan:
Size:

1 byte(s)

Range:

Chann Map:
Size:

5 byte(s)

Range:

CrcInit:
Size:

3 byte(s)

Range:

The array of parameters ends here.

HCI_EXT_CoexEnableDone

Opcode:

0x042E

Event Description:

This event is sent to indicate the Enable Coex feature, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetDefaultChannelMapDone

Opcode:

0x042F

Event Description:

This event is sent to indicate the Set Default Channel Map feature, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetConnectionChannelMapDone

Opcode:

0x0430

Event Description:

This event is sent to indicate the Set Connection Channel Map feature, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_LLTestModeDone

Opcode:

0x0470

Event Description:

LL Test Mode event.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

CommandStatus

Opcode:

0x067F

Event Description:

The Command Status event is used to indicate that the command given by opCode parameter has been received and is being processed. If successful, an HCI vendor specific event that corresponds to the command will follow if applicable. Otherwise, no event will follow since the command was not started.

Event Parameters

Status:
Size:

1 byte(s)

Range:

Value

Description

0x00

SUCCESS

0x12

bleIncorrectMode

0x02

INVALIDPARAMETER

opCode:

opCode from the corresponding command

Size:

2 byte(s)

Range:

See Command Table

length:

Payload length

Condition:

(StatOpCode!=0x010C && StatOpCode!=0xFCF3 && StatOpCode!=0xFCF4 && StatOpCode!=0xFCF5 && StatOpCode!=0xFE84 && StatOpCode!=0xFE87 && StatOpCode!=0xFE3E && StatOpCode!=0xFE54 && StatOpCode!=0xFE56 && StatOpCode!=0xFE58 && StatOpCode!=0xFE61 && StatOpCode!=0x0682 && StatOpCode!=0xFE43 && StatOpCode!=0xFE37 && StatOpCode!=0xFE49)

Size:

1 byte(s)

payload:

See the corresponding command for payload parsing information if it exists.

Condition:

(StatOpCode!=0x010C && StatOpCode!=0xFCF3 && StatOpCode!=0xFCF4 && StatOpCode!=0xFCF5 && StatOpCode!=0xFE84 && StatOpCode!=0xFE87 && StatOpCode!=0xFE3E && StatOpCode!=0xFE54 && StatOpCode!=0xFE56 && StatOpCode!=0xFE58 && StatOpCode!=0xFE61 && StatOpCode!=0x0682 && StatOpCode!=0xFE43 && StatOpCode!=0xFE37 && StatOpCode!=0xFE49)

Size:

length byte(s)