.. _sec-mcuboot-imgtool:

Post-Build Script imgtool
=========================

The compiler output requires a post-build step to generate a .bin file that can
be used by MCUboot. An MCUboot compatible image tool must be executed called
``imgtool``. It is responsible for adding the MCUBoot image header, managing
keys and sign the image. More detailed description is provided on the
`imgtool documentation page <https://docs.mcuboot.com/imgtool.html>`_.
This tool requires Python3 and is included in the SimpleLink SDK in the folder
``<simplelink-install-dir>\source\third_party\mcuboot\scripts``.

The script can be executed automatically after every build by adding below lines
as ``Post-Build steps`` in ``Properties > Build`` as shown below. This command
defines the image version. To update the version number, adjust the string
``--version 1.0.0``.

.. ifconfig:: device == 'cc23xx'

    .. code-block:: c
        :caption: Post-Build Steps
        :linenos:
    
        ${CG_TOOL_ROOT}/bin/tiarmobjcopy ${ProjName}.out --output-target binary ${ProjName}.bin --remove-section=.ccfg
        ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/tools/common/mcuboot/imgtool sign --header-size 0x100 --align 4 --slot-size 0x4C000 --version 1.0.0 --pad-header --key ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/third_party/mcuboot/root-ec-p256.pem ${ProjName}.bin ${ProjName}.bin
    
    .. figure:: resources/mcuboot_postscriptsteps-cc23xx.png
        :align: center
    
        Post-Build steps included in CCS properties

.. ifconfig:: device == 'cc13xx_cc26xx'

    .. code-block:: c
        :caption: Post-Build Steps
        :linenos:
    
        ${CG_TOOL_ROOT}/bin/tiarmobjcopy -O binary ${ProjName}.out ${ProjName}.bin --remove-section=.ccfg
        ${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/tools/common/mcuboot/imgtool sign --header-size 0x100 --align 4 --slot-size 0x4BF00 --version 1.0.0 --pad-header --pad --key ${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/third_party/mcuboot/root-ec-p256.pem ${ProjName}.bin ${ProjName}.bin
    
    .. figure:: resources/mcuboot_postscriptsteps-cc13xx_cc26xx.png
        :align: center
    
        Post-Build steps included in CCS properties