.. _sec-mcuboot-oad-flash-layout-on-chip-stack-library:

Flash Layout for On-Chip OAD
=============================

This section will describe the method for placing images in internal
flash when using on-chip OAD.


Constraints and Requirements for On-chip OAD (stack library)
------------------------------------------------------------

The following points must be considered for On-chip OAD applications:

  - The user application must be sufficiently small in order to fit into the
    flash layout system described below
  - User app functionality is lost while performing OAD (Persistent app is
    running)

.. _sect-mcuboot-on-chip-memory-layout-stack-library:

Internal Flash Memory Layout
----------------------------

The internal flash of the device contains the active user application, the user
application's stack, the persistent application, the persistent application's
stack, and the secure bootloader. Each application's role is defined below.

.. note::     
    As we have assumed the stack-library approach, the stack images
    referenced below are a part of each application image (i.e. the user and
    persistent apps have their own dedicated stack)

+------------------------+---------------------------------------------------------------------+
| Application Name       | Description                                                         |
+------------------------+---------------------------------------------------------------------+
| MCUBoot bootloader     | - Search for the proper image in FLASH                              |
|                        | - Ensure validity and security of image before running              |
|                        | - Jump to the valid and newest image                                |
+------------------------+---------------------------------------------------------------------+
| Persistent application | - Providing lightweight application that implements the OAD profile |
+------------------------+---------------------------------------------------------------------+
| Stack (2)              | - BLE protocol stack implementation                                 |
+------------------------+---------------------------------------------------------------------+
| User application       | - User application                                                  |
|                        | - Must implement OAD reset service                                  |
+------------------------+---------------------------------------------------------------------+

.. _fig-mcuboot-on-chip-oad-target-memory-partition:
.. ditaa::
    :--no-separation:

                                                       Internal Flash
                                                   +-------------------+ <- 0x00000000
                                                   |   MCUBoot         |
                                                   |   Bootloader      |
                                                   |      cRED         |
                                                   +-------------------+ <- 0x00006000
                                                   | MCUBoot           |
                                                   | Header            |
                                                   | c777              |
                                                   +-------------------+ <- 0x00006100
                                                   | Persistent App    |
                                                   | Header            |
                                                   | c7AF              |
                                                   +-------------------+
                                                   |   Persistent      |
                                                   |   Application     |  Secondary Slot
                                                   |        +          |
                                                   |   Stack Library   |
                                                   |       c7AF        |
                                                   +-------------------+ <- 0x00030000
                                                   | User App + Stack  |
                                                   | Header            |
                                                   | c7AF              |
                                                   +-------------------+
                                                   |  User Application |
                                                   |        +          |  Primary Slot
                                                   |  Stack Library    |
                                                   |      c7AF         |
                                                   |                   |
                                                   |                   |
                                                   |                   |
                                         /-------> +-------------------+ <- Device Flash Size - 0x4000
     +------------------------------+    |         |   NV Space        |
     |  NV Information is           |    |         |   Reserved for    |
     |  shared between              |    |         |   Bonding         |
     |  Persistent and User         |    |         |   Information     |
     |  Application                 |    |         |        c777       |
     |                              |    |         |                   |
     +------------------------------+----\-------> +-------------------+ <- Device Flash Size

The user application pictured above is responsible for the following:

    - Implementing the protocol stack definition of the OAD reset service
    - Implementing customer defined behavior

The persistent application pictured above is responsible for the following:

    - Implementing the protocol stack definition of the OAD service
    - It is permanently resident on the device

.. note:: 

    Based on different devices, the address of each component listed above might
    vary. The address used in the persistent application linker file
    should match the settings in the ``flash_map_backend.h`` file.

    .. code-block:: c
        :caption: Flash addresses for various components

        #define MCUBOOT_BASE    0x0000000
        #define PERSISTENT_BASE 0x0006000
        #define APP_BASE        0x0030000
        #define NVS_BASE        (FLASH_SIZE - NVS_SIZE)
        #define NVS_SIZE        0x4000
        #define MCU_HDR_SIZE    0x100
        #define MCUBOOT_SIZE    0x6000
        #define MCU_OVERHEADS   (MCU_HDR_SIZE + MCU_TLV_SIZE)