.. _sec-freertos-config:

Kernel Configuration
--------------------

The FreeRTOS kernel is configured by FreeRTOSConfig.h file which can be found
in ``{SDK_INSTALL_DIR}\kernel\freertos\builds\{DEVICE}\release\pregenerated_configuration``,
you can change the configuration file so that the kernel will be tailored to your application.
For more information about kernel configuration, please see |FreeRTOS KERNEL CONFIGURATION|.

In the |SDK|, all FreeRTOS application routines are abstracted using the following:

- A POSIX layer, which was designed for use with this |SDK|
- A Driver Porting Layer (DPL) for use by the TI Drivers

You can find example FreeRTOS projects that use the |SDK| in the ``examples/rtos/``
folder for all supported IDEs.

No native FreeRTOS examples are provided in this |SDK|. If you want to use the native
FreeRTOS routines without the abstractions provided by the |SDK|, documentation is provided
on the |FREERTOS_WEB|.

.. ifconfig:: device != 'cc23xx' and doctarget=='ble5'

  .. note::

      At this moment, the only example with FreeRTOS support is ``multi_role`` inside the SimpleLink_Lowpower_F2 SDK.

POSIX Support
-------------

Portable Operating System Interface (POSIX) is an IEEE industry API standard for
OS compatibility. The |SDK| provides support for POSIX APIs on top of
FreeRTOS (as it does for TI-RTOS7). For a more detailed description of the POSIX
support in the |SDK|, please refer to the
`POSIX Overview Workshop <https://dev.ti.com/tirex/explore/node?node=ACzypa9NTyZS--.cZMxD.g__BSEc4rl__LATEST>`_

Driver Porting Layer (DPL)
--------------------------

The TI Drivers (e.g. UART2, I2C, Power Management, etc.) are written to be used
with the Driver Porting Layer (DPL). The |SDK| includes a DPL
implementation for both FreeRTOS, TI-RTOS7 and no RTOS.

        .. figure:: resources/driver_levels_dpl.png
            :align: center

Using FreeRTOS with CCS
-----------------------

In order to use FreeRTOS within CCS, you must specify the location of the FreeRTOS
installation. To do this, follow these steps:

.. only:: sdk_includes_ble

  1. In CCS, choose Window |rarr| Preferences from the menus.
  2. Select the General |rarr| Workspace |rarr| Linked Resource category.
  3. Click New and add a link with the following settings.

      * Name: ``FREERTOS_INSTALL_DIR``
      * Value: The location of your FreeRTOS installation

          .. figure:: resources/freertos_install_dir.png
              :align: center

  These steps only need to be performed once per CCS workspace that you create.

.. ifconfig:: device != 'cc23xx'

  Using FreeRTOS with IAR
  -----------------------

  The Quick Start guide has step-by-step instructions for building SDK Projects
  with IAR. Once these steps are followed, the user still needs to give IAR the
  location of the FREERTOS_INSTALL_DIR in the Custom Argvars:

  1. Open Tools -> Configure Custom Argument Variables
  2. Open the Global SDK paths.
  3. Configure the FREERTOS_INSTALL_DIR variable to match your install directory.

      .. figure:: resources/configure_iar.png
          :align: center
          :width: 600px


.. ifconfig:: device != 'cc23xx' and doctarget=='ble5'

  .. _freertos_examples:

  FreeRTOS examples
  -----------------

  As mentioned before, only the ``multi_role`` example supports FreeRTOS and
  it needs to be used with the gcc compiler, therefore please import the
  project located in ``multi_role/freertos/gcc``.

          .. figure:: resources/freertos_project_import.png
              :align: center

  Two projects will get imported:

          .. figure:: resources/multi_role_freertos_import.png
              :align: center


FreeRTOS vs. TI-RTOS7 modules
-----------------------------

The application and the ICall layer communicate using events to call the
OS and made context switch. The table below shows the modules that are used by
TI-RTOS7 in a typical example flow, at the same time explains which modules are
used by FreeRTOS.

.. _tbl-freertos-modules:
.. table:: Replacing modules that supports FreeRTOS in place of TI-RTOS7 modules

    +----------------------------+----------------------------------+-------------------------------------+
    | **Example flow**           | **TI-RTOS7 modules**             | **FreeRTOS modules**                |
    +----------------------------+----------------------------------+-------------------------------------+
    | 1. *Application Thread*    | *TI-RTOS7* Semaphore/Event       | SemaphoreP (used through DPL layer) |
    | Listen (pend) on event     |                                  | and mq_send / mq_receive *Blocking* |
    | number                     |                                  | Mqueue (POSIX queues)               |
    |                            |                                  |                                     |
    |                            |                                  |                                     |
    +----------------------------+----------------------------------+-------------------------------------+
    | 2. *Stack Thread*          | *TI-RTOS7* Timers                | TimersP (used through DPL layer)    |
    | Doing whatever he asked    |                                  |                                     |
    | to do by the app called    |                                  |                                     |
    |                            |                                  |                                     |
    |                            |                                  |                                     |
    +----------------------------+----------------------------------+-------------------------------------+
    | 3. *Stack Thread*          | *TI-RTOS7* utility Queue         | mq_send / mq_receive *NON-Blocking* |
    | Push a message (or number  |                                  | Mqueue (POSIX queues)               |
    | of messages) into the      |                                  |                                     |
    | queue and post an event    |                                  |                                     |
    | Queue                      |                                  |                                     |
    +----------------------------+----------------------------------+-------------------------------------+
    | 4. *Application Thread*    | *TI-RTOS7* utility Queue         | mq_send / mq_receive *NON-Blocking* |
    | OS wakes the application   |                                  | Mqueue (POSIX queues)               |
    | thread and the application |                                  |                                     |
    | pulls the message from the |                                  |                                     |
    | Non-OS queue               |                                  |                                     |
    +----------------------------+----------------------------------+-------------------------------------+
    | 5. *Application Thread*    | *TI-RTOS7* event                 | mq_send / mq_receive *Blocking*     |
    | Listen (pend) on event     |                                  | Mqueue (POSIX queues)               |
    | number - cycle has         |                                  |                                     |
    | completed                  |                                  |                                     |
    |                            |                                  |                                     |
    +----------------------------+----------------------------------+-------------------------------------+

.. only:: sdk_includes_ble

    icall_POSIX
    -----------

    The file ICall_POSIX is based on POSIX, DPL and FreeRTOS bare APIs
    calls. This implementation should allow us to support different Operating Systems if
    required. In order to do this, all the ``#ifdef FreeRTOS`` on the current ICall_POSIX
    could be changed to support a different OS.

    Here are some of the places where these defines are used (``icall_POSIX.c``):

       .. code-block:: c
         :caption: ``ical_POSIX.c - Includes``
         :emphasize-lines: 1, 2, 3, 4

         #ifdef FREERTOS
         #include <FreeRTOS.h>
         #include <task.h>
         #endif

       .. code-block:: c
         :caption: ``ical_POSIX.c - ICall_taskSelf()``
         :emphasize-lines: 4, 5, 6

         Task_Handle ICall_taskSelf(void)
         {
           Task_Handle task = NULL;
         #ifdef FREERTOS
           task = (Task_Handle) xTaskGetCurrentTaskHandle();
         #else
           task = <handler need to be returned according to the chosen OS>;
         #endif // FREERTOS
           return (task);
         }

       .. code-block:: c
         :caption: ``ical_POSIX.c``
         :emphasize-lines: 9-10

         #ifndef FREERTOS
         #if defined(HEAPMGR_CONFIG) && ((HEAPMGR_CONFIG == 0) || (HEAPMGR_CONFIG == 0x80))
         #include <rtos_heaposal.h>
         #elif defined(HEAPMGR_CONFIG) && ( (HEAPMGR_CONFIG == 1) || (HEAPMGR_CONFIG == 0x81))
         #include <rtos_heapmem.h>
         #elif defined(HEAPMGR_CONFIG) && ( (HEAPMGR_CONFIG == 2) || (HEAPMGR_CONFIG == 0x82))
         #include <rtos_heaptrack.h>
         #else
         static ICall_CSState ICall_heapCSState;
         #include <rtos_heaposal.h>
         #endif
         #endif // !FREERTOS