.. WARNING
    R&D is refactoring OAD for Q1 SDK, and the application will look quite 
    different and some of the states might no longer be applicable.
    Remember to scrub this rst again.

.. _sec-mcuboot-oad-process:

OAD Application
===============

The application layer is responsible for plugging the OAD service. The OAD
profile and communication with the BLE-Stack is encapsulated inside the OAD
module. An application developer wishing to implement use the TI OAD solution
will not need to worry about implementing the OAD state machine. The details 
of the OAD application layer are documented here for completeness 
and to aide in debugging.

OAD Software Architecture
-------------------------

The building blocks of the OAD software architecture are detailed below.
In the figure below the following terms have been abbreviated for compactness in
the image.

    - CB : Callback
    - SVC: BLE Service
    - Func: Function

.. ditaa::
    :--no-separation:

        +--------------------------------+
        |       Application Task         |
        |           cGRE                 |
        +-+-+--------------------+-+-----+
          | |         ^          | |  ^ ^
    Func  | |  Event  |          | |  | | Other BLE Stack
    calls | |    CB   |          | |  | | Func calls and events/CBs
          | |         |          | |  | |
          | |         |          | |  | |
          v v         |          | |  | |
        +-------------+-+        | |  | |
        |      OAD      |        | |  | |
        |      cRED     |        | |  | |
        +-+-+-----------+        | |  | |
    GATT  | |     SVC ^          | |  | |
    SVC   | |     CBs |          | |  | |
    func  | |         |          | |  | |
    calls | |         |          | |  | |
          V V         |          V V  | |
        +-------------+---------------+-++
        |            BLE-Stack           |
        |              cBLK              |
        +--------------------------------+

Internally the OAD service is responsible for the following:

    - Implementing the OAD profile
    - Plugging the GATT read and write callback from the |STACK|
    - Serializing and de-serializing structures from over the messages
    - Sending OAD related requests and responses to the |STACK| to be sent over
      the air
    - Queuing up messages from stack callbacks to be processed later by the
      application
    - Implementing the OAD state machine, and ensuring proper state transitions
    - Implementing the OAD inactivity timers
    - Implementing getter/setter functions for the application to use and
      configure the OAD service

External to the OAD service the application task is responsible for the
following. For more information, see the OAD Advanced lab of the SimpleLink
Academy.

    - Plugging an OAD event handler
    - Calling the OAD event processing function in a task context when events
      are posted.
    - Resetting the device when the ``OAD_DL_COMPLETE`` event is received.

A message sequence chart is included below to show a sample of an application's
interaction with the OAD service.


    .. _fig-mcuboot-oad-call-graph:
    .. uml::
        :caption: OAD service/ Application interaction
        :align: center

        @startuml
        hide footbox

        participant app_task.c as app
        participant oad.c as oad
        participant "BLE Stack" as BLE
        participant "OAD Queue" as OADQ

        box "BLE-Stack Context"
            participant "GATT R/W Callback" as GATT
        end box

        activate app

        group Initialize OAD service
            app -> oad : OAD_open()

            activate oad
            oad -> BLE : GATTServApp_InitCharCfg() (repeat for each char CCCD)
            oad -> BLE : GATTServApp_RegisterService()

            oad -> OADQ : Queue_construct()
            deactivate oad

            app -> oad : OAD_register()
        end

        BLE -> app : ATT_MTU_UPDATED_EVENT
        app -> oad : OAD_setBlockSize()


        group Processing OAD Service Messages
            note over oad, BLE
                Peer device sends OTA command/write
            end note

            activate GATT
            GATT -> oad : oadWriteAttrCB()

            activate oad
            oad -> OADQ : oadEnqueueMsg()
            oad -> app : Execute (*oadWriteCB_t)
            deactivate OAD
            deactivate GATT

            app -> oad : OAD_processQueue()
            oad -> OADQ : Queue_get()

            note over oad
                Process event
            end note
        end

        group
        @enduml


OAD State Machine
-----------------

The OAD service implements an 'OAD State Machine' for performing the OAD. The
following state machine depicts the OAD service state transitions and its
interactions with the OAD communication profile messages for both on-chip and
off-chip OAD.

.. _fig-mcuboot-oad-state-machine:
.. figure:: resources/oad_state_machine.png
    :align: center

    OAD Types Overview

The states and state transitions are encapsulated inside the OAD service, but
some of the critical states are described below to aide in understanding.

Note these sections refer to internal state handling and transitions local to
the target device. For a summary of the over the air sequence see
:ref:`fig-mcuboot-oad-sequence-diagram` and for a breakdown of the different types of
profile messages and how to interpret them over the air please see
:ref:`sect-mcuboot-oad-profile`.

Image Validation
""""""""""""""""

After establishing a new connection, updating the connection interval
for a faster OAD and enabling notifications of OAD Image Identify and
OAD Image Block characteristics on the OAD target, the
OAD distributor shall write to the Image Identify characteristic of the
OAD target. The message data will be the header retrieved from the OAD
Image available for OAD.

On receiving the `Image Identify` message, the OAD target will get ready
for OAD process. The image validation is done by secure bootloader.
That means, there is no image validation in the OAD application.

Image Block Transfers
"""""""""""""""""""""

Once the OAD target is ready for receiving image, it will switch to
the configuration state. There it will get the block size and set image count.
When the OAD distributor sends the Start OAD Command to the Control
Characteristic (for more details see
:ref:`tbl-mcuboot-oad-control-supported-commands`), the OAD target will respond
with a Control characteristic notification requesting the first block. The OAD
distributor will then send the first block to the OAD target.

This process continues with the OAD target notifying the OAD distributor
of the next block it needs and the OAD distributor sending the requested
image block until all blocks have been transferred.

Completion of the OAD Process
"""""""""""""""""""""""""""""

After receiving the complete image, OAD application will transit to
*OAD_COMPLETE* state and then trigger a reset. After reset the secure
bootloader will start the new image validation.