.. _gatt:

Generic Attribute Profile (GATT)
--------------------------------

Just as the GAP layer handles most connection-related functionality,
the GATT layer of the Bluetooth Low Energy protocol stack is used by
the application for data communication between two connected
devices. Data is passed and stored in the form of characteristics
which are stored in memory on the Bluetooth Low Energy device. From
a GATT standpoint, when two devices are connected they are each in
one of two roles.

-  The **GATT server**

      the device containing the characteristic
      database that is being read or written by a GATT client.

-  The **GATT client**

      the device that is reading or writing data
      from or to the GATT server.

:numref:`gatt_client_server` shows this relationship in a sample Bluetooth low
energy connection where the peripheral device (that is, a |LP|)
is the GATT server and the central device (that is, a smart phone) is the GATT
client.

.. _gatt_client_server:
.. figure:: resources/gatt_client_server.png
    :align: center

    GATT Client and Server Interaction Overview

The GATT roles of client and server are independent from the GAP
roles of peripheral and central. A peripheral can be either a GATT
client or a GATT server, and a central can be either a GATT client
or a GATT server. A peripheral can act as both a GATT client and a
GATT server. For a hands-on review of GATT services and
characteristics, see |SLA|.

GATT Characteristics and Attributes
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

While characteristics and attributes are sometimes used
interchangeably when referring to Bluetooth Low Energy, consider
characteristics as groups of information called attributes.
Attributes are the information actually transferred between devices.
Characteristics organize and use attributes as data values,
properties, and configuration information. A typical characteristic
is composed of the following attributes.

-  Characteristic Value

      data value of the characteristic

-  Characteristic Declaration

      descriptor storing the properties,
      location, and type of the characteristic value

-  Client Characteristic Configuration

      a configuration that allows the GATT server to
      configure the characteristic to be notified (send message
      asynchronously) or indicated (send message asynchronously
      with acknowledgment)

-  Characteristic User Description

      an ASCII string describing the characteristic

These attributes are stored in the GATT server in an attribute
table. In addition to the value, the following properties are
associated with each attribute.

-  Handle

      the index of the attribute in the table (Every attribute has
      a unique handle.)

-  Type

      indicates what the attribute data represents (referred to as a
      UUID [universal unique identifier]. Some of these are Bluetooth
      SIG-defined and some are custom.)

-  Permissions

      enforces if and how a GATT client device can access the
      value of an attribute

GATT Client Abstraction
^^^^^^^^^^^^^^^^^^^^^^^

Like the GAP layer, the GATT layer is also abstracted. This
abstraction depends on whether the device is acting as a GATT client
or a GATT server. As defined by the |CORESPEC|, the
GATT layer is an abstraction of the ATT layer.

GATT clients do not have attribute tables or profiles as they are
gathering, not serving, information. Most of the interfacing with
the GATT layer occurs directly from the application.

.. figure:: resources/gatt_client_abstract.jpg
    :align: center

    Visualization of GATT Client Abstraction.

.. _gatt_server_abstraction:

GATT Server Abstraction
^^^^^^^^^^^^^^^^^^^^^^^

As a GATT server, most of the GATT functionality is handled by the
individual GATT profiles. These profiles use the
GATTServApp ( see :ref:`ble_api_reference`, GATTServApp Section) (a
configurable module that stores and manages the attribute table).
:numref:`gatt_server_abstract` shows this abstraction hierarchy.

.. _gatt_server_abstract:

.. figure:: resources/gatt_server_abstract.jpg
    :align: center

    Visualization of GATT Server abstraction.

The design process involves creating GATT profiles that configure
the GATTServApp module and use its API to interface with the GATT
layer. In this case of a GATT server, direct calls to GATT layer
functions are unnecessary. The application then interfaces with the
profiles.


.. _gatt_services_and_profile:

GATT Services and Profile
^^^^^^^^^^^^^^^^^^^^^^^^^

A GATT service is a collection of characteristics. For example, the
heart rate service contains a heart rate measurement characteristic
and a body location characteristic, among others. Multiple services
can be grouped together to form a profile. Many profiles only
implement one service so the two terms are sometimes used
interchangeably.

.. note::
    TI intends this section as an introduction to the attribute
    table by using basic\_ble as an example. For information on how this
    profile is implemented within the stack, see :ref:`gatt_server_abstraction`.

There are four GATT profiles defined in the basic\_ble example
application project.

*  :ref:`gap_gatt_service`

      This service contains device and access information
      such as the device name, vendor identification, and product
      identification.

      The following characteristics are defined for this service:

      -  Device name
      -  Appearance
      -  Peripheral preferred connection parameters

      .. note::
         See the Gap Service and Characteristics for GATT Server section
         ([Vol. 3], Part C, Section 12) of the
         |CORESPEC| for more information on these characteristics.

*  Generic Attribute Service

      This service contains information about
      the GATT server, is a part of the Bluetooth Low Energy protocol
      stack, and is required for every GATT server device as per the
      |CORESPEC|.

*  Device Info Service

      This service exposes information about the
      device such as the hardware, software version, firmware version,
      regulatory information, compliance information, and manufacturer
      name. The Device Info Service is part of the Bluetooth Low Energy
      protocol stack and configured by the application.

*  Simple\_gatt\_profile Service

      This service is a sample profile for
      testing and for demonstration. The full source code is provided
      in the simple\_gatt\_profile.c and simple\_gatt\_profile.h files.

:numref:`sbp_attr_table` shows the attribute table in the basic\_ble project.

.. _sbp_attr_table:

.. figure:: resources/sbp_attr_table.jpg
    :align: center

    Simple GATT Profile Characteristic Table taken with BTool. Red indicates
    a Profile declaration, Yellow indicates character declaration, and White
    indicates Attributes related to a particular characteristic declaration.

The simple\_gatt\_profile contains the following characteristics:

*  SIMPLEGATTPROFILE\_CHAR1

      1-byte value that can be read or written from a GATT client device

*  SIMPLEGATTPROFILE\_CHAR2

      1-byte value that can be read from a GATT client device but cannot be
      written

*  SIMPLEGATTPROFILE\_CHAR3

      1-byte value that can be written from a GATT client device but cannot be
      read

*  SIMPLEGATTPROFILE\_CHAR4

      1-byte value that cannot be directly read or written from a GATT client
      device (This value is notifiable: This value can be configured for
      notifications to be sent to a GATT client device.)

*  SIMPLEGATTPROFILE\_CHAR5

      5-byte value that can be read (but not written) from a GATT client device

The following is a line-by-line description of the simple profile attribute
table, referenced by the following handle.

*  0x001C is the **simple\_gatt\_profile service declaration**.

      This declaration has a UUID of 0x2800 (Bluetooth-defined
      ``GATT_PRIMARY_SERVICE_UUID``). The value of this declaration is
      the UUID of the simple\_gatt\_profile (custom-defined).

*  0x001D is the **SimpleProfileChar1 characteristic declaration**.

      This declaration can be thought of as a pointer to the
      SimpleProfileChar1 value. The declaration has a UUID of 0x2803
      (Bluetooth-defined ``GATT_CHARACTER_UUID``). The value of the
      declaration characteristic, as well as all other characteristic
      declarations, is a 5-byte value explained here (from MSB to LSB):

      *  Byte 0 is the properties of the SimpleProfileChar1 as defined in the
         |CORESPEC| (The following are some of the relevant
         properties.)

         -  0x02: permits reads of the characteristic value

         -  0x04: permits writes of the characteristic value (without a response)

         -  0x08: permits writes of the characteristic value (with a response)

         -  0x10: permits of notifications of the characteristic value (without
            acknowledgment)

         -  0x20: permits notifications of the characteristic value (with
            acknowledgment)

      The value of 0x0A means the characteristic is readable (0x02) and
      writeable (0x08).

      *  Bytes 1-2: the byte-reversed handle where the SimpleProfileChar1's
         value is (handle 0x001E)

      *  Bytes 3-4: the UUID of the SimpleProfileChar1 value (custom-defined
         0xFFF1)

*  0x001E is the SimpleProfileChar1 Characteristic Value

      This value has a UUID of
      0xFFF1 (custom-defined). This value is the actual payload data of
      the characteristic. As indicated by its characteristic
      declaration (handle 0x01D), this value is readable and
      writable.

*  0x001F is the SimpleProfileChar1 Characteristic User Description

      This description has a UUID of 0x2901 (Bluetooth-defined). The value of
      this description is a user-readable string describing the characteristic.

*  0x0020 - 0x002C

      are attributes that follow the same structure as the simpleProfileChar1
      described previously with regard to the remaining four characteristics.
      The only different attribute, handle 0x0028, is described as follows.

      **0x0028 is the SimpleProfileChar4 Client Characteristic Configuration**.
      This configuration has a UUID of 0x2902 (Bluetooth-defined). By
      writing to this attribute, a GATT server can configure the
      SimpleProfileChar4 for notifications (writing 0x0001) or
      indications (writing 0x0002). Writing 0x0000 to this attribute
      disable notifications and indications.

GATT Security
^^^^^^^^^^^^^

As described in :ref:`gatt_server_abstraction`, the GATT server may define
permissions independently for each characteristic. The server may
allow some characteristics to be accessed by any client, while
limiting access to other characteristics to only authenticated or
authorized clients. These permissions are usually defined as part of
a higher level profile specification. For custom profiles, the user
may select the permissions as they see fit. For more information
about the GATT Security, refer to the Security Considerations section
([Vol 3], Part G, Section 8) of the |CORESPEC|.

Authentication
""""""""""""""

Characteristics that require authentication cannot be accessed until
the client has gone through an authenticated pairing method. This
verification is performed within the stack, with no processing
required by the application. The only requirement is for the
characteristic to be registered properly with the GATT server.

For example, characteristic 5 of the simple\_gatt\_profile allows on
authenticated reads.

.. code-block:: c

   // Characteristic Value 5
   GATT_BT_ATT( simpleGattProfile_char5UUID, GATT_PERMIT_AUTHEN_READ, simpleGattProfile_Char5 ),

When an un-authenticated client attempts to read this value, the GATT
server automatically rejects it with ``ERROR_INSUFFICIENT_AUTHEN (0x41)``,
without invoking the simpleProfile\_ReadAttrCB(). See an example of this
in :ref:`gatt_sniffer_capture`.

.. _gatt_sniffer_capture:
.. figure:: resources/image134.jpeg
    :align: center

    Sniffer Capture Example

After the client has successfully authenticated, read/write requests
are forwarded to the profiles read/write callback. See the code
below for a simple\_gatt\_profile example:

.. code-block:: c

    case SIMPLEGATTPROFILE_CHAR5_UUID:
        *pLen = SIMPLEGATTPROFILE_CHAR5_LEN;
        VOID memcpy( pValue, pAttr->pValue, SIMPLEGATTPROFILE_CHAR5_LEN );
        break;


Authorization
"""""""""""""

Authorization is a layer of security provided in addition to what
BLE already implements. Because applications are required to define
their own requirements for authorization, the stack forwards
read/write requests on these characteristics to the application
layer of the profile.

For the profile to register for authorization information from the
GATT server, it must define an authorization callback with the
stack. The simple\_gatt\_profile does not do this by default, but
below is an example of how it could be modified to do this.

1. Register profile level authorization callback.

.. code-block:: c

   CONST gattServiceCBs_t simpleProfileCBs =
   {
      simpleProfile_ReadAttrCB,      // Read callback function pointer
      simpleProfile_WriteAttrCB,     // Write callback function pointer
      simpleProfile_authorizationCB  // Authorization callback function pointer
   };

2. Implement authorization callback code.

.. code-block:: c

   static bStatus_t simpleProfile_authorizationCB( uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode )
   {
      //This is just an example implementation, normal use cases would require
      //more complex logic to determine that the device is authorized

      if(clientIsAuthorized)
         return SUCCESS;
      else
         return ATT_ERR_INSUFFICIENT_AUTHOR;
   }

The authorization callback executes in the stack context, thus
intensive processing should not be performed in this function. The
implementation is left up to the developer; the above callback
should be treated as a shell. The return value should be either
``SUCCESS`` if the client is authorized to access the characteristic, or
``ATT_ERR_INSUFFICIENT_AUTHOR`` if they have not yet obtained proper
authorization. Authorization requires the connection to be authenticated
beforehand, or ``ATT_ERR_INSUFFICIENT_AUTHEN`` will be sent as an error
response.

If a characteristic that requires authorization is registered with
the GATT server, but no application level authorization callback is
defined, the stack will return ``ATT_ERR_UNLIKELY``. Because this
error can be cryptic, TI recommends using an authorization callback.

.. _using_the_gatt_layer_directly:

Using the GATT Layer Directly
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

This section describes how to use the GATT layer in an application.
The functionality of the GATT layer is implemented in the library
but header functions can be found in the gatt.h file.
The :ref:`ble_api_reference` within the ATT/GATT section has
the complete API for the GATT layer. The |CORESPEC|
provides more information on the functionality of these commands. These
functions are used primarily for GATT client applications. A few server-specific
functions are described in the API. Most of the GATT functions
returns ATT events to the application, review :ref:`ble_api_reference` for details.

The general procedure to use the GATT layer when functioning as a GATT client
is as follows:

.. _cd_gatt_att_write_rsp_event:
.. uml::
    :caption: Context Diagram of Application using GATT layer.
    :align: center

    @startuml
    participant "Application" as App
    participant ICALL
    participant "BLE Stack"


    App->ICALL: VOID GATT_InitClient(); \nInitialize Client
    App->ICALL: GATT_RegisterForInd(selfEntity); \nRegister to receive incoming \nATT Indications or Notification

    App->ICALL: GATT_WriteCharValue(connHandle,\n&req, selfEntity);

    activate ICALL

      rnote over "ICALL"
      Translate into ATT function
      and send it to the BLE stack
      end note

    ICALL->"BLE Stack" : ATT_WriteReq
    Deactivate "ICALL"

    group Invalid Write Req
      "BLE Stack"-> ICALL : return(INVALIDPARAMETER)
      ICALL-> App : return(INVALIDPARAMETER)
    end

    group Valid Write Req
      "BLE Stack"-->]: Send ATT_WRITE_REQ

      "BLE Stack"-->ICALL : return(SUCCESS)
      ICALL-->App : return(SUCCESS)
      ...
      ... Wait for the server to respond ...
      ...
      "BLE Stack"<--]: Receive ATT_WRITE_RSP\nor ATT_ERROR_RSP

    "BLE Stack"->ICALL: Parse the msg

    activate ICALL

    ICALL->App : Notify application
    deactivate "ICALL"

    App->App: BLEAppUtil_processStackMsgCB

    App->App: BLEAppUtil_processGATTEvents
    end

    @enduml

.. note::
    Even though the event sent to the application is an ATT
    event, it is sent as a GATT protocol stack message
    (``GATT_MSG_EVENT``).

.. note::
    In addition to receiving responses to its own commands, a GATT client may
    also receive asynchronous data from the GATT server as indications or
    notifications. Use (``GATT_RegisterForInd(selfEntity)``) to receive these
    ATT notifications and indications. These notifications and indications are
    also sent as ATT events (``ATT_HANDLE_VALUE_NOTI`` &
    ``ATT_HANDLE_VALUE_IND``) in GATT messages to the application. These events
    must be handled as described in :ref:`gatt_services_and_profile`.

.. _maximum-transmission-unit-mtu:

Maximum Transmission Unit (MTU)
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The size of the L2CAP PDU also defines the size of the Attribute
Protocol Maximum Transmission Unit (``ATT_MTU``). See :ref:`l2cap-mtu` for more
information about L2CAP MTU settings and how it interacts with GATT/ATT.

By default, LE devices assume the size of the L2CAP PDU is 27 bytes, which
corresponds to the maximum size of the LE packet that can transmit
in a single connection event packet. The L2CAP protocol header for a B-frame
is 4 bytes, resulting in a default size for ``ATT_MTU`` of 23. See
:ref:`l2cap-frames` for more information.

.. note::
   When using the LE Data Length Extension feature, the
   length of the LE packet can be up to 251 bytes. See
   :ref:`le_data_length_extension`

.. _configuring_for_larger_MTU_values:

Configuring for Larger MTU Values
"""""""""""""""""""""""""""""""""

A client device can request a larger ``ATT_MTU`` during a connection by
using the :ble_api:`GATT_ExchangeMTU` command.
During this procedure, the client informs the server of its maximum
supported receive MTU size and the server responds with its maximum supported
receive MTU size. Only the client can initiate this procedure. When
the messages are exchanged, the ``ATT_MTU`` for the duration of the
connection is the minimum of the client MTU and server MTU values.
If the client indicates it can support an MTU of 200 bytes and the
server responds with a maximum size of 150 bytes, the ``ATT_MTU`` size
is 150 for that connection.

For more information, see the MTU Exchange section of the |CORESPEC|.

Take the following steps to configure the stack to support larger
MTU values.

1. Set the ``MAX_PDU_SIZE`` preprocessor symbol in the application project
   to the desired value to the maximum desired
   size of the L2CAP PDU size. The maximum is set by the following equation
   ``ATT_MTU=MAX_PDU_SIZE-L2CAP_HDR_SIZE``


2. Call :ble_api:`GATT_ExchangeMTU` after a connection is formed (GATT client
   only). The MTU parameter passed into this function must be less
   than or equal to the definition from step 1.

3. Receive the ``ATT_MTU_UPDATED_EVENT`` in the calling task to verify
   that the MTU was successfully updated. This update requires the
   calling task to have registered for GATT messages.
   See :ref:`registering_to_receive_additional_gatt_events_in_the_application`
   for more information.

Though the stack can be configured to support a ``MAX_PDU_SIZE`` up to
255 bytes, each Bluetooth Low Energy connection initially uses the
default 27 bytes (``ATT_MTU`` = 23 bytes) value until the exchange MTU
procedure results in a larger MTU size. The exchange MTU procedure
must be performed on each Bluetooth Low Energy connection and must
be initiated by the client.

.. note::
    If the Secure Connections BLE 4.2 Feature is enabled,
    the local device will support an MTU of 65 by default. This is required
    by LE Secure Connections. Remember that that the actual resulting MTU
    must still be negotiated via MTU exchange procedure using
    ``GATT_ExchangeMTU``. All connections will begin with a default MTU of 23
    bytes.

    See ``ble_user_config.h`` for details.

Increasing the size of the ``ATT_MTU`` increases the amount of data
that can be sent in a single ATT packet. The longest attribute that
can be sent in a single packet is (``ATT_MTU``-1) bytes. Procedures,
such as notifications, have additional length restrictions. If an
attribute value has a length of 100 bytes, a read of this entire
attribute requires a read request to obtain the first (``ATT_MTU``-1)
bytes, followed by multiple read blob request to obtain the
subsequent (``ATT_MTU``-1) bytes. To transfer the entire 100 bytes of
payload data with the default ``ATT_MTU`` = 23 bytes, five request or
response procedures are required, each returning 22 bytes. If the
exchange MTU procedure was performed and an ``ATT_MTU`` was configured
to 101 bytes (or greater), the entire 100 bytes could be read in a
single read request or response procedure.

.. note::
   Due to memory and processing limitations, not all
   Bluetooth Low Energy systems support larger MTU sizes. Know the
   capabilities of expected peer devices when defining the behavior of
   the system. If the capability of peer devices is unknown, design the
   system to work with the default 27-byte L2CAP PDU/23-byte ``ATT_MTU``
   size. For example, sending notifications with a length greater than
   20 bytes (``ATT_MTU``-3) bytes results in truncation of data on devices
   that do not support larger MTU sizes.

.. _gap_gatt_service:

GAP GATT Service (GGS)
----------------------

The GAP GATT Service (GGS) is required for Bluetooth low-energy devices that
implement the **central** or **peripheral** GAP role. Multirole devices that
implement either of these roles **must** also contain the GGS. The
purpose of the GGS is to aid in the device discovery and the connection
initiation process.

.. note::
    For more information about the GGS, refer to the GAP Service and
    and Characteristics for GATT Server section ([Vol 3], Part C, Section 12)
    of the |CORESPEC|.

Using the GGS
^^^^^^^^^^^^^

The GAP GATT Service is implemented as part of the Bluetooth Low Energy library
code and the related APIs are found in ``GATTServApp`` and ``ATT_GATT``
sections in :ref:`ble_api_reference`.

This section describes what the application must do to configure,
start, and use the GAP Gatt Service.

1. **Include the header file**.

.. code-block:: c

   #include "gapgattserver.h"

2. **Initialize the GGS parameters.** Code snippet example from *simple peripheral*.

.. code-block:: c
  :caption: **ble_stack_api.c :: bleStack_initGatt()** - Initialize the GGS parameters.
  :linenos:

   // GAP GATT Attributes
   static uint8_t attDeviceName[GAP_DEVICE_NAME_LEN] = "Simple BLE Peripheral";

   GGS_SetParameter(GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN, attDeviceName);

3. **Initialize the application callbacks with GGS** (optional). This notifies the
   application when any of the characteristics in the GGS have changed.

.. code-block:: c

   GGS_RegisterAppCBs(&appGGSCBs);

4. **Add the GGS to the GATT server.**

.. code-block:: c
  :caption: **ble_stack_api.c :: bleStack_initGatt()** - Add GGS to the GATT server.

   bStatus_t GGS_AddService(GATT_ALL_SERVICES);

Generic Attribute Profile Service (GATT Service)
------------------------------------------------

The Generic Attribute Profile (GATT) Service provides information
about the GATT services registered with a device.

.. note::
      For more information on the GATT Service, refer to the Defined Generic
      Attribute Profile Service section ([Vol 3], Part G, Section 7) of the
      |CORESPEC|.

The service changed characteristic is used to inform bonded devices
that services have changed on the server upon reconnection. Service
changed updates are sent in the form of GATT indications, and the
service changed characteristic is not writeable or readable. In the
TI Bluetooth Low Energy stack, the service changed characteristic is
implemented as part of the gattservapp, which is part of library
code.

Per the |CORESPEC|, it is safe for server
devices whose characteristic tables do not change over their
lifetime to exclude the service changed characteristic. Support for
indications from this characteristic must be supported on GATT
client devices.

.. _sec-gatt-coc:

Using the GATT Service
^^^^^^^^^^^^^^^^^^^^^^

This section describes what the user must do to enable the GATT
service changed feature in the Bluetooth Low Energy stack. Once the
service changed feature is enabled, the GAPBondMgr will handle
sending the service changed indication to clients who have enabled
it using the CCCD.

1. Use a supported build config for the stack; only stack libraries with
   v4.1 features and L2CAP connection-oriented channels will support
   the service changed characteristic.

   Enable this feature by enabling the option "L2CAP Connection Oriented 
   Channels" in SysConfig. The "L2CAP Connection Oriented Channels" option has 
   to be enabled in the "BLE" menu of SysConfig. 

2. From this point, the GAPBondMgr handles sending an indication to
   connected clients when the service has changed and the CCCD is
   enabled. If the feature is enabled, the peripheral role invokes
   the necessary APIs to send the indication through the GAPBondMgr.

3. On the client side, service changed indications can be registered
   using the same method as registering for other indications.

.. _gattservapp_module:

GATTServApp Module
------------------

The GATT Server Application (GATTServApp) stores and manages the 
application-wide attribute table. Various profiles use this module to add their 
characteristics to the attribute table. The Bluetooth Low Energy stack uses this
module to respond to discovery requests from a GATT client. For
example, a GATT client may send a **Discover all Primary
Characteristics** message. The Bluetooth Low Energy stack on the GATT
server side receives this message and uses the GATTServApp to find and
send over-the-air all of the primary characteristics stored in the
attribute table. This type of functionality is beyond the scope of
this document and is implemented in the library code. The
GATTServApp functions accessible from the profiles are defined in
''gattservapp\_util.c'' and the API described in :ref:`ble_api_reference`
(GATTServApp section).
These functions include finding specific attributes and reading or modifying
client characteristic configurations. See :numref:`gatt_att_table_init` for an
example of how GATTServApp functions in an application.


.. _gatt_att_table_init:
.. uml::
    :caption: Attribute Table Initialization Diagram.
    :align: center

    @startuml

    participant App.c
    participant "Profile A"
    participant "Profile B"
    participant GATTServApp
    participant "GATT Server"

    rnote over "Profile A", "Profile B"
      Service A and Service B
      Table initialization
    end note

    App.c -> "GATT Server" : GGS_AddService()

    note right
      GAP Service
    end note

    group Add GATTServApp to attribute table
        App.c -> GATTServApp : GATTServApp_AddService()
        GATTServApp -> "GATT Server" : RegisterService

        note right
          GAP Service
          GATT Service
        end note
    end

    App.c -> "Profile A" : ProfileA_AddService()
    "Profile A" -> GATTServApp : RegisterService(A)


    GATTServApp -> "GATT Server" : RegisterService

    note right
      GAP Service
      GATT Service
      Service A
    end note

    deactivate GATTServApp
    deactivate "Profile A"


    == Profile B ==


    App.c -> "Profile B" : ProfileB_AddService()
    "Profile B" -> GATTServApp : RegisterService(B)
    GATTServApp -> "GATT Server" : RegisterService


    note right
      GAP Service
      GATT Service
      Service A
      Service B
    end note
    @enduml


Building up the Attribute Table
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

Upon power-on or reset, the application builds the GATT table by
using the GATTServApp to add services. Each service consists of a
list of attributes with UUIDs, values, permissions, and read and
write call-backs. As :numref:`gatt_att_table_init` shows, all of this
information is passed through the GATTServApp to GATT and stored in the stack.

Attribute table initialization must occur in the application
initialization function, that is, bleStack\_initGatt().

.. code-block:: c

   // Initialize GATT attributes
   GGS_AddService(GATT_ALL_SERVICES);         // GAP
   GATTServApp_AddService(GATT_ALL_SERVICES); // GATT attributes

Implementing Profiles in Attributes Table
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

This section describes the general architecture for implementing profiles and
provides specific functional examples in relation to the
simple\_gatt\_profile in the basic\_ble project. See
:ref:`gatt_services_and_profile` for an overview of the simple\_gatt\_profile.

Attribute Table Definition
""""""""""""""""""""""""""

Each service or group of GATT attributes must define a fixed size
attribute table that gets passed into GATT. This table in
simple\_gatt\_profile.c is defined as the following.

.. code-block:: c

   static gattAttribute_t simpleProfileAttrTbl[SERVAPP_NUM_ATTR_SUPPORTED]

Each attribute in this table is of the following type.

.. code-block:: c

   typedef struct attAttribute_t
   {
      gattAttrType_t type; //!< Attribute type (2 or 16 octet UUIDs)
      uint8 permissions; //!< Attribute permissions

      uint16 handle; //!< Attribute handle - assigned internally by attribute server

      uint8* const pValue; //!< Attribute value - encoding of the octet array is defined in
                           //!< the applicable profile. The maximum length of an attribute
                           //!< value shall be 512 octets.
   } gattAttribute_t;

When utilizing gattAttribute_t, the various fields have specific meanings.

* gattAttrType_t type

      type is the UUID associated with the attribute being placed into the table. gattAttrType_t itself is defined as:

      .. code-block:: c

         typedef struct
         {
            uint8 len;         //!< Length of UUID (2 or 16)
            const uint8 *uuid; //!<Pointer to UUID
         } gattAttrType_t;

      Where length can be either ``ATT_BT_UUID_SIZE`` (2 bytes), or
      ``ATT_UUID_SIZE`` (16 bytes). The \*uuid is a pointer to a number either
      reserved by Bluetooth SIG (defined in gatt\_uuid.c) or a custom UUID
      defined in the profile.

* uint8 permissions

      enforces how and if a GATT client device can access the
      value of the attribute. Possible permissions are defined in
      gatt.h as follows:

      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_READ             |    0x01    |     //!< Attribute is Readable           |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_WRITE            |    0x02    |     //!< Attribute is Writable           |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_AUTHEN\_READ     |    0x04    |     //!< Read requires Authentication    |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_AUTHEN\_WRITE    |    0x08    |     //!< Write requires Authentication   |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_AUTHOR\_READ     |    0x10    |     //!< Read requires Authorization     |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_AUTHOR\_WRITE    |    0x20    |     //!< Write requires Authorization    |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_ENCRYPT\_READ    |    0x40    |     //!< Read requires Encryption        |
      +----------------------------------------+------------+------------------------------------------+
      | #define GATT\_PERMIT\_ENCRYPT\_WRITE   |    0x80    |     //!< Write requires Encryption       |
      +----------------------------------------+------------+------------------------------------------+

      :ref:`allocating_memory_for_gatt_procedures` further describes authentication, authorization, and encryption.

* uint16 handle

      handle is a placeholder in the table where GATTServApp assigns a
      handle. This placeholder is not customizable. Handles are
      assigned sequentially.

* uint8* const pValue

      pValue is a pointer to the attribute value. The size is unable to
      change after initialization. The maximum size is 512 octets.

Service Declaration
"""""""""""""""""""

Consider the following simple\_gatt\_profile service declaration
attribute:

.. code-block:: c

   // Simple Profile Service
   GATT_BT_ATT( primaryServiceUUID, GATT_PERMIT_READ, (uint8 *) &simpleGattProfile_Service ),

The type is set to the Bluetooth SIG-defined primary service UUID
(0x2800). A GATT client is permitted to read this service with the permission
is set to ``GATT_PERMIT_READ``. The pValue is a pointer to the UUID of
the service, custom-defined as 0xFFF0. SimpleProfileService itself is defined to
reference the profile's UUID.

.. code-block:: c

   // Simple GATT Profile Service attribute
   static CONST gattAttrType_t simpleGattProfile_Service = { ATT_BT_UUID_SIZE, simpleGattProfile_ServUUID };

Characteristic Declaration
""""""""""""""""""""""""""

Consider the following simple\_gatt\_profile
simpleProfileCharacteristic1 declaration.

.. code-block:: c

   // Characteristic 1 Declaration
   GATT_BT_ATT( characterUUID, GATT_PERMIT_READ, &simpleGattProfile_Char1Props ),

The type is set to the Bluetooth SIG-defined characteristic UUID
(0x2803). This makes simpleProfileCharacteristic1 read only to the GATT client
with the permissions set to ``GATT_PERMIT_READ``.

For functional purposes, the only information required to be passed
to the GATTServApp in pValue is a pointer to the properties of the
characteristic value. The GATTServApp adds the UUID and the handle
of the value. These properties are defined to allow this particular
characteristic in this service to be read and written to.

.. code-block:: c

   // Simple GATT Profile Characteristic 1 Properties
   static uint8 simpleGattProfile_Char1Props = GATT_PROP_READ | GATT_PROP_WRITE;

.. note::
   An important distinction exists between these properties
   and the GATT permissions of the characteristic value. These
   properties are visible to the GATT client stating the properties of
   the characteristic value. The GATT permissions of the characteristic
   value affect its functionality in the protocol stack. These
   properties must match that of the GATT permissions of the
   characteristic value.

Characteristic Value
""""""""""""""""""""

Consider the simple\_gatt\_profile simpleProfileCharacteristic1
value.

.. code-block:: c

   // Characteristic Value 1
   GATT_BT_ATT( simpleGattProfile_char1UUID, GATT_PERMIT_READ | GATT_PERMIT_WRITE, &simpleGattProfile_Char1 ),

The type is set to the custom-defined simpleProfilechar1 UUID
(0xFFF1). The properties of the characteristic value in the attribute
table must match the properties from the characteristic value
declaration. The pValue is a pointer to the location of the actual
value, statically defined in the profile as follows.

.. code-block:: c

  // Characteristic 1 Value
  static uint8 simpleGattProfile_Char1 = 0;

.. _client_characteristic_configuration:

Client Characteristic Configuration
"""""""""""""""""""""""""""""""""""

Consider the simple\_gatt\_profile simpleProfileCharacteristic4
configuration.

.. code-block:: c

  // Characteristic 4 configuration
   GATT_BT_ATT( clientCharCfgUUID, GATT_PERMIT_READ | GATT_PERMIT_WRITE, (uint8 *) &simpleGattProfile_Char4Config ),

The type is set to the Bluetooth SIG-defined client characteristic
configuration UUID (0x2902) GATT clients must read and write to this
attribute so the GATT permissions are set to readable and writable.
The pValue is a pointer to the location of the client characteristic
configuration array, defined in the profile as follows.

.. _sgp_characteristic_4_pvalue:
.. code-block:: c
  :caption: simple\_gatt\_profile characteristic 4 pValue pointer define.
  :linenos:

  static gattCharCfg_t *simpleGattProfile_Char4Config;

.. note::
   Client characteristic configuration is represented as an
   array because this value must be cached for each connection. The
   catching of the client characteristic configuration is described in
   more detail in :ref:`gatt_add_service_function`.

.. _gatt_add_service_function:

Add Service Function
^^^^^^^^^^^^^^^^^^^^

As described in :ref:`gattservapp_module`, when an application starts up it
requires adding the GATT services it supports. Each profile needs a
global AddService function that can be called from the application.
Some of these services are defined in the protocol stack, such as
GAP GATT Service and GATT Service. User-defined services must expose
their own AddService function that the application can call for
profile initialization. Using SimpleGattProfile\_addService() as an
example, these functions should do as follows.

-  Allocate space for the client characteristic configuration (CCC)
   arrays. As an example, a pointer to one of these arrays was
   initialized in the profile as described in
   ref:`client_characteristic_configuration`.

   In the AddService function, the supported connections is declared and memory
   is allocated for each array. Only one CCC is defined in the
   simple\_gatt\_profile but there can be multiple CCCs.

.. code-block:: c

    // Allocate Client Characteristic Configuration table
    simpleGattProfile_Char4Config = (gattCharCfg_t *)ICall_malloc( sizeof( gattCharCfg_t ) * MAX_NUM_BLE_CONNS );
    if ( simpleGattProfile_Char4Config == NULL )
    {
      return ( bleMemAllocError );
    }

-  Initialize the CCC arrays. CCC values are persistent between power
   downs and between bonded device connections. For each CCC in the
   profile, the :ble_api:`GATTServApp_InitCharCfg` function must be called.
   This function tries to initialize the CCCs with information from
   a previously bonded connection and set the initial values to
   default values if not found.

.. code-block:: c

   GATTServApp_InitCharCfg( LINKDB_CONNHANDLE_INVALID, simpleGattProfile_Char4Config );

-  Register the profile with the GATTServApp. This function passes the
   attribute table of the profile to the GATTServApp so that the
   attributes of the profile are added to the application-wide
   attribute table managed by the protocol stack and handles are
   assigned for each attribute. This also passes pointers to the
   callbacks of the profile to the stack to initiate communication
   between the GATTServApp and the profile.

.. code-block:: c

  // Register GATT attribute list and CBs with GATT Server App
  status = GATTServApp_RegisterService( simpleGattProfile_attrTbl,
                                        GATT_NUM_ATTRS( simpleGattProfile_attrTbl ),
                                        GATT_MAX_ENCRYPT_KEY_SIZE,
                                        &simpleGattProfile_CBs );

Register Application Callback Function
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

Profiles can relay messages to the application using callbacks. In
the basic\_ble project, the simple\_gatt\_profile calls an
application callback whenever the GATT client writes a
characteristic value. For these application callbacks to be used,
the profile must define a Register Application Callback function
that the application uses to set up callbacks during its
initialization. The register application callback function for the
simple\_gatt\_profile is the following:

.. _sgp_client_configuration_register_app_cb:
.. code-block:: c
   :caption: Register application callbacks.
   :linenos:

   bStatus_t SimpleGattProfile_registerAppCBs( SimpleGattProfile_CBs_t *appCallbacks )
   {
     if ( appCallbacks )
     {
       simpleGattProfile_appCBs = appCallbacks;

       return ( SUCCESS );
     }
     else
     {
       return ( bleAlreadyInRequestedMode );
     }
   }

Where the callback typedef is defined as the following.

.. code-block:: c

   typedef struct
   {
     pfnSimpleGattProfile_Change_t pfnSimpleGattProfile_Change;  // Called when characteristic value changes
   } SimpleGattProfile_CBs_t;

The application must then define a callback of this type and pass it
to the simple\_gatt\_profile with the
SimpleGattProfile\registerAppCBs() function. This occurs in
app\_simple\_gatt.c as follows.

.. code-block:: c

   // Simple GATT Profile Callbacks
   static SimpleGattProfile_CBs_t simpleGatt_profileCBs =
   {
      SimpleGatt_changeCB // Simple GATT Characteristic value change callback
   };

   //...

   // Register callback with SimpleGATTprofile
   status = SimpleGattProfile_registerAppCBs( &simpleGatt_profileCBs );

See :ref:`read_and_write_callback_functions` for further information on how this
callback is used.

.. _read_and_write_callback_functions:

Read and Write Callback Functions
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The profile must define Read and Write callback functions which the
protocol stack calls when one of the attributes of the profile are
written to or read from. The callbacks must be registered with
GATTServApp as mentioned in :ref:`gatt_add_service_function`. These callbacks
perform the characteristic read or write and other processing (possibly calling
an application callback) as defined by the specific profile.

Read Request from Client
^^^^^^^^^^^^^^^^^^^^^^^^

When a read request from a GATT Client is received for a given
attribute, the protocol stack checks the permissions of the
attribute and, if the attribute is readable, calls the read call-back
profile. The profile copies in the value, performs any
profile-specific processing, and notifies the application if
desired. This procedure is illustrated in :numref:`gatt_read_cb_flow_fig` for a read
of simpleGattProfile\_Char1 in the simple\_gatt\_profile.


.. _gatt_read_cb_flow_fig:
.. uml::
  :caption: Read Request illustration
  :align: center

   @startuml
    participant "Service CB \n(simple_gatt_profile.c)" as App
    participant GATTServApp
    participant "BLE Stack"  as BLE

    BLE <--]: Receive Attribute Read Request

    BLE -> GATTServApp : GATT_MSG_EVENT

    Activate "GATTServApp"
     GATTServApp -> GATTServApp : Process Event
     GATTServApp -> GATTServApp : Process Msg "ATT Read Req"

    group status != SUCCESS
      GATTServApp -> BLE : ATT_ErrorRsp
      Deactivate "GATTServApp"
      BLE -->] : Send ATT_ERROR_RSP
    end


    group status == SUCCESS
      GATTServApp -> App : Find Attribute CB
      App -> App : SimpleGattProfile_readAttrCB
      rnote over "App"
        Copy the values
      end note
      App -> GATTServApp
      GATTServApp -> BLE : ATT_ReadRsp
      BLE -->] : ATT_READ_RSP
    end

   @enduml



The processing is in the context of the protocol stack. If any
intensive profile-related processing that must be done in the case
of an attribute read, this should be split up and done in the
context of the Application task. See the :ref:`write_request_from_client` for
more information.

.. note:: If desired, the GATT server may choose to delay the handling of the
          ATT_ReadReq and return a blePending response.    A user-defined service can call
          GATTServApp_ReadRsp() to send the response to the GATT server as soon as the
          data becomes available.     See the :ref:`delaying_an_att_read_request` for more
          information.

.. _write_request_from_client:

Write Request from Client
^^^^^^^^^^^^^^^^^^^^^^^^^

When a write request from a GATT client is received for a given
attribute, the protocol stack checks the permissions of the
attribute and, if the attribute is write-permitted, calls the write callback of
the profile. The profile stores the value to be written, performs
any profile-specific processing, and notifies the application if
desired. :numref:`gatt_write_cb_flow_fig` shows this procedure for a write
of simpleGattProfile\_Char3 in the simple\_gatt\_profile.

.. _gatt_write_cb_flow_fig:
.. uml::
  :caption: Write Request illustration
  :align: center

   @startuml
    participant "User Define Post Processing" as User
    participant "Service CB \n(simple_gatt_profile.c)" as App
    participant GATTServApp
    participant "BLE Stack"  as BLE

    BLE <--]: Receive Attribute Write Request

    BLE -> GATTServApp : GATT_MSG_EVENT

    Activate "GATTServApp"
     GATTServApp -> GATTServApp : Process Event
     GATTServApp -> GATTServApp : Process Msg "ATT Write Req"

    group status != SUCCESS
      GATTServApp -> BLE : ATT_ErrorRsp
      Deactivate "GATTServApp"
      BLE -->] : Send ATT_ERROR_RSP
    end


    group status == SUCCESS
      GATTServApp -> App : Find Attribute CB
      App -> App : SimpleGattProfile_writeAttrCB
      rnote over "App"
                         update the value
                                     &
        find user defined application callback
      end note

      GATTServApp -> BLE : ATT_WriteRsp
      BLE -->] : ATT_Write_RSP

      App -> App : SimpleGattProfile_callback()

      App -> App : BLEAppUtil_invokeFunction()
      
      App-> User : SimpleGatt_changeCB()
    end



   @enduml


.. important::
    Minimizing the processing in protocol stack context is
    important. In this example, additional processing beyond storing the
    attribute write value in the profile occurs in the application context by enqueuing a message in the
    queue of the application.

.. _gatt_get_and_set_functions:

Get and Set Functions
^^^^^^^^^^^^^^^^^^^^^

The profile containing the characteristics shall provide set and get
abstraction functions for the application to read and write a
characteristic of the profile. The set parameter function also
includes logic to check for and implement notifications and
indications if the relevant characteristic has notify or indicate
properties. :numref:`gatt_get_set_pp` and the following code show this example
for setting simpleGattProfile\_Char4 in the simple\_gatt\_profile.

.. _gatt_get_set_pp:
.. uml::
  :caption: Set Profile Parameter
  :align: center

   @startuml
    participant App
    participant "Profile \n(simple_gatt_profile.c)" as profile
    participant GATTServApp
    participant "BLE Stack"  as BLE

    App -> profile : SetParameter(param, len, value)

    group Invalid operation
      profile -> App : return(bleInvalidRange|\nINVALIDPARAMETER)
    end note


    group Valid operation (correct len etc)

    rnote over "profile"
      Copy and update the values
    end note
    profile -> GATTServApp : GATTServApp_ProcessCharCfg()

    rnote over "GATTServApp"
      Check if the notification has
      already been enabled
    end note

    group Notification is not enabled
      GATTServApp -> profile : return(SUCCESS)
      profile -> App : return(SUCCESS)
    end


    group Notification is enabled
      GATTServApp -> BLE : GATT_Notification()
      BLE -->]: Send notification to client
      BLE->GATTServApp : return(status)
      GATTServApp -> profile : return(status)
      profile -> App : return(SUCCESS)
    end

    end note


   @enduml


For example, the application initializes
simpleGattProfile\_Char4 to 0 in app\_simple\_gatt.c through
the following.

.. code-block:: c

    uint8_t charValue4 = 4;
    SimpleGattProfile_setParameter( SIMPLEGATTPROFILE_CHAR4, sizeof(uint8_t),
                                    &charValue4 );

The code for this function is displayed in the following code
snippet (from simple\_gatt\_profile.c). Besides setting the value of
the static simpleGattProfile\_Char4, this function also calls
:ble_api:`GATTServApp_ProcessCharCfg` because it has notify properties. This
action forces GATTServApp to check if notifications have been
enabled by the GATT Client. If so, the GATTServApp sends a
notification of this attribute to the GATT Client. 
.. Add when feature is public
.. If a notification
.. fails to transmit, then retransmissions may be attempted.
.. Retransmissions for failed notifications can be enabled via the GATT_RetransLimitEnable
.. API. The number of retransmissions can be configured by the user through the GATT_SetupRetrans
.. API.

.. _simpleprofilecharacteristic4_setparameter:
.. code-block:: c
  :caption: Set characteristic 4 in SimpleGattProfile\_setParameter().
  :linenos:

  case SIMPLEGATTPROFILE_CHAR4:
      if ( len == sizeof ( uint8 ) )
      {
        simpleGattProfile_Char4 = *((uint8*)value);

        // See if Notification has been enabled
        GATTServApp_ProcessCharCfg( simpleGattProfile_Char4Config, &simpleGattProfile_Char4, FALSE,
                                    simpleGattProfile_attrTbl, GATT_NUM_ATTRS( simpleGattProfile_attrTbl ),
                                    INVALID_TASK_ID, SimpleGattProfile_readAttrCB );
      }
      else
      {
        status = bleInvalidRange;
      }
      break;

Queued Writes
^^^^^^^^^^^^^

Prepare Write commands allows a GATT server to send more payload
data by queuing up multiple write requests. The default queue size
is 5. With a default MTU of 23 and payload of 18 bytes, up to 90
bytes of payload can be sent. For more information on queued writes, refer to
the Queued Writes section ([Vol 3], Part F, Section 3.4.6) of the |CORESPEC|.

Adjust the Prepare Write queue with :ble_api:`GATTServApp_SetParameter` with
parameter ``GATT_PARAM_NUM_PREPARE_WRITES``. There is no specified
limit, but it is bounded by the available HEAPMGR space.

.. _allocating_memory_for_gatt_procedures:

Allocating Memory for GATT Procedures
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

To support fragmentation, GATT and ATT payload structures must be
dynamically allocated for commands sent wirelessly. For example, a
buffer must be allocated when sending a GATT\_Notification. The
stack does this allocation if the preferred method to send a GATT
notification or indication is used: calling a SetParameter function
of the profile (that is, SimpleProfile\_SetParameter()) and calling
:ble_api:`GATTServApp_ProcessCharCfg` as described in
:ref:`gatt_get_and_set_functions`.

If using :ble_api:`GATT_Notification` or :ble_api:`GATT_Indication` directly,
memory management must be added as follows.

1. Try to allocate memory for the notification or indication payload
   using :ble_api:`GATT_bm_alloc`.

2. Send notification or indication using :ble_api:`GATT_Notification` or
   :ble_api:`GATT_Indication` if the allocation succeeds.

.. note::
   If the return value of the notification or indication is
   ``SUCCESS (0x00)``, the stack freed the memory. 
   
   .. Add when feature is public
   .. If retransmissions are enabled and a transmission fails, 
   .. then a specified number of transmissions (as configured by GATT_SetupRetrans API) .
   .. will be attempted until the transmission succeeds.

3. Use :ble_api:`GATT_bm_free` to free the memory if the return value is
   something other than ``SUCCESS`` (for example, ``blePending``).

   The following is an example of this in the ``GATTServApp_SendNotiInd``
   function in the gattservapp\_util.c file.

.. _gattservapp_mem_alloc:
.. code-block:: c
   :caption: gattServApp\_SendNotiInd().
   :linenos:

   noti.pValue = (uint8 *)GATT_bm_alloc( connHandle, ATT_HANDLE_VALUE_NOTI, GATT_MAX_MTU, &len );

   if ( noti.pValue != NULL )
   {
      status = (*pfnReadAttrCB)( connHandle, pAttr, noti.pValue, &noti.len, 0, len, GATT_LOCAL_READ );

      if ( status == SUCCESS )
      {
         noti.handle = pAttr->handle;

         if ( cccValue & GATT_CLIENT_CFG_NOTIFY )
         {
            status = GATT_Notification( connHandle, &noti, authenticated );
         }

         else // GATT_CLIENT_CFG_INDICATE
         {
            status = GATT_Indication( connHandle, (attHandleValueInd_t *)&noti, authenticated, taskId );
         }
      }

      if ( status != SUCCESS )
      {
         GATT_bm_free( (gattMsg_t *)&noti, ATT_HANDLE_VALUE_NOTI );
      }
   }

   else
   {
      status = bleNoResources;
   }

For other GATT procedures, take similar steps as noted in
:ref:`ble_api_reference` (specifically ATT/GATT section).

.. _registering_to_receive_additional_gatt_events_in_the_application:

Registering to Receive Additional GATT Events in the Application
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

Using :ble_api:`GATT_RegisterForMsgs`, receiving additional
GATT messages to handle certain corner cases is possible. The event will be
first handled by BLEAppUtil\_processGATTEvents() in bleapputil\_process.c. Then
feed to GATT\_EventHandler() in app\_data.c.
  

.. _delaying_an_att_read_request:

Delaying an ATT Read Request
^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The stack supports a delayed response to the following read requests using a few APIs. 

      +------------------------+--------------------------------+
      | Type of read request   | API to be used                 |
      +========================+================================+
      | ATT_READ_REQ           | :ble_api:`ATT_ReadRsp`         |
      +------------------------+--------------------------------+
      | ATT_READ_BLOB_REQ      | :ble_api:`ATT_ReadBlobRsp`     |
      +------------------------+--------------------------------+  
      | ATT_READ_BY_TYPE_REQ   | :ble_api:`GATTServApp_ReadRsp` |
      +------------------------+--------------------------------+


Using :ble_api:`GATTServApp_ReadRsp`, delaying an ``ATT_READ_REQ`` from a
registered service is possible. If enabled, the GATT Server can handle read
requests in two ways. When a read request is received, the GATT Server will
issue a callback to the registered service.  The callback can return:

      +------------+--------------------------------------------------------------------------------------------------------+
      | SUCCESS    | the GATT Server will issue the appropriate ATT_Read_Rsp on behalf of the application                   |
      +------------+--------------------------------------------------------------------------------------------------------+
      | blePending | the service can call :ble_api:`GATTServApp_ReadRsp` to handle the read request when data is available  |
      +------------+--------------------------------------------------------------------------------------------------------+  

To enable this feature, choose the option that applies to your case:

   * in SysConfig, in the "BLE" menu, activate the option "Delaying an 
     ATT Read Request"

   * [If SysConfig is not available] define the symbol ``ATT_DELAYED_REQ``.
     For a two-project example, ``ATT_DELAYED_REQ`` has to be defined in
     the STACK library project.

The service callback function that requires a delay can add the following to its read callback function:

.. code-block:: c
    
    if( (method == ATT_READ_REQ) || (method == ATT_READ_BLOB_REQ) || (method == ATT_READ_BY_TYPE_REQ) )
    {
        status = blePending;
    }
    

At a later point in the code execution when the data is ready to be sent back, a decision tree similar to the one below can be used:

.. code-block:: c

    switch( cmdID )
        {
        case ATT_READ_REQ:
        {
            attReadRsp_t rsp;
            rsp.pValue = (uint8_t *) GATT_bm_alloc( connId, ATT_READ_RSP, (uint16_t) pCmd->len, NULL );
            if( rsp.pValue )
            {
                rsp.len = (uint16_t) pCmd->len;
                memcpy( rsp.pValue, pCmd->val, rsp.len );
                Status = ATT_ReadRsp( usConnId , &rsp );
                if( Status != SUCCESS )
                {
                    GATT_bm_free( (gattMsg_t * ) &rsp, ATT_READ_RSP );
                }
            }
            else
            {
                return ( bleMemAllocError );
            }
            break;
        }
        case ATT_READ_BLOB_REQ:
        {
            attReadBlobRsp_t rsp;
            rsp.pValue = (uint8_t *) GATT_bm_alloc( connId, ATT_READ_BLOB_RSP, (uint16_t) pCmd->len, NULL );
            if( rsp.pValue )
            {
                rsp.len = (uint16_t) pCmd->len;
                memcpy( rsp.pValue, pCmd->val, rsp.len );
                xStackStatus = ATT_ReadBlobRsp( usConnId , &rsp );
                if( xStackStatus != SUCCESS )
                {
                    GATT_bm_free( (gattMsg_t * ) &rsp, ATT_READ_BLOB_RSP );
                }
            }
            else
            {
                return ( bleMemAllocError );
            }
            break;
        }
        case ATT_READ_BY_TYPE_REQ:
        {
            Status = GATTServApp_ReadRsp( ConnHandle, pAttrValue, attrLen, attrHandle );
            break;
        }
    }

This procedure is illustrated in :numref:`gatt_delay_read_req_fig`

.. _gatt_delay_read_req_fig:
.. uml::
  :caption: Delay Read Request Illustration
  :align: center

   @startuml
    participant "Service CB \n(simple_gatt_profile.c)" as App
    participant GATTServApp
    participant "BLE Stack"  as BLE

    BLE <--]: Receive Attribute Read Request

    BLE -> GATTServApp : GATT_MSG_EVENT

    Activate "GATTServApp"
     GATTServApp -> GATTServApp : Process Event
     GATTServApp -> GATTServApp : Process Msg "ATT Read Req"

    group status != (SUCCESS | BLE_PENDING)
      GATTServApp -> BLE : ATT_ErrorRsp
      Deactivate "GATTServApp"
      BLE -->] : Send ATT_ERROR_RSP
    end


    group status == SUCCESS
      GATTServApp -> App : Find Attribute CB
      App -> App : SimpleGattProfile_ReadAttrCB
      rnote over "App"
        Copy the values
      end note
      App -> GATTServApp
      GATTServApp -> BLE : ATT_ReadRsp
      BLE -->] : ATT_READ_RSP
    end

    group status == BLE_PENDING
      GATTServApp -> App : Find Attribute CB
      App -> App : SimpleGattProfile_ReadAttrCB
      rnote over "App"
        Wait for data
      end note
      App -> GATTServApp
      GATTServApp -> BLE : GATTServApp_ReadRsp
      BLE -->] : ATT_READ_RSP
    end

   @enduml