..  README
    Newest guides at the top. Previous one-time guides go into Previous Migration
    Guides section. The nice thing here is that you just need to move the guide.
    Also, these guide are intended to be static one-time snapshots. No effort
    will be made to re-purpose each porting guide for the next release.


Porting and Migration Guides
============================


Porting Guides
--------------

Porting guides are used to port incremental changes from the previous SDK.

SDK porting guides
^^^^^^^^^^^^^^^^^^

.. toctree::
    :titlesonly:
    
    /ble-stack-5.x-guide/porting-guides/cc23xx/CC23XX_SDK_7.10_to_7.20.rst


Fixed Issues
^^^^^^^^^^^^

.. toctree::
    :titlesonly:
    
    /ble-stack-5.x-guide/porting-guides/cc23xx/CC23XX_comprehensive_fix_list.rst

.. Year-to-Year Migration Guides
.. -----------------------------
.. The following migration guides are designed to help migrate across multiple SDK releases.

.. .. toctree: ..:
..     :titlesonly:

..     porting-guides/ble5stack2.01.02-to-ble5stack2.02.01.rst
..     porting-guides/ble5stack2.01.01-to-ble5stack2.02.01.rst


Migration Guides
----------------
Migration guides are used to migrate major changes, e.g. from one device to
another device or from one configuration to another.

Device migration guides
^^^^^^^^^^^^^^^^^^^^^^^

.. toctree::
    :titlesonly:
                                                                                                                                                                                                                                                 
    /ble-stack-5.x-guide/porting-guides/cc26x2_to_cc23xx.rst
    /ble-stack-5.x-guide/porting-guides/cc2640r2_to_cc23xx.rst
    /ble-stack-5.x-guide/porting-guides/cc254x_to_cc23xx.rst

Other migration guides
^^^^^^^^^^^^^^^^^^^^^^

.. toctree::
    :titlesonly:
    
    /cc23xx/uart_to_uart2.rst
    /cc23xx/gpio-porting-guide-cc23xx.rst
    /ble-stack-5.x-guide/porting-guides/blestack_to_ble5stack-cc23xx.rst