API Documentation  3.02.02.00
Data Fields
PWMTimerCC26XX_Object Struct Reference

PWMTimer26XX Object. More...

Data Fields

uint32_t dutyCounts
 
PWM_Duty_Units dutyUnit
 
uint32_t dutyValue
 
GPTimerCC26XX_Handle hTimer
 
PWM_IdleLevel idleLevel
 
bool isOpen
 
bool isRunning
 
uint32_t periodCounts
 
PWM_Period_Units periodUnit
 
uint32_t periodValue
 

Detailed Description

PWMTimer26XX Object.

These fields are used by the driver to store and modify PWM configuration during run-time. The application must not edit any member variables of this structure. Appplications should also not access member variables of this structure as backwards compatibility is not guaranteed.

Field Documentation

§ dutyCounts

uint32_t PWMTimerCC26XX_Object::dutyCounts

Current duty in raw timer counts

§ dutyUnit

PWM_Duty_Units PWMTimerCC26XX_Object::dutyUnit

Current duty cycle unit

§ dutyValue

uint32_t PWMTimerCC26XX_Object::dutyValue

Current duty cycle value in unit

§ hTimer

GPTimerCC26XX_Handle PWMTimerCC26XX_Object::hTimer

Handle to underlying GPTimer peripheral

§ idleLevel

PWM_IdleLevel PWMTimerCC26XX_Object::idleLevel

PWM idle level when stopped / not started

§ isOpen

bool PWMTimerCC26XX_Object::isOpen

open flag used to check if PWM is opened

§ isRunning

bool PWMTimerCC26XX_Object::isRunning

running flag, set if the output is active

§ periodCounts

uint32_t PWMTimerCC26XX_Object::periodCounts

Current period in raw timer counts

§ periodUnit

PWM_Period_Units PWMTimerCC26XX_Object::periodUnit

Current period unit

§ periodValue

uint32_t PWMTimerCC26XX_Object::periodValue

Current period value in unit


The documentation for this struct was generated from the following file: