API Documentation  3.02.02.00
Data Fields
PWMTimerCC26XX_HwAttrs Struct Reference

PWMTimer26XX Hardware attributes. More...

Data Fields

uint8_t gpTimerUnit
 
uint8_t pwmPin
 

Detailed Description

PWMTimer26XX Hardware attributes.

These fields are used by the driver to set up underlying GPIO and GPTimer driver statically.

Field Documentation

§ gpTimerUnit

uint8_t PWMTimerCC26XX_HwAttrs::gpTimerUnit

GPTimer unit index (0A, 0B, 1A..)

§ pwmPin

uint8_t PWMTimerCC26XX_HwAttrs::pwmPin

Pin to output PWM signal on


The documentation for this struct was generated from the following file: