|
API Documentation
3.02.02.00
|
Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout() More...
Data Fields | |
| void * | arg |
| void * | readBuf |
| size_t | readCount |
| uint_least8_t | slaveAddress |
| volatile int_fast16_t | status |
| void * | writeBuf |
| size_t | writeCount |
Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout()
After a call to I2C_transfer(), the I2C_Transaction.status reflects the current transfer status.
| void* I2C_Transaction::arg |
Pointer to a custom argument to be passed to the I2C_CallbackFxn function via the I2C_Transaction structure.
| void* I2C_Transaction::readBuf |
Pointer to a buffer of at least I2C_Transaction.readCount bytes. If I2C_Transaction.readCount is 0, this pointer is not used.
| size_t I2C_Transaction::readCount |
Number of bytes to read from the I2C slave device. A value of 0 indicates no data will be read and only a write will occur. If I2C_Transaction.writeCount is not 0, this driver will perform the write first, followed by the read. The data read from the bus is preceded by the I2C_Transaction.slaveAddress with the read bit set. After readCount bytes are successfully read, the transfer will complete.
| uint_least8_t I2C_Transaction::slaveAddress |
I2C slave address used for the transaction. The slave address is the first byte transmitted during an I2C transfer. The read/write bit is automatically set based upon the I2C_Transaction.writeCount and I2C_Transaction.readCount.
| volatile int_fast16_t I2C_Transaction::status |
I2C status of the current transaction. The status may be used to determine why a transaction failed. Potential codes are:
This status may also be used to determine if a transaction is queued (I2C_STATUS_QUEUED) or in progress (I2C_STATUS_INCOMPLETE).
| void* I2C_Transaction::writeBuf |
Pointer to a buffer of at least I2C_Transaction.writeCount bytes. If I2C_Transaction.writeCount is 0, this pointer is not used.
| size_t I2C_Transaction::writeCount |
Number of bytes to write to the I2C slave device. A value of 0 indicates no data will be written to the slave device and only a read will occur. If this value is not 0, the driver will always perform the write transfer first. The data written to the I2C bus is preceded by the I2C_Transaction.slaveAddress with the write bit set. If writeCount bytes are successfully sent and acknowledged, the transfer will complete or perform a read–depending on I2C_Transaction.readCount.
1.8.12