|
API Documentation
3.02.02.00
|
DisplayHost Attributes. More...
Data Fields | |
| char * | strBuf |
| uint16_t | strBufLen |
DisplayHost Attributes.
The DisplayHost driver uses a buffer for formatting messages, which is then passed to an fwrite() function. The location and size of the buffer are specified in a DisplayHost_HWAttrs structure.
| char* DisplayHost_HWAttrs::strBuf |
Buffer for formatting messages
| uint16_t DisplayHost_HWAttrs::strBufLen |
Size of buffer
1.8.12