API Documentation  3.02.02.00
Data Fields
ADCBuf_Conversion Struct Reference

Defines a conversion to be used with ADCBuf_convert(). More...

Data Fields

uint32_t adcChannel
 
void * arg
 
void * sampleBuffer
 
void * sampleBufferTwo
 
uint16_t samplesRequestedCount
 

Detailed Description

Defines a conversion to be used with ADCBuf_convert().

See also
ADCBuf_convert()
ADCBuf_Recurrence_Mode
ADCBuf_Return_Mode

Field Documentation

§ adcChannel

uint32_t ADCBuf_Conversion::adcChannel

ADCBuf channel to perform conversions on. Mapping of channel to pin or internal signal is device specific. Refer to the device specific implementation.

§ arg

void* ADCBuf_Conversion::arg

Pointer to a custom argument to be passed to the ADCBuf_Callback function via the ADCBuf_Conversion structure.

Note
The ADCBuf_Callback function is only called when operating in ADCBuf_RETURN_MODE_CALLBACK.
See also
ADCBuf_RETURN_MODE_CALLBACK
ADCBuf_Callback

§ sampleBuffer

void* ADCBuf_Conversion::sampleBuffer

Buffer to store ADCBuf conversion results. This buffer must be at least (ADCBuf_Conversion.samplesRequestedCount * 2) bytes. When using ADCBuf_RECURRENCE_MODE_ONE_SHOT, only this buffer is used.

§ sampleBufferTwo

void* ADCBuf_Conversion::sampleBufferTwo

Buffer to store ADCBuf conversion results. This buffer must be at least (ADCBuf_Conversion.samplesRequestedCount * 2) bytes. When using ADCBuf_RECURRENCE_MODE_ONE_SHOT, this buffer is not used. When using ADCBuf_RECURRENCE_MODE_CONTINUOUS, this must point to a valid buffer.

See also
ADCBuf_RECURRENCE_MODE_CONTINUOUS

§ samplesRequestedCount

uint16_t ADCBuf_Conversion::samplesRequestedCount

Defines the number of samples to be performed on the ADCBuf_Conversion.channel. The application buffers provided by ADCBuf_Conversion.sampleBuffer and ADCBuf_Conversion.sampleBufferTwo must be large enough to hold samplesRequestedCount samples.


The documentation for this struct was generated from the following file: