API Documentation  3.02.02.00
DisplayHost.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016-2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
81 #ifndef ti_display_DisplayHost__include
82 #define ti_display_DisplayHost__include
83 
84 #include <ti/display/Display.h>
85 
86 #ifdef __cplusplus
87 extern "C" {
88 #endif
89 
97 typedef struct DisplayHost_HWAttrs
98 {
100  char *strBuf;
102  uint16_t strBufLen;
104 
110 typedef struct DisplayHost_Object
111 {
112  int dummy;
114 
115 /* DisplayHost function table pointer */
116 extern const Display_FxnTable DisplayHost_fxnTable;
117 
118 /* DisplayHost functions */
119 void DisplayHost_init(Display_Handle handle);
120 Display_Handle DisplayHost_open(Display_Handle handle, Display_Params *params);
121 void DisplayHost_clear(Display_Handle handle);
122 void DisplayHost_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine);
123 void DisplayHost_vprintf(Display_Handle handle, uint8_t line, uint8_t column, const char *fmt, va_list va);
124 void DisplayHost_close(Display_Handle handle);
125 int DisplayHost_control(Display_Handle handle, unsigned int cmd, void *arg);
126 unsigned int DisplayHost_getType(void);
127 #ifdef __cplusplus
128 }
129 #endif
130 
131 #endif /* ti_display_DisplayHost__include */
uint16_t strBufLen
Definition: DisplayHost.h:102
DisplayHost Object.
Definition: DisplayHost.h:110
Display Parameters.
Definition: Display.h:485
struct DisplayHost_HWAttrs DisplayHost_HWAttrs
DisplayHost Attributes.
Generic interface for text output.
DisplayHost Attributes.
Definition: DisplayHost.h:97
struct DisplayHost_Object DisplayHost_Object
DisplayHost Object.
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:535
char * strBuf
Definition: DisplayHost.h:100
Display Global configuration.
Definition: Display.h:558