API Documentation  3.02.02.00
DisplayDogm1286.h
1 /*
2  * Copyright (c) 2016-2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_display_DisplayDogm1286__include
34 #define ti_display_DisplayDogm1286__include
35 
36 #include <ti/drivers/dpl/SemaphoreP.h>
37 
38 #include <ti/drivers/SPI.h>
39 #include <ti/display/Display.h>
40 #include <ti/display/lcd/LCDDogm1286.h>
41 
42 #include <stdint.h>
43 
44 extern const Display_FxnTable DisplayDogm1286_fxnTable;
45 
47 {
48  LCD_Handle lcdHandle;
49  uint_least8_t powerPin;
51 
52 typedef struct DisplayDogm1286_Object
53 {
54  LCD_Handle hLcd;
55  Display_LineClearMode lineClearMode;
56  SemaphoreP_Struct lcdMutex;
57  char lcdBuffer0[1024];
58  LCD_Buffer lcdBuffers[1];
60 
61 void DisplayDogm1286_init(Display_Handle handle);
62 Display_Handle DisplayDogm1286_open(Display_Handle handle, Display_Params *params);
63 void DisplayDogm1286_clear(Display_Handle handle);
64 void DisplayDogm1286_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine);
65 void DisplayDogm1286_vprintf(Display_Handle handle, uint8_t line, uint8_t column, const char *fmt, va_list va);
66 void DisplayDogm1286_close(Display_Handle handle);
67 int DisplayDogm1286_control(Display_Handle handle, unsigned int cmd, void *arg);
68 unsigned int DisplayDogm1286_getType(void);
69 #endif // ti_display_DisplayDogm1286__include
Serial Peripheral Interface (SPI) Driver Interface.
Display Parameters.
Definition: Display.h:485
Generic interface for text output.
Definition: DisplayDogm1286.h:52
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:535
Definition: DisplayDogm1286.h:46
Display Global configuration.
Definition: Display.h:558
Display_LineClearMode
How to treat existing elements on a line when writing text.
Definition: Display.h:469