![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.02.00
|
PSM information format. More...
Data Fields | |
| uint16 | initPeerCredits |
| Number of LE-frames that peer device can send. | |
| uint8 | maxNumChannels |
| Maximum number of CO Channels supported by PSM. | |
| uint16 | mps |
| Maximum payload size that can be received by local device. | |
| uint16 | mtu |
| Maximum SDU size that can be received by local device. | |
| uint8 | numActiveChannels |
| Number of active CO Channels. | |
| uint16 | peerCreditThreshold |
| Low threshold for number of peer credits. | |
PSM information format.