![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.02.00
|
LE Periodic Advertising Sync Established event. More...
Data Fields | |
| uint8 | address [B_ADDR_LEN] |
| Peer address. | |
| uint8 | addrType |
| Peer address type. | |
| uint8 | BLEEventCode |
| BLE Event Code. | |
| uint8 | clockAccuracy |
| Peer Clock Accuracy. | |
| osal_event_hdr_t | hdr |
| osal event header | |
| uint16 | periodicInterval |
| Periodic interval. | |
| uint8 | phy |
| Peer PHY. | |
| uint8 | sid |
| Peer SID. | |
| uint8 | status |
| status of event | |
| uint16 | syncHandle |
| sync handle | |
LE Periodic Advertising Sync Established event.