![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.02.00
|
LE Periodic Advertising Report event. More...
Data Fields | |
| uint8 | BLEEventCode |
| BLE Event Code. | |
| uint8 | cteType |
| CTE type received. | |
| uint8 * | data |
| Periodic data received from peer. | |
| uint8 | dataLen |
| Periodic data length. | |
| uint8 | dataStatus |
| Periodic data status. | |
| osal_event_hdr_t | hdr |
| osal event header | |
| int8 | rssi |
| RSSI of the received packet. | |
| uint16 | syncHandle |
| sync handle | |
| int8 | txPower |
| Tx Power information. | |
LE Periodic Advertising Report event.