![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.02.00
|
Data Fields | |
| uint8_t | accepted |
| TRUE if host accepts parameter update, FALSE otherwise. | |
| uint16_t | connectionHandle |
| Connection handle of the update. | |
| uint16_t | connLatency |
| Connection Latency. | |
| uint16_t | connTimeout |
| Connection Timeout. | |
| uint16_t | intervalMax |
| Maximum Connection Interval. | |
| uint16_t | intervalMin |
| Minimum Connection Interval. | |
| uint8_t | signalIdentifier |
| L2CAP Signal Identifier. | |
Update Link Parameters Request Reply parameters
This is used by GAP_UpdateLinkParamReqReply