![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.02.00
|
Data Fields | |
| uint8_t | channel |
| BLE RF channel index (0-39) | |
| uint16_t | errors |
| Total number of CRC errors for the entire connection. | |
| uint16_t | handle |
| connection handle | |
| int8_t | lastRssi |
| uint32_t | nextTaskTime |
| Time to next BLE task (in us). 0xFFFFFFFF if there is no next task. | |
| GAP_ConnEvtTaskType_t | nextTaskType |
| Type of next BLE task. | |
| uint16_t | packets |
| Number of packets received for this connection event. | |
| GAP_ConnEvtPhy_t | phy |
| PHY of connection event. | |
| GAP_ConnEvtStat_t | status |
| status of connection event | |
Report describing connection event Returned via a pfnGapConnEvtCB_t.
| int8_t lastRssi |
RSSI of last packet received