![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.02.00
|
This module implements the Host Initiator. More...
Modules | |
| GapInit Constants | |
| GapInit Params | |
| GapInit Structures | |
Files | |
| file | gap_initiator.h |
| GAP Initiator layer interface. | |
Functions | |
| status_t | GapInit_cancelConnect (void) |
| status_t | GapInit_connect (GAP_Peer_Addr_Types_t peerAddrType, uint8_t *pPeerAddress, uint8_t phys, uint16_t timeout) |
| status_t | GapInit_connectWl (uint8_t phys, uint16_t timeout) |
| status_t | GapInit_getPhyParam (uint8_t phy, GapInit_PhyParamId_t paramId, uint16_t *pValue) |
| status_t | GapInit_setPhyParam (uint8_t phys, GapInit_PhyParamId_t paramId, uint16_t value) |
This module implements the Host Initiator.
| status_t GapInit_cancelConnect | ( | void | ) |
Cancel the ongoing connection process.
| status_t GapInit_connect | ( | GAP_Peer_Addr_Types_t | peerAddrType, |
| uint8_t * | pPeerAddress, | ||
| uint8_t | phys, | ||
| uint16_t | timeout | ||
| ) |
Initiate connection with the specified peer device
| peerAddrType | peer device's address type. |
| pPeerAddress | peer device's address |
| phys | PHY to try making connection on: shall be one from GapInit_InitPhy_t. |
| timeout | If there is no chance to initiate a connection within timeout ms, this connect request will be canceled automatically. if timeout is 0, the initiator will keep trying to get a chance to make a connection until GapInit_cancelConnect is called. |
| status_t GapInit_connectWl | ( | uint8_t | phys, |
| uint16_t | timeout | ||
| ) |
| phys | PHY to try making connection on: shall be one from GapInit_InitPhy_t. |
| timeout | If there is no chance to initiate a connection within timeout ms, this connect request will be canceled automatically. if timeout is 0, the initiator will keep trying to get a chance to make a connection until GapInit_cancelConnect is called. |
| status_t GapInit_getPhyParam | ( | uint8_t | phy, |
| GapInit_PhyParamId_t | paramId, | ||
| uint16_t * | pValue | ||
| ) |
Get parameters of the specified PHY.
| phy | connection channel PHY: shall be one from GapInit_InitPhy_t. |
| paramId | parameter ID |
| pValue | pointer to where the parameter value is to be stored |
| status_t GapInit_setPhyParam | ( | uint8_t | phys, |
| GapInit_PhyParamId_t | paramId, | ||
| uint16_t | value | ||
| ) |
Set parameters dependent on PHY.
| phys | connection channel PHY(s): Individual PHY values of GapInit_InitPhy_t can be OR'ed. |
| paramId | parameter ID |
| value | parameter value |