TI BLE5-Stack API Documentation  3.02.02.00
File List
Here is a list of all documented files with brief descriptions:
 att.hATT layer interface
 bcomdef.hType definitions and macros for BLE stack
 comdef.hCommon Defines
 gap.hGAP layer interface
 gap_advertiser.hGAP Advertiser layer interface
 gap_initiator.hGAP Initiator layer interface
 gap_scanner.hGAP Scanner layer interface
 gapbondmgr.h
 gapgattserver.h
 gatt.hGATT layer interface
 gattservapp.hGATTServApp layer interface
 hci.hHCI layer interface
 hci_tl.hTypes, constants, external functions etc. for the BLE HCI Transport Layer
 icall.hICall layer interface
 icall_addrs.hStack image address information specific to build
 icall_cc26xx_defs.hIndirect function Call dispatcher constant definitions specific to CC26xx platform
 l2cap.hL2CAP layer interface
 linkdb.h
 osal.hThis API allows the software components in the Z-Stack to be written independently of the specifics of the operating system, kernel, or tasking environment (including control loops or connect-to-interrupt systems)
 osal_memory.hHis module defines the OSAL memory control functions
 sm.hThis file contains the interface to the SM
 uble.hThis file contains configuration, initialization, and parameter management of Micro BLE Stack. It also contains interfacing between Micro BLE Stack and the application
 ugap.hMicro BLE GAP API
 util.hUtil layer interface
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale