Changelog

Table of Contents

 

New Features

BLE5-Stack

ID Summary
BLE_LOKI-794 Introduced No Delay Advertising Feature
BLE_LOKI-709 [BASIC BLE] [Profiles] Glucose Profile added to ble_basic profiles
BLE_LOKI-674 Connection Monitor example introduced
BLE_LOKI-473 [OAD] OAD Dual Image Support
BLE_LOKI-224 Use RSSI/Channel/Timestamp reported by the RCL

TI Proprietary RF

ID Summary
PROPRF-1226 [F3] Update 500kbps MSK PHY to 250kbps MSK FEC

TI-RTOS and Drivers

ID Summary
TIDRIVERS-6110 Add API for modular reduction for non-curve length input length
TIDRIVERS-6025 Add Elliptic Curve Integrated Encryption Scheme (ECIES) driver for CC23x0

Radio Control Library (RCL)

ID Summary
RCL-409 Improve robustness of radio entropy generation in the presence of a strong RF signal
RCL-238 Added support for HFXT SW TCXO by compensating RF PLL

 

Fixed Issues

BLE5-Stack

ID Summary
BLE_LOKI-768 Device stops responding after multiple connections

TI Proprietary RF

ID Summary
None None

TI-RTOS and Drivers

ID Summary
TIDRIVERS-6065 Some PWM files not exported into SDK

Radio Control Library (RCL)

ID Summary
RCL-384 RSSI read back-to-back reading sometimes returns unexpected value
RCL-392 PBE fails to respond if a timer interrupt flag is unexpectedly set at first execution

 

Known Issues

BLE5-Stack

ID Summary
BLE_LOKI-1016 CC2340 unintended wakeup from standby, interval gets shorter and shorter
BLE_LOKI-939 Fails to Change Connection PHY to Coded in multi-role with multiple connections
BLE_LOKI-872 [Application] basic_ble_Central - Missing Addresses In Scan Results When Duplicate Filters Is Enable
BLE_LOKI-694 [GATT_WriteLongCharValue] Large data size (300 bytes) results in incomplete writes

TI Proprietary RF

ID Summary
None None

TI-RTOS and Drivers

ID Summary
TIPOSIX-4 clock_nanosleep() with CLOCK_REALTIME broken on msp432
SYSBIOS-642 Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field
SYSBIOS-446 Reported CPU load is not 100% when a task is in “while 1 {}” loop
SYSBIOS-98 Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432
FREERTOS-8 Tasks view in ROV for FreeRTOS does not show if a task is blocked on a semaphore or mutex

Radio Control Library (RCL)

ID Summary
RCL-343 PBE NESB - Address mismatch counter not implemented