Platform Support Package (PSP) Software Manifest
Legend
|
Package Name |
The name of the application or files |
|
Version |
Version of the application or files |
|
License |
Name of the license or licenses that apply to the Package. |
|
Location |
The directory name and path on the media (or in an archive) where the Package is located. |
|
Delivered As |
This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in. If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided. |
|
Modified |
This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes. |
|
This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded. |
Manifest
Note: Replace MM.mm.pp.bb in the directory path below
with the PSP release version you are using.
|
Package Name |
Version |
License |
Delivered As |
Modified |
|
|
|
ARM NOR/NAND/SPI User Boot Loader |
NA |
GPLv2 |
Source and Binary |
NA |
Location |
Source at DA850/OMAP-L138/AM18xx Pre-built binaries at DA830/OMAP-L137 Pre-built binaries at AM17xx Pre-built binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/am17xx/arm-spi-ais.bin |
|
Obtained from[1] |
TI |
|||||
|
DSP NAND/SPI User Boot Loader |
NA |
GPLv2 |
Source and Binary |
NA |
Location |
Source at DA830/OMAP-L137 Pre-built binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x7/dsp-spi-ais.bin |
|
Obtained from[1] |
TI |
|||||
|
SPI Flash Writer |
NA |
GPLv2 |
Source and Binary |
YES |
Location |
Source at DA830/OMAP-L137/AM17xx Binary at DA850/OMAP-L138/AM18xx Binary at |
|
Obtained from[1] |
SPI flash code in U-Boot obtained from http://git.denx.de/?p=u-boot.git;a=summary. Commit ID 3d1c46b2efcf4c56226d6bc5b8a3c2372e7ab517. |
|||||
|
NAND Flash Writer |
NA |
GPLv2 |
Source and Binary |
NA |
Location |
Source at DA830/OMAP-L137/AM17xx Binary at DA850/OMAP-L138/AM18xx Binary at |
|
Obtained from[1] |
TI |
|||||
|
NOR Flash Writer |
NA |
GPLv2 |
Source and Binary |
NA |
Location |
Source at DA850/OMAP-L138/AM18xx Binary at |
|
Obtained from[1] |
TI |
|||||
|
U-Boot |
2009.11 |
GPLv2 |
Source and Binary |
YES |
Location |
Source at DA830/OMAP-L137/AM17xx SPI Boot mode Binary at DA850/OMAP-L138/AM18xx SPI Boot mode Binary at |
|
Obtained from[1] |
U-Boot 2009.11 obtained from http://git.denx.de/?p=u-boot.git;a=commit; h=bb3bcfa2426cc6a0aecec7270e3ee67ca843a125. |
|||||
|
Video
Sample Code |
NA |
BSD |
Source and binary |
NA |
Location |
Source at Binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/vpif_test_userptr_loopback |
|
Obtained from[1] |
TI |
|||||
|
GPIO/EDMA/McBSP
Sample Code |
NA |
GPLv2 |
Source and binary |
NA |
Location |
Source at Binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/mcbsp_test.ko |
|
Linux Functional Testbench(LFTB) |
01.00.00.13 |
TI New BSD (user space) & GPLV2 for kernel space |
Source and Binary |
NA |
Location |
Source at DaVinci-PSP-SDK-MM.mm.pp.bb/test-suite |
|
Obtained from[1] |
TI |
|||||
|
Open source Linux (based on |
2.6.33-rc4 |
GPLv2 |
Source and Binary |
YES |
Location |
Source at DA830/OMAP-L137/AM17xx Binary at DA850/OMAP-L138/AM18xx Binary at |
|
Obtained from[1] |
Linux 2.6.33-rc4 obtained from http://git.kernel.org/?p=linux/kernel/git/khilman/linux-davinci.git;a=commit; h=887f8d18de5efbeafc76e5c509fd53f9018992fa. |
|||||
[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.