#! /usr/bin/perl
# -*- Perl -*-
# Generated from bin/autoconf.in; do not edit by hand.

eval 'case $# in 0) exec /usr/bin/perl -S "$0";; *) exec /usr/bin/perl -S "$0" "$@";; esac'
    if 0;

# autoconf -- create 'configure' using m4 macros.

# Copyright (C) 1992-1994, 1996, 1999-2017, 2020-2023 Free Software
# Foundation, Inc.

# This program is free software: you can redistribute it and/or modify
# it under the terms of the GNU General Public License as published by
# the Free Software Foundation, either version 3 of the License, or
# (at your option) any later version.

# This program is distributed in the hope that it will be useful,
# but WITHOUT ANY WARRANTY; without even the implied warranty of
# MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
# GNU General Public License for more details.

# You should have received a copy of the GNU General Public License
# along with this program.  If not, see <https://www.gnu.org/licenses/>.

use 5.006;
use strict;
use warnings FATAL => 'all';

BEGIN
{
  my $pkgdatadir = $ENV{'autom4te_perllibdir'} || '/usr/share/autoconf';
  unshift @INC, $pkgdatadir;

  # Override SHELL.  On DJGPP SHELL may not be set to a shell
  # that can handle redirection and quote arguments correctly,
  # e.g.: COMMAND.COM.  For DJGPP always use the shell that configure
  # has detected.
  $ENV{'SHELL'} = '/bin/bash' if ($^O eq 'dos');
}

use Autom4te::ChannelDefs;
use Autom4te::Channels qw(msg);
use Autom4te::General;

# Lib files.
my $autom4te = $ENV{'AUTOM4TE'} || '/usr/bin/autom4te';
my $trailer_m4 = $ENV{'trailer_m4'} || '/usr/share/autoconf/autoconf/trailer.m4';

# $HELP
# -----
$help = "Usage: $0 [OPTION]... [TEMPLATE-FILE]

Generate a configuration script from a TEMPLATE-FILE if given, or
'configure.ac' if present, or else 'configure.in'.  Output is sent
to the standard output if TEMPLATE-FILE is given, else into
'configure'.

Operation modes:
  -h, --help                print this help, then exit
  -V, --version             print version number, then exit
  -v, --verbose             verbosely report processing
  -d, --debug               don't remove temporary files
  -f, --force               consider all files obsolete
  -o, --output=FILE         save output in FILE (stdout is the default)
  -W, --warnings=CATEGORY   report the warnings falling in CATEGORY
                            (comma-separated list accepted)

" . Autom4te::ChannelDefs::usage . "

Library directories:
  -B, --prepend-include=DIR  prepend directory DIR to search path
  -I, --include=DIR          append directory DIR to search path

Tracing:
  -t, --trace=MACRO[:FORMAT]  report the list of calls to MACRO
  -i, --initialization        also trace Autoconf's initialization process

In tracing mode, no configuration script is created.  FORMAT defaults
to '\$f:\$l:\$n:\$%'; see 'autom4te --help' for information about FORMAT.

Report bugs to <bug-autoconf\@gnu.org>.

The full documentation for Autoconf can be read via 'info autoconf',
or on the Web at <https://www.gnu.org/software/autoconf/manual/>.
";

# $VERSION
# --------
$version = "autoconf (GNU Autoconf) 2.72e
Copyright (C) 2023 Free Software Foundation, Inc.
License GPLv3+/Autoconf: GNU GPL version 3 or later
<https://gnu.org/licenses/gpl.html>, <https://gnu.org/licenses/exceptions.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.

Written by David J. MacKenzie and Akim Demaille.
";

## ---------- ##
## Routines.  ##
## ---------- ##

my $infile;
my $outfile;
my @autom4te_options;
my @traces;

# parse_args ()
# -------------
# Process any command line arguments.
sub parse_args ()
{
  getopt (
    # Arguments passed as-is to autom4te.
    'I|include=s'         => sub { push @autom4te_options, '--include='.$_[1] },
    'B|prepend-include=s' => sub { push @autom4te_options,
                                     '--prepend-include='.$_[1] },
    'W|warnings=s'        => sub { push @autom4te_options,
                                     '--warnings='.$_[1] },

    # Arguments processed (somewhat) in this program.
    'i|initialization' => sub { push @autom4te_options, '--melt' },
    't|trace=s'        => sub { push @traces, '--trace='.$_[1] },
    'o|output=s'       => \$outfile,
  );

  # Also pass down certain options that were processed into their own
  # variables by Autom4te::General::getopt.
  push @autom4te_options, '--debug' if $debug;
  push @autom4te_options, '--force' if $force;
  push @autom4te_options, '--verbose' if $verbose;

  # Find the input file.
  if (@ARGV == 0)
    {
      $outfile = 'configure' if !$outfile && !@traces;

      if (-f 'configure.ac')
        {
          $infile = 'configure.ac';
          if (-f 'configure.in')
            {
              msg 'obsolete',
                q(both 'configure.ac' and 'configure.in' are present);
              msg 'obsolete',
                q(proceeding with 'configure.ac');
            }
        }
      elsif (-f 'configure.in')
        {
          $infile = 'configure.in';
        }
      else
        {
          fatal 'no input file';
        }
    }
  elsif (@ARGV == 1)
    {
      $infile = $ARGV[0];
    }
  else
    {
      fatal "invalid number of arguments.\n"
        . "Try '$me --help' for more information.";
    }

  # Unless already set, the output is stdout.
  $outfile = '-' if !$outfile;
}

## -------------- ##
## Main program.  ##
## -------------- ##

parse_args;

# Construct the autom4te invocation.
# $autom4te might contain additional command line options; word-split it
# exactly as the shell would.
my @autom4te_command = split /[ \t\n]+/, $autom4te;
push @autom4te_command, @autom4te_options;
push @autom4te_command, '--language=autoconf', "--output=$outfile", @traces;

# Don't read trailer.m4 if we are tracing.
# trailer.m4 is read _before_ $infile, despite the name,
# because putting it afterward screws up autom4te's location tracing.
push @autom4te_command, $trailer_m4 if !@traces;
push @autom4te_command, $infile;

print {*STDERR} $me,
  ': running ',
  join (" ", map { shell_quote($_) } @autom4te_command),
  "\n"
  if $verbose;

exec {$autom4te_command[0]} @autom4te_command;

### Setup "GNU" style for perl-mode and cperl-mode.
## Local Variables:
## perl-indent-level: 2
## perl-continued-statement-offset: 2
## perl-continued-brace-offset: 0
## perl-brace-offset: 0
## perl-brace-imaginary-offset: 0
## perl-label-offset: -2
## cperl-indent-level: 2
## cperl-brace-offset: 0
## cperl-continued-brace-offset: 0
## cperl-label-offset: -2
## cperl-extra-newline-before-brace: t
## cperl-merge-trailing-else: nil
## cperl-continued-statement-offset: 2
## End: