# @name
#	CAN suspend test
# @desc
#	CAN suspend tests. No physical cables are required to run this test.
#	EVM needs to be in the right profile which supports the pinmux for
#	CAN. This comment applies to am335x-evm which requires EVM to be in
#	profile 1. Profile 1 supports CAN instead of wlan on this EVM.
# @requires can

CAN_S_FUNC_SUSPEND source 'common.sh';  interface='can0'; bitrate=1000000; do_cmd "ip link set $interface down"; do_cmd "ip link set $interface type can bitrate $bitrate"; do_cmd "ip link set $interface up"; init_state=`cat /sys/class/net/$interface/operstate`; run_processes.sh -c "/opt/ltp/runltp -P $PLATFORM -f ddt/powermgr_suspend -s 'POWERMGR_S_FUNC_SIMPLE_SUSPEND '";final_state=`cat /sys/class/net/$interface/operstate`; if [ $init_state != $final_state ]; then die "Suspend resume did not restore CAN state"; fi

CAN_S_FUNC_SUSPEND_MAIN_MCAN0_1000000 source 'common.sh'; interface='main_mcan0'; bitrate=1000000; do_cmd cantest.sh --suspend -i $interface -b $bitrate

CAN_S_FUNC_SUSPEND_MAIN_MCAN1_1000000 source 'common.sh'; interface='main_mcan1'; bitrate=1000000; do_cmd cantest.sh --suspend -i $interface -b $bitrate

CAN_S_FUNC_SUSPEND_MCU_MCAN0_1000000 source 'common.sh'; interface='mcu_mcan0'; bitrate=1000000; do_cmd cantest.sh --suspend -i $interface -b $bitrate

CAN_S_FUNC_SUSPEND_MCU_MCAN1_1000000 source 'common.sh'; interface='mcu_mcan1'; bitrate=1000000; do_cmd cantest.sh --suspend -i $interface -b $bitrate