# TTY, where emptty will start.
TTY_NUMBER=7

# Enables switching to defined TTY number.
SWITCH_TTY=true

# Enables printing of /etc/issue in daemon mode.
PRINT_ISSUE=true

# Enables printing of default motd, /etc/emptty/motd or /etc/emptty/motd-gen.sh.
PRINT_MOTD=true

# Preselected user, if AUTOLOGIN is enabled, this user is logged in.
DEFAULT_USER=weston

# Enables Autologin, if DEFAULT_USER is defined and part of nopasswdlogin group. Possible values are "true" or "false".
AUTOLOGIN=true

# The default session used, if Autologin is enabled. If session is not found in list of session, it proceeds to manual selection.
AUTOLOGIN_SESSION=Weston

# If Autologin is enabled and session does not start correctly, the number of retries in short period is kept to eventually stop the infinite loop of restarts. -1 is for infinite retries, 0 is for no retry.
AUTOLOGIN_MAX_RETRY=-1

# Default LANG, if user does not have set own in init script.
#LANG=en_US.UTF-8

# Starts desktop with calling "dbus-launch".
DBUS_LAUNCH=true

# Starts Xorg desktop with calling "~/.xinitrc" script, if is true, file exists and selected WM/DE is Xorg session, it overrides DBUS_LAUNCH.
XINITRC_LAUNCH=false

# Prints available WM/DE each on new line instead of printing on single line.
VERTICAL_SELECTION=false

# Defines the way, how is logging handled. Possible values are "rotate", "appending" or "disabled".
#LOGGING=rotate

# Overrides path of log file
#LOGGING_FILE=/var/log/emptty/[TTY_NUMBER].log

# Arguments passed to Xorg server.
#XORG_ARGS=

# Allows to use dynamic motd script to generate custom MOTD.
#DYNAMIC_MOTD=false

# Allows to override default path to dynamic motd.
#DYNAMIC_MOTD_PATH=/etc/emptty/motd-gen.sh

# Allows to override default path to static motd.
#MOTD_PATH=/etc/emptty/motd

# Foreground color, available only in daemon mode.
#FG_COLOR=LIGHT_BLACK

# Background color, available only in daemon mode.
#BG_COLOR=BLACK

# Enables numlock in daemon mode. Possible values are "true" or "false".
#ENABLE_NUMLOCK=false

# Defines the way, how is logging of session errors handled. Possible values are "rotate", "appending" or "disabled".
SESSION_ERROR_LOGGING=rotate

# Overrides path of session errors log file
#SESSION_ERROR_LOGGING_FILE=/var/log/emptty/session-errors.[TTY_NUMBER].log

# If set true, it will not use `.emptty-xauth` file, but the standard `~/.Xauthority` file. This allows to handle xauth issues.
#DEFAULT_XAUTHORITY=false

#If set true, Xorg will be started as rootless, if system allows and emptty is running in daemon mode.
#ROOTLESS_XORG=false

#If set true, environmental groups are printed to differ Xorg/Wayland/Custom/UserCustom desktops.
IDENTIFY_ENVS=false