Jacinto Connected Cars on AWS Version 2.4.0, updated 10/5/2021 This directory contains prebuilt installers for Amazon Web Service (AWS) Greengrass Corretto-11, as well as the Getting Started Guide to create a Jacinto Connected Cars demo with the AWS Connected Mobility Solutions (CMS). These packages can be installed to the DRA82x EVM Linux file system by executing the following commands on the target board running Linux: >opkg install corretto-11-bin__aarch64.ipk >opkg install greengrass__aarch64.ipk Refer to the "Jacinto Connected Cars on AWS: Getting Started Guide" in this package for detailed instructions to install and configure the complete demonstration.