Software Name | The name of the application or files |
Version | Version of the application or files |
License Type | Type of license(s) under which TI will be providing software to the licensee (e.g. BSD, GPLv2, TI TSPA License, TI Commercial License). See Open Source Reference License Disclaimer in the Disclaimers Section. |
Location | The directory name and path on the media (or in an archive) where the Package is located. |
Delivered As | This field will either be “Source”, “Binary” or “Source and Binary“ and is the form the content of the Package is delivered in. If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided. |
Modified by TI | This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Software. A “No” means TI has not made any changes. NOTE: This field is not applicable for Software “Obtained from” TI. |
Obtained from | This field specifies from where or from whom TI obtained the Software. It may be a URL to an Open Source site, a 3rd party companylicensor, or TI (if TI developed the software). If this field contains a link to an Open Source software, the date it was downloaded is also recorded. See Links Disclaimer in the Disclaimers Section. |
Any use of ECCNs listed in the Manifest is at the user's risk and without recourse to TI. Your company, as the exporter of record, is responsible for determining the correct classification of any item at the time of export. Any export classification by TI of Software is for TI's internal use only and shall not be construed as a representation or warranty regarding the proper export classification for such Software or whether an export license or other documentation is required for exporting such Software.
Any links appearing on this Manifest (for example in the “Obtained from” field) were verified at the time the Manifest was created. TI makes no guarantee that any listed links will remain active in the future.
Your company is responsible for confirming the applicable license terms for any open source Software listed in this Manifest that was not “Obtained from” TI. Any open source license specified in this Manifest for Sotware that was not “Obtained from” TI is for TI's internal use only and shall not be construed as a representation of warranty regarding the proper open source license terms for such Software.
ECCN for Software included in this release: Publicly Available
ECCN for Technology (e.g., user documentation, specifications) included in this release: Publicly Available
See Legend above for a description of the columns and possible values.
This table describes any GPLv3 software being delivered that is expected to run on a Development Host, instead of the target device.
Software Name | Version | License | Location | Delivered As | Modified by TI | Obtained from |
gdb-cross-canadian-arm | 9.1-r0.0 | GPLv2 & GPLv3 & LGPLv2 & LGPLv3 | gdb-cross-canadian-arm_9.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/gdb/gdb-9.1.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-autoconf | 2.69-r11.0 | GPLv2 & GPLv3 | nativesdk-autoconf_2.69-r11.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/autoconf/autoconf-2.69.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-bison | 3.5.4-r0.0 | GPLv3 | nativesdk-bison_3.5.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/bison/bison-3.5.4.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-gcc-arm-baremetal | 7-2018 | GPL-3.0-with-GCC-exception & GPLv3 | nativesdk-gcc-arm-baremetal_7-2018-q2-update-r0.0_x86_64-nativesdk.ipk | Binary | No | https://developer.arm.com/-/media/Files/downloads/gnu-rm/7-2018q2/gcc-arm-none-eabi-7-2018-q2-update-linux.tar.bz2;name=gcc-arm-none |
nativesdk-libgdbm6 | 1.18.1-r0.0 | GPLv3 | nativesdk-libgdbm6_1.18.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/gdbm/gdbm-1.18.1.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libgdbm-compat4 | 1.18.1-r0.0 | GPLv3 | nativesdk-libgdbm-compat4_1.18.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/gdbm/gdbm-1.18.1.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libreadline8 | 8.0-r0.0 | GPLv3+ | nativesdk-libreadline8_8.0-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/readline/readline-8.0.tar.gz;name=archive Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-m4 | 1.4.18-r0.0 | GPLv3 | nativesdk-m4_1.4.18-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/m4/m4-1.4.18.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
This table describes any software being delivered that is expected to run on a Development Host, instead of the target device. Some of this software may be licensed under GPLv3 but it is not expected to be shipped as a product.
Software Name | Version | License | Location | Delivered As | Modified by TI | Obtained from |
binutils-cross-canadian-arm | b'2.33.1'-r9.0 | MIT | binutils-cross-canadian-arm_b'2.33.1'-r9.0_x86_64-nativesdk.ipk | Binary | No | |
gcc-cross-canadian-arm | 9.2.1-r9.0 | MIT | gcc-cross-canadian-arm_9.2.1-r9.0_x86_64-nativesdk.ipk | Binary | No | |
gdb-cross-canadian-arm | 9.1-r0.0 | GPLv2 & GPLv3 & LGPLv2 & LGPLv3 | gdb-cross-canadian-arm_9.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/gdb/gdb-9.1.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
meta-environment-am437x-evm | 1.0-r8.0 | MIT | meta-environment-am437x-evm_1.0-r8.0_x86_64-nativesdk.ipk | Binary | No | |
nativesdk-autoconf | 2.69-r11.0 | GPLv2 & GPLv3 | nativesdk-autoconf_2.69-r11.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/autoconf/autoconf-2.69.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-automake | 1.16.1-r0.0 | GPLv2 | nativesdk-automake_1.16.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/automake/automake-1.16.1.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-bison | 3.5.4-r0.0 | GPLv3 | nativesdk-bison_3.5.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/bison/bison-3.5.4.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-buildtools-perl-dummy | 1.0-r2.0 | MIT | nativesdk-buildtools-perl-dummy_1.0-r2.0_buildtools-dummy-nativesdk.ipk | Binary | No | |
nativesdk-ca-certificates | 20210119-r0.0 | GPL-2.0+ & MPL-2.0 | nativesdk-ca-certificates_20210119-r0.0_x86_64-nativesdk.ipk | Binary | No | git://salsa.debian.org/debian/ca-certificates.git;protocol=https Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-clacc | 1.5.6.0-r0.0.0 | BSD | nativesdk-clacc_1.5.6.0-r0.0.0_x86_64-nativesdk.ipk | Binary | No | git://git.ti.com/openmp/ti-openmpacc.git;protocol=git;branch=master |
nativesdk-clocl | 1.2.00.02-r0.0.0 | BSD | nativesdk-clocl_1.2.00.02-r0.0.0_x86_64-nativesdk.ipk | Binary | No | git://git.ti.com/opencl/ti-opencl.git;protocol=git;branch=master |
nativesdk-cmake | 3.16.5-r0.0 | BSD-3-Clause | nativesdk-cmake_3.16.5-r0.0_x86_64-nativesdk.ipk | Binary | No | https://cmake.org/files/v3.16/cmake-3.16.5.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-dtc | 1.6.0-r0.0 | GPLv2 | BSD | nativesdk-dtc_1.6.0-r0.0_x86_64-nativesdk.ipk | Binary | No | git://git.kernel.org/pub/scm/utils/dtc/dtc.git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-flex | 2.6.4-r0.0 | BSD-2-Clause | nativesdk-flex_2.6.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://github.com/westes/flex/releases/download/v2.6.4/flex-2.6.4.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-gcc-arm-baremetal | 7-2018 | GPL-3.0-with-GCC-exception & GPLv3 | nativesdk-gcc-arm-baremetal_7-2018-q2-update-r0.0_x86_64-nativesdk.ipk | Binary | No | https://developer.arm.com/-/media/Files/downloads/gnu-rm/7-2018q2/gcc-arm-none-eabi-7-2018-q2-update-linux.tar.bz2;name=gcc-arm-none |
nativesdk-git | 2.24.3-r0.0 | GPLv2 | nativesdk-git_2.24.3-r0.0_x86_64-nativesdk.ipk | Binary | No | https://cdn.kernel.org/pub/software/scm/git/git-2.24.3.tar.gz;name=tarballhttps://cdn.kernel.org/pub/software/scm/git/git-manpages-2.24.3.tar.gz;name=manpages |
nativesdk-gnu-config | 20200117+git0+5256817ace-r0.0 | GPL-3.0-with-autoconf-exception | nativesdk-gnu-config_20200117+git0+5256817ace-r0.0_x86_64-nativesdk.ipk | Binary | No | git://git.savannah.gnu.org/config.git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-ldconfig | 2.31+git0+f84949f1c4-r0.0 | GPLv2 & LGPLv2.1 | nativesdk-ldconfig_2.31+git0+f84949f1c4-r0.0_x86_64-nativesdk.ipk | Binary | No | git://sourceware.org/git/glibc.git;branch=release/2.31/master;name=glibc Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libarchive | 3.4.2-r0.0 | BSD-2-Clause | nativesdk-libarchive_3.4.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://libarchive.org/downloads/libarchive-3.4.2.tar.gz |
nativesdk-libblkid1 | 2.35.1-r0.0 | GPLv2+ & LGPLv2.1+ & BSD-3-Clause & BSD-4-Clause | nativesdk-libblkid1_2.35.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://cdn.kernel.org/pub/linux/utils/util-linux/v2.35/util-linux-2.35.1.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libbz2-1 | 1.0.8-r0.0 | bzip2-1.0.6 | nativesdk-libbz2-1_1.0.8-r0.0_x86_64-nativesdk.ipk | Binary | No | https://sourceware.org/pub/bzip2/bzip2-1.0.8.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libc6 | 2.31+git0+f84949f1c4-r0.0 | GPLv2 & LGPLv2.1 | nativesdk-libc6_2.31+git0+f84949f1c4-r0.0_x86_64-nativesdk.ipk | Binary | No | git://sourceware.org/git/glibc.git;branch=release/2.31/master;name=glibc Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libcrypt2 | 4.4.15-r0.0 | LGPLv2.1 | nativesdk-libcrypt2_4.4.15-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/besser82/libxcrypt.git;branch=develop |
nativesdk-libcrypto1.1 | 1.1.1j-r0.0 | openssl | nativesdk-libcrypto1.1_1.1.1j-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.openssl.org/source/openssl-1.1.1j.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libcurl4 | 7.69.1-r0.0 | MIT | nativesdk-libcurl4_7.69.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://curl.haxx.se/download/curl-7.69.1.tar.bz2 Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libexpat1 | 2.2.9-r0.0 | MIT | nativesdk-libexpat1_2.2.9-r0.0_x86_64-nativesdk.ipk | Binary | No | https://downloads.sourceforge.net/expat/expat-2.2.9.tar.bz2 Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libffi7 | 3.3-r0.0 | MIT | nativesdk-libffi7_3.3-r0.0_x86_64-nativesdk.ipk | Binary | No | https://github.com/libffi/libffi/releases/download/v3.3/libffi-3.3.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libfl2 | 2.6.4-r0.0 | BSD-2-Clause | nativesdk-libfl2_2.6.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://github.com/westes/flex/releases/download/v2.6.4/flex-2.6.4.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libgcc1 | arm-9.2 | GPL-3.0-with-GCC-exception | nativesdk-libgcc1_arm-9.2-r2019.12.0_x86_64-nativesdk.ipk | Binary | No | |
nativesdk-libgdbm6 | 1.18.1-r0.0 | GPLv3 | nativesdk-libgdbm6_1.18.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/gdbm/gdbm-1.18.1.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libgdbm-compat4 | 1.18.1-r0.0 | GPLv3 | nativesdk-libgdbm-compat4_1.18.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/gdbm/gdbm-1.18.1.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libglib-2.0-0 | 1:2.62.6-r0.0 | LGPLv2.1+ & BSD & PD | nativesdk-libglib-2.0-0_1:2.62.6-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnome.org/pub/GNOME/sources/glib/2.62/glib-2.62.6.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-liblzma5 | 5.2.4-r0.0 | PD | nativesdk-liblzma5_5.2.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://tukaani.org/xz/xz-5.2.4.tar.gz |
nativesdk-liblzo2-2 | 2.10-r0.0 | GPLv2+ | nativesdk-liblzo2-2_2.10-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.oberhumer.com/opensource/lzo/download/lzo-2.10.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libmount1 | 2.35.1-r0.0 | GPLv2+ & LGPLv2.1+ & BSD-3-Clause & BSD-4-Clause | nativesdk-libmount1_2.35.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://cdn.kernel.org/pub/linux/utils/util-linux/v2.35/util-linux-2.35.1.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libncursesw5 | 6.2-r0.0 | MIT | nativesdk-libncursesw5_6.2-r0.0_x86_64-nativesdk.ipk | Binary | No | git://salsa.debian.org/debian/ncurses.git;protocol=https Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libnsl2 | 1.2.0+git0+4a062cf418-r0.0 | LGPL-2.1 | nativesdk-libnsl2_1.2.0+git0+4a062cf418-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/thkukuk/libnsl |
nativesdk-libopkg1 | 1:0.4.2-r0.0 | GPLv2+ | nativesdk-libopkg1_1:0.4.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://downloads.yoctoproject.org/releases/opkg/opkg-0.4.2.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libpanelw5 | 6.2-r0.0 | MIT | nativesdk-libpanelw5_6.2-r0.0_x86_64-nativesdk.ipk | Binary | No | git://salsa.debian.org/debian/ncurses.git;protocol=https Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libpcre1 | 8.44-r0.0 | BSD-3-Clause | nativesdk-libpcre1_8.44-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.pcre.org/pub/pcre/pcre-8.44.tar.bz2 Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libpixman-1-0 | 1:0.38.4-r0.0 | MIT & MIT-style & PD | nativesdk-libpixman-1-0_1:0.38.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://www.cairographics.org/releases/pixman-0.38.4.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libpython3.8-1.0 | 3.8.2-r0.0 | PSFv2 | nativesdk-libpython3.8-1.0_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libreadline8 | 8.0-r0.0 | GPLv3+ | nativesdk-libreadline8_8.0-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/readline/readline-8.0.tar.gz;name=archive Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libsdl2-2.0-0 | 2.0.12-r0.0 | Zlib | nativesdk-libsdl2-2.0-0_2.0.12-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.libsdl.org/release/SDL2-2.0.12.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libsolv | 0.7.10-r0.0 | BSD-3-Clause | nativesdk-libsolv_0.7.10-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/openSUSE/libsolv.git |
nativesdk-libsqlite3-0 | 3:3.31.1-r0.0 | PD | nativesdk-libsqlite3-0_3:3.31.1-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.sqlite.org/2020/sqlite-autoconf-3310100.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libssl1.1 | 1.1.1j-r0.0 | openssl | nativesdk-libssl1.1_1.1.1j-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.openssl.org/source/openssl-1.1.1j.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libstdc++6 | arm-9.2 | GPL-3.0-with-GCC-exception | nativesdk-libstdc++6_arm-9.2-r2019.12.0_x86_64-nativesdk.ipk | Binary | No | |
nativesdk-libtinfo5 | 6.2-r0.0 | MIT | nativesdk-libtinfo5_6.2-r0.0_x86_64-nativesdk.ipk | Binary | No | git://salsa.debian.org/debian/ncurses.git;protocol=https Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libtirpc3 | 1.2.6-r0.0 | BSD-3-Clause | nativesdk-libtirpc3_1.2.6-r0.0_x86_64-nativesdk.ipk | Binary | No | https://downloads.sourceforge.net/libtirpc/libtirpc-1.2.6.tar.bz2 |
nativesdk-libtool | 2.4.6-r0.0 | GPLv2 & LGPLv2.1 | nativesdk-libtool_2.4.6-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/libtool/libtool-2.4.6.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libuuid1 | 2.35.1-r0.0 | GPLv2+ & LGPLv2.1+ & BSD-3-Clause & BSD-4-Clause | nativesdk-libuuid1_2.35.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://cdn.kernel.org/pub/linux/utils/util-linux/v2.35/util-linux-2.35.1.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libx11-6 | 1:1.6.9-r0.0 | MIT & MIT-style & BSD | nativesdk-libx11-6_1:1.6.9-r0.0_x86_64-nativesdk.ipk | Binary | No | https://www.x.org/releases//individual/lib/libX11-1.6.9.tar.bz2 Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libxau6 | 1:1.0.9-r0.0 | MIT-style | nativesdk-libxau6_1:1.0.9-r0.0_x86_64-nativesdk.ipk | Binary | No | https://www.x.org/releases//individual/lib/libXau-1.0.9.tar.bz2 |
nativesdk-libxcb1 | 1.13.1-r0.0 | MIT | nativesdk-libxcb1_1.13.1-r0.0_x86_64-nativesdk.ipk | Binary | No | http://xcb.freedesktop.org/dist/libxcb-1.13.1.tar.bz2 Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libxdmcp6 | 1:1.1.3-r0.0 | MIT-style | nativesdk-libxdmcp6_1:1.1.3-r0.0_x86_64-nativesdk.ipk | Binary | No | https://www.x.org/releases//individual/lib/libXdmcp-1.1.3.tar.bz2 |
nativesdk-libxml2-2 | 2.9.10-r0.0 | MIT | nativesdk-libxml2-2_2.9.10-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.xmlsoft.org/sources/libxml2-2.9.10.tar.gz;name=libtarhttp://www.w3.org/XML/Test/xmlts20080827.tar.gz;subdir=libxml2-2.9.10;name=testtar Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-libz1 | 1.2.11-r0.0 | Zlib | nativesdk-libz1_1.2.11-r0.0_x86_64-nativesdk.ipk | Binary | No | https://downloads.sourceforge.net/libpng/zlib/1.2.11/zlib-1.2.11.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-m4 | 1.4.18-r0.0 | GPLv3 | nativesdk-m4_1.4.18-r0.0_x86_64-nativesdk.ipk | Binary | No | https://ftp.gnu.org/gnu/m4/m4-1.4.18.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-makedevs | 1.0.1-r0.0 | GPLv2 | nativesdk-makedevs_1.0.1-r0.0_x86_64-nativesdk.ipk | Binary | No | Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-mbedtls | 2.16.6-r0.0 | Apache-2.0 | nativesdk-mbedtls_2.16.6-r0.0_x86_64-nativesdk.ipk | Binary | No | https://tls.mbed.org/download/mbedtls-2.16.6-apache.tgz |
nativesdk-meson | 0.53.2-r0.0 | Apache-2.0 | nativesdk-meson_0.53.2-r0.0_x86_64-nativesdk.ipk | Binary | No | https://github.com/mesonbuild/meson/releases/download/0.53.2/meson-0.53.2.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-mtd-utils-ubifs | 2.1.1-r0.arago1.0 | GPLv2+ | nativesdk-mtd-utils-ubifs_2.1.1-r0.arago1.0_x86_64-nativesdk.ipk | Binary | No | git://git.infradead.org/mtd-utils.git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-ncurses-terminfo-base | 6.2-r0.0 | MIT | nativesdk-ncurses-terminfo-base_6.2-r0.0_x86_64-nativesdk.ipk | Binary | No | git://salsa.debian.org/debian/ncurses.git;protocol=https Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-ninja | 1.10.0-r0.0 | Apache-2.0 | nativesdk-ninja_1.10.0-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/ninja-build/ninja.git;branch=release |
nativesdk-open62541-examples | 1.0.1+git0+e4309754fc-r0.0 | MPL-2.0 | nativesdk-open62541-examples_1.0.1+git0+e4309754fc-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/open62541/open62541.git;protocol=https;branch=1.0git://github.com/OPCFoundation/UA-Nodeset.git;protocol=https;branch=v1.04;destsuffix=git/deps/ua-nodeset;name=ua-nodesetgit://github.com/Pro/mdnsd.git;protocol=https;branch=master;destsuffix=git/deps/mdnsd;name=mdnsd Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-open62541-tests | 1.0.1+git0+e4309754fc-r0.0 | MPL-2.0 | nativesdk-open62541-tests_1.0.1+git0+e4309754fc-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/open62541/open62541.git;protocol=https;branch=1.0git://github.com/OPCFoundation/UA-Nodeset.git;protocol=https;branch=v1.04;destsuffix=git/deps/ua-nodeset;name=ua-nodesetgit://github.com/Pro/mdnsd.git;protocol=https;branch=master;destsuffix=git/deps/mdnsd;name=mdnsd Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-openssl-bin | 1.1.1j-r0.0 | openssl | nativesdk-openssl-bin_1.1.1j-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.openssl.org/source/openssl-1.1.1j.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-openssl-conf | 1.1.1j-r0.0 | openssl | nativesdk-openssl-conf_1.1.1j-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.openssl.org/source/openssl-1.1.1j.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-openssl | 1.1.1j-r0.0 | openssl | nativesdk-openssl_1.1.1j-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.openssl.org/source/openssl-1.1.1j.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-opkg | 1:0.4.2-r0.0 | GPLv2+ | nativesdk-opkg_1:0.4.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://downloads.yoctoproject.org/releases/opkg/opkg-0.4.2.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-packagegroup-arago-qte-toolchain-host | 1.0-r10.0 | MIT | nativesdk-packagegroup-arago-qte-toolchain-host_1.0-r10.0_x86_64-nativesdk.ipk | Binary | No | |
nativesdk-packagegroup-arago-tisdk-host | 1.0-r2.0 | MIT | nativesdk-packagegroup-arago-tisdk-host_1.0-r2.0_x86_64-nativesdk.ipk | Binary | No | |
nativesdk-packagegroup-sdk-host | 1.0-r12.0 | MIT | nativesdk-packagegroup-sdk-host_1.0-r12.0_x86_64-nativesdk.ipk | Binary | No | |
nativesdk-pkgconfig | 0.29.2+git0+edf8e6f0ea-r0.0 | GPLv2+ | nativesdk-pkgconfig_0.29.2+git0+edf8e6f0ea-r0.0_x86_64-nativesdk.ipk | Binary | No | git://anongit.freedesktop.org/pkg-config Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-pseudo | 1.9.0+git0+60e25a3655-r0.0 | LGPL2.1 | nativesdk-pseudo_1.9.0+git0+60e25a3655-r0.0_x86_64-nativesdk.ipk | Binary | No | git://git.yoctoproject.org/pseudo;branch=oe-core Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-2to3 | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-2to3_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-asyncio | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-asyncio_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-audio | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-audio_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-codecs | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-codecs_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-compile | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-compile_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-compression | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-compression_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-core | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-core_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-crypt | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-crypt_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-ctypes | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-ctypes_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-curses | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-curses_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-datetime | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-datetime_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-db | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-db_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-debugger | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-debugger_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-difflib | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-difflib_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-distutils | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-distutils_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-doctest | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-doctest_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-email | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-email_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-fcntl | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-fcntl_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-html | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-html_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-idle | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-idle_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-image | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-image_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-io | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-io_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-json | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-json_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-logging | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-logging_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-mailbox | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-mailbox_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-math | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-math_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-mime | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-mime_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-misc | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-misc_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-mmap | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-mmap_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-modules | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-modules_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-multiprocessing | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-multiprocessing_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-netclient | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-netclient_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-netserver | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-netserver_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-nose | 1.3.7-r0.0 | LGPLv2.1 | nativesdk-python3-nose_1.3.7-r0.0_x86_64-nativesdk.ipk | Binary | No | https://files.pythonhosted.org/packages/source/n/nose/nose-1.3.7.tar.gz |
nativesdk-python3-numbers | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-numbers_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-numpy | 1.17.4-r0.0 | BSD-3-Clause & BSD-2-Clause & PSF & Apache-2.0 & BSD & MIT | nativesdk-python3-numpy_1.17.4-r0.0_x86_64-nativesdk.ipk | Binary | No | https://github.com/numpy/numpy/releases/download/v1.17.4/numpy-1.17.4.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-pickle | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-pickle_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-pkg-resources | 45.2.0-r0.0 | MIT | nativesdk-python3-pkg-resources_45.2.0-r0.0_x86_64-nativesdk.ipk | Binary | No | https://files.pythonhosted.org/packages/source/s/setuptools/setuptools-45.2.0.zip Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-pkgutil | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-pkgutil_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-plistlib | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-plistlib_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-pprint | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-pprint_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-profile | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-profile_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-pydoc | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-pydoc_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-resource | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-resource_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-setuptools | 45.2.0-r0.0 | MIT | nativesdk-python3-setuptools_45.2.0-r0.0_x86_64-nativesdk.ipk | Binary | No | https://files.pythonhosted.org/packages/source/s/setuptools/setuptools-45.2.0.zip Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-shell | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-shell_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-smtpd | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-smtpd_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-sqlite3 | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-sqlite3_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-stringold | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-stringold_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-syslog | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-syslog_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-terminal | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-terminal_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-threading | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-threading_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-tkinter | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-tkinter_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-typing | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-typing_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-unittest | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-unittest_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-unixadmin | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-unixadmin_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-venv | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-venv_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-xml | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-xml_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-python3-xmlrpc | 3.8.2-r0.0 | PSFv2 | nativesdk-python3-xmlrpc_3.8.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://www.python.org/ftp/python/3.8.2/Python-3.8.2.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-qemu | 4.2.0-r0.0 | GPLv2 & LGPLv2.1 | nativesdk-qemu_4.2.0-r0.0_x86_64-nativesdk.ipk | Binary | No | https://download.qemu.org/qemu-4.2.0.tar.xz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-qemu-helper | 1.0-r9.0 | GPLv2 | nativesdk-qemu-helper_1.0-r9.0_x86_64-nativesdk.ipk | Binary | No | Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-qtbase | 5.14.2+git0+3a6d8df521-r0.0 | GFDL-1.3 & BSD & ( GPL-3.0 & The-Qt-Company-GPL-Exception-1.0 | The-Qt-Company-Commercial ) & ( GPL-2.0+ | LGPL-3.0 | The-Qt-Company-Commercial ) | nativesdk-qtbase_5.14.2+git0+3a6d8df521-r0.0_x86_64-nativesdk.ipk | Binary | No | git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.14;protocol=git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-qttools | 5.14.2+git0+9d5d92a492-r0.0 | GFDL-1.3 & BSD & ( GPL-3.0 & The-Qt-Company-GPL-Exception-1.0 | The-Qt-Company-Commercial ) & ( GPL-2.0+ | LGPL-3.0 | The-Qt-Company-Commercial ) | nativesdk-qttools_5.14.2+git0+9d5d92a492-r0.0_x86_64-nativesdk.ipk | Binary | No | git://code.qt.io/qt/qttools.git;name=qttools;branch=5.14;protocol=git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-qttools-plugins | 5.14.2+git0+9d5d92a492-r0.0 | GFDL-1.3 & BSD & ( GPL-3.0 & The-Qt-Company-GPL-Exception-1.0 | The-Qt-Company-Commercial ) & ( GPL-2.0+ | LGPL-3.0 | The-Qt-Company-Commercial ) | nativesdk-qttools-plugins_5.14.2+git0+9d5d92a492-r0.0_x86_64-nativesdk.ipk | Binary | No | git://code.qt.io/qt/qttools.git;name=qttools;branch=5.14;protocol=git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-qttools-qmlplugins | 5.14.2+git0+9d5d92a492-r0.0 | GFDL-1.3 & BSD & ( GPL-3.0 & The-Qt-Company-GPL-Exception-1.0 | The-Qt-Company-Commercial ) & ( GPL-2.0+ | LGPL-3.0 | The-Qt-Company-Commercial ) | nativesdk-qttools-qmlplugins_5.14.2+git0+9d5d92a492-r0.0_x86_64-nativesdk.ipk | Binary | No | git://code.qt.io/qt/qttools.git;name=qttools;branch=5.14;protocol=git Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-sdk-provides-dummy | 1.0-r0.0 | MIT | nativesdk-sdk-provides-dummy_1.0-r0.0_sdk-provides-dummy-nativesdk.ipk | Binary | No | |
nativesdk-shadow | 4.8.1-r0.0 | BSD | Artistic-1.0 | nativesdk-shadow_4.8.1-r0.0_x86_64-nativesdk.ipk | Binary | No | https://github.com/shadow-maint/shadow/releases/download/4.8.1/shadow-4.8.1.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-shared-mime-info | 1.15-r0.0 | GPLv2 | nativesdk-shared-mime-info_1.15-r0.0_x86_64-nativesdk.ipk | Binary | No | git://gitlab.freedesktop.org/xdg/shared-mime-info.git;protocol=https |
nativesdk-ti-cgt6x | 1:8.3.2-r0.0 | (TI-TSPA & Thai-Open-Source-Software-Center) & BSD-3-Clause & BSL-1.0 & Patrick-Powell & AFL-3.0 & MIT & BSD-2-Clause & PD | nativesdk-ti-cgt6x_1:8.3.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://software-dl.ti.com/codegen/esd/cgt_public_sw/C6000/8.3.2/ti_cgt_c6000_8.3.2_linux_installer_x86.bin;name=cgt6x_x86_installer |
nativesdk-ti-cgt-pru | 2.3.2-r0.0 | (TI-TSPA & Thai-Open-Source-Software-Center) & BSD-3-Clause & BSL-1.0 & Hewlett-Packard & AFL-3.0 & MIT & BSD-2-Clause & PD | nativesdk-ti-cgt-pru_2.3.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://software-dl.ti.com/codegen/esd/cgt_public_sw/PRU/2.3.2/ti_cgt_pru_2.3.2_linux_installer_x86.bin;name=cgt-pru-x86 |
nativesdk-unfs3 | 0.9.22+0+c12a5c69a8-r0.0 | unfs3 | nativesdk-unfs3_0.9.22+0+c12a5c69a8-r0.0_x86_64-nativesdk.ipk | Binary | No | git://github.com/unfs3/unfs3.git;protocol=https Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
nativesdk-update-alternatives-opkg | 0.4.2-r0.0 | GPLv2+ | nativesdk-update-alternatives-opkg_0.4.2-r0.0_x86_64-nativesdk.ipk | Binary | No | http://git.yoctoproject.org/cgit/cgit.cgi/opkg-utils/snapshot/opkg-utils-0.4.2.tar.gz Files from: git://arago-project.org/git/meta-arago.git git://arago-project.org/git/meta-ti.git |
packagegroup-cross-canadian-am437x-evm | 1.0-r0.arago0.0 | MIT | packagegroup-cross-canadian-am437x-evm_1.0-r0.arago0.0_x86_64-nativesdk.ipk | Binary | No |
This table describes any GPLv3 software being delivered that is expected to run on the target device.
This table describes any software being delivered that is expected to run on the target device.