AM263Px MCU+ SDK  26.00.00
ub_strutils.h File Reference

Introduction

Utility functions for strings.

Go to the source code of this file.

Typedefs

typedef uint8_t ub_bytearray8_t[8]
 8-byte binary array More...
 
typedef ub_bytearray8_t ub_streamid_t
 8-byte binary array is used for Stream ID More...
 
typedef uint8_t ub_bytearray6_t[6]
 6-byte binary array More...
 
typedef ub_bytearray6_t ub_macaddr_t
 6-byte binary array is used for MAC Address More...
 

Functions

void ub_hexdump (bool console, bool debug, unsigned char *buf, int size, int addr)
 dump out data in hex format to the console More...
 
void ub_byte2hexstr (uint8_t a, char *astr)
 convert a byte to 2-digit hex string More...
 
int ub_hexstr2barray (const char *bstr, uint8_t *bytes, const char delim, int len)
 convert array of 2-digit hex string More...
 
char * ub_bmac2smac (ub_macaddr_t bmac, char *smac)
 convert a binary type mac address to a string type mac address('XX:XX:XX:XX:XX:XX' format) More...
 
uint8_t * ub_smac2bmac (const char *smac, ub_macaddr_t bmac)
 convert a string type mac address('XX:XX:XX:XX:XX:XX' format) to a binary type mac address. More...
 
char * ub_bsid2ssid (ub_streamid_t bsid, char *ssid)
 convert a binary type stream id to a string type stream id ('XX:XX:XX:XX:XX:XX:XX:XX' format) More...
 
uint8_t * ub_ssid2bsid (const char *ssid, ub_streamid_t bsid)
 convert a string type stream id('XX:XX:XX:XX:XX:XX:XX:XX' format) to a binary type stream id More...
 
int ub_str2bytearray (uint8_t *dest, const char *input, uint8_t base)
 convert a string type byte array('01,00,1e,00,00,03,....02,00,01') to a byte array More...
 
char * ub_bytearray2str (char *dest, const unsigned char *bytes, int len)
 convert a byte array to a string type byte array('01,00,1e,00,00,03,....02,00,01') More...
 
int ub_find_nospace (const char *astr, int maxn)
 look for non space charcter and return the number of passed characters More...
 
int ub_find_space (const char *astr, int maxn)
 look for space charcter and return the number of passed characters More...
 
int ub_command_line_parser (char *line, char *argv[], int maxargc)
 parse a command line string and make argc,argv[] for main function, More...
 
int ub_strncpy (char *dest, const char *src, int maxlen)
 copy a string More...