AM263Px MCU+ SDK  26.00.00
uart_dma_edma.h File Reference

Go to the source code of this file.

Data Structures

struct  UART_EdmaChConfig
 
struct  UART_DmaConfig
 UART DMA Configuration, these are filled by SysCfg based on the DMA driver that is selected. More...
 

Typedefs

typedef struct UART_EdmaChConfig_s * UART_DmaChConfig
 
typedef EDMA_ConfigUART_DmaHandle
 

Typedef Documentation

◆ UART_DmaChConfig

typedef struct UART_EdmaChConfig_s* UART_DmaChConfig

◆ UART_DmaHandle