AM263Px MCU+ SDK  26.00.00
delayReqRespParams_t Struct Reference

Detailed Description

Parameters required for calculating Cable Delay.

Data Fields

uint64_t correctionField
 
uint64_t timeStampSec
 
uint32_t timeStampNS
 
uint32_t delReqTxTsSec
 
uint32_t delReqTxTsNS
 

Field Documentation

◆ correctionField

uint64_t delayReqRespParams_t::correctionField

Correction Field. Nanoseconds

◆ timeStampSec

uint64_t delayReqRespParams_t::timeStampSec

Delay Response Rx Timestamp on master in (seconds)

◆ timeStampNS

uint32_t delayReqRespParams_t::timeStampNS

Delay Response Rx Timestamp on master in nanoseconds

◆ delReqTxTsSec

uint32_t delayReqRespParams_t::delReqTxTsSec

Delay Request Tx Timestamp in Seconds

◆ delReqTxTsNS

uint32_t delayReqRespParams_t::delReqTxTsNS

Delay Request Tx Timestamp in Nanoseconds