AM263Px MCU+ SDK  26.00.00

Detailed Description

Parameters passed during TCA6424_open()

Data Fields

uint32_t i2cInstance
 
uint32_t i2cAddress
 

Field Documentation

◆ i2cInstance

uint32_t TCA6424_Params::i2cInstance

Underlying peripheral driver instance that is used by the IO Expander driver incase of I2C controlled IO Expander

◆ i2cAddress

uint32_t TCA6424_Params::i2cAddress

I2C address for IO expander