AM263Px MCU+ SDK  26.00.00

Detailed Description

Structure containing R5F CPU Static Registers.

Design: PROC_SDL-6331

Data Fields

uint32_t SCTLR
 
uint32_t ACTLR
 
uint32_t SecondaryACTLR
 
uint32_t CPACR
 
uint32_t BTCMRegionR
 
uint32_t ATCMRegionR
 
uint32_t SlavePortControlR
 
uint32_t CONTEXTIDR
 
uint32_t nVALIRQSET
 
uint32_t nVALFIQSET
 
uint32_t nVALRESETSET
 
uint32_t nVALDEBUGSET
 
uint32_t nVALIRQCLEAR
 
uint32_t nVALFIQCLEAR
 
uint32_t nVALRESETCLEAR
 
uint32_t nVALDEBUGCLEAR
 
uint32_t BuildOption1R
 
uint32_t BuildOption2R
 
uint32_t PinOptionR
 
uint32_t LLPPnormalAXIRR
 
uint32_t LLPPvirtualAXIRR
 
uint32_t AHBRR
 
uint32_t PMCR
 
uint32_t PMCNTENSET
 
uint32_t PMUSERENR
 
uint32_t PMINTENSET
 
uint32_t PMINTENCLR
 

Field Documentation

◆ SCTLR

uint32_t SDL_R5FCPU_StaticRegs::SCTLR

◆ ACTLR

uint32_t SDL_R5FCPU_StaticRegs::ACTLR

◆ SecondaryACTLR

uint32_t SDL_R5FCPU_StaticRegs::SecondaryACTLR

◆ CPACR

uint32_t SDL_R5FCPU_StaticRegs::CPACR

◆ BTCMRegionR

uint32_t SDL_R5FCPU_StaticRegs::BTCMRegionR

◆ ATCMRegionR

uint32_t SDL_R5FCPU_StaticRegs::ATCMRegionR

◆ SlavePortControlR

uint32_t SDL_R5FCPU_StaticRegs::SlavePortControlR

◆ CONTEXTIDR

uint32_t SDL_R5FCPU_StaticRegs::CONTEXTIDR

◆ nVALIRQSET

uint32_t SDL_R5FCPU_StaticRegs::nVALIRQSET

◆ nVALFIQSET

uint32_t SDL_R5FCPU_StaticRegs::nVALFIQSET

◆ nVALRESETSET

uint32_t SDL_R5FCPU_StaticRegs::nVALRESETSET

◆ nVALDEBUGSET

uint32_t SDL_R5FCPU_StaticRegs::nVALDEBUGSET

◆ nVALIRQCLEAR

uint32_t SDL_R5FCPU_StaticRegs::nVALIRQCLEAR

◆ nVALFIQCLEAR

uint32_t SDL_R5FCPU_StaticRegs::nVALFIQCLEAR

◆ nVALRESETCLEAR

uint32_t SDL_R5FCPU_StaticRegs::nVALRESETCLEAR

◆ nVALDEBUGCLEAR

uint32_t SDL_R5FCPU_StaticRegs::nVALDEBUGCLEAR

◆ BuildOption1R

uint32_t SDL_R5FCPU_StaticRegs::BuildOption1R

◆ BuildOption2R

uint32_t SDL_R5FCPU_StaticRegs::BuildOption2R

◆ PinOptionR

uint32_t SDL_R5FCPU_StaticRegs::PinOptionR

◆ LLPPnormalAXIRR

uint32_t SDL_R5FCPU_StaticRegs::LLPPnormalAXIRR

◆ LLPPvirtualAXIRR

uint32_t SDL_R5FCPU_StaticRegs::LLPPvirtualAXIRR

◆ AHBRR

uint32_t SDL_R5FCPU_StaticRegs::AHBRR

◆ PMCR

uint32_t SDL_R5FCPU_StaticRegs::PMCR

◆ PMCNTENSET

uint32_t SDL_R5FCPU_StaticRegs::PMCNTENSET

◆ PMUSERENR

uint32_t SDL_R5FCPU_StaticRegs::PMUSERENR

◆ PMINTENSET

uint32_t SDL_R5FCPU_StaticRegs::PMINTENSET

◆ PMINTENCLR

uint32_t SDL_R5FCPU_StaticRegs::PMINTENCLR