AM263Px MCU+ SDK  26.00.00
PeakHistogram_observationalData Struct Reference

Detailed Description

Struct to hold the peakHistogram Buckets for Ideal Sample Calculation by SW. once the auto ideal sample detection has ran for the given train limit, these histograms may be read the bucket with highest value may be selected as the ideal sample bucket.

Values that can be passed to RDC_getPeakHistogramObservationalData() as, PeakHistogram_observationalData parameter

Data Fields

uint8_t peakHistgoramBucket [20]
 

Field Documentation

◆ peakHistgoramBucket

uint8_t PeakHistogram_observationalData::peakHistgoramBucket[20]