AM263Px MCU+ SDK  26.00.00

Detailed Description

This is the entire OTFA structure which holds all regions' information 4 regions in AM263Px and AM261x.

Data Fields

OTFA_Region_t OTFA_Reg [4]
 
uint8_t numRegions
 
uint8_t keySize
 
uint8_t macSize
 
uint8_t masterEnable
 

Field Documentation

◆ OTFA_Reg

OTFA_Region_t OTFA_Config_t::OTFA_Reg[4]

◆ numRegions

uint8_t OTFA_Config_t::numRegions

◆ keySize

uint8_t OTFA_Config_t::keySize

◆ macSize

uint8_t OTFA_Config_t::macSize

◆ masterEnable

uint8_t OTFA_Config_t::masterEnable