AM263Px MCU+ SDK  26.00.00

Detailed Description

Region config structure, this used by SysConfig and not to be used by end-users directly.

Data Fields

uint32_t baseAddr
 
uint32_t size
 
MpuP_RegionAttrs attrs
 

Field Documentation

◆ baseAddr

uint32_t MpuP_RegionConfig::baseAddr

region start address, MUST aligned to region size

◆ size

uint32_t MpuP_RegionConfig::size

region size, see MpuP_RegionSize

◆ attrs

MpuP_RegionAttrs MpuP_RegionConfig::attrs

region attributes, see MpuP_RegionAttrs