AM263Px MCU+ SDK  26.00.00
KeyWriterCertHeader_t Struct Reference

Detailed Description

This is a keywriter_cert_header type which holds the information of customer key certificate and debug responce.

Data Fields

uint8_t * certAddress
 
uint32_t certSize
 
uint32_t debugResponse
 
uint32_t reserved
 

Field Documentation

◆ certAddress

uint8_t* KeyWriterCertHeader_t::certAddress

◆ certSize

uint32_t KeyWriterCertHeader_t::certSize

◆ debugResponse

uint32_t KeyWriterCertHeader_t::debugResponse

◆ reserved

uint32_t KeyWriterCertHeader_t::reserved